Cypress
  • Products & Partners
  • Manufacturers
  • Cypress
  • More
  • Cancel
Cypress
Forum QUERY- Regarding PSoC Programming using Miniprog3.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 7 subscribers
  • Views 647 views
  • Users 0 members are here
Related

QUERY- Regarding PSoC Programming using Miniprog3.

e14 Contributor
e14 Contributor over 16 years ago

Hello

 

I have procured sample of PSoC 1 device part no CY8C28645-24LTXI and also the programmer for the same i.e Miniprog3 part no  CY8CKIT-002CY8CKIT-002 Miniprog3 I have got done the design for the target board(See attachment 1 for pin details file name PLACEMENT.pdf so as to program my device I connected the miniprog3 to the target board run the PSoC Designer 5.0 and have tried to program my device using all these setup I have written the application program and also done with user module configuration prior writing the application The application is compiled built successfully without any errors nor warnings I have come across a problem during programming i.e"Cannot acquire device Please verify the device connection to the programmer(Check attachment 2 for snap shot of the error msg fine name errormsg.bmp I have referred a document for pin configuration which is attached in attachment 3(file name miniprog3 connector.pdf I have verified the pin connections from the programmer to the target board finding no errors Please provide some information on this

Attachments:
imageminiprog3 connector.pdf
image
imagePLACEMENT.pdf
  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hello Manohar,

     

    From the files attached, looks like you are using JTAG connector to program PSoC1 part. Please use 5 pin header available on miniprog3 to program PSoC1 devices.

     

    Best regards,

    Sachin