Cypress
  • Products & Partners
  • Manufacturers
  • Cypress
  • More
  • Cancel
Cypress
Documents PRESS RELEASE - Cypress - New Cypress Kit Demonstrates Precision Analog of PSoC®︎ 3 Architecture via Highly Integrated Voltmeter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rwang
  • Date Created: 28 Dec 2009 6:59 AM Date Created
  • Last Updated Last Updated: 7 Oct 2021 2:09 AM
  • Views 596 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

PRESS RELEASE - Cypress - New Cypress Kit Demonstrates Precision Analog of PSoC®︎ 3 Architecture via Highly Integrated Voltmeter

Device Leverages 20-bit Delta Sigma ADC to Offer Unparalleled Analog Integration, Enabling Concurrent Measurement of Low-Amplitude Signals and Functions such as LCD Drive

 

SAN JOSE, Calif., December 7, 2009 – Cypress Semiconductor Corp. (NASDAQ: CY) today introduced a demonstration kit highlighting the broad precision analog capabilities of its new PSoCRegistered 3 architecture. The new CY8CKIT-007 PSoC 3 Precision Analog Voltmeter Demo Kit showcases a PSoC 3 device as a single-chip voltmeter, using an onboard 20-bit Delta Sigma Analog-to-Digital Converter (ADC) to measure the voltage from the included test leads and onboard thermocouple while directly driving an LCD. With the kit, designers can use pre-configured op amp, ADC and analog mux components in the PSoC CreatorTm Integrated Development Environment (IDE) to quickly and easily design industrial sensors, consumer sensors, glucose meters and other analog applications.

 

The flexible PSoC 3 architecture combines highly integrated, programmable analog and digital peripheral functions, memory and a microcontroller on a single chip. Precise analog resources available in the kit include four digital-to-analog converters (DACs), four comparators, four op amps and  four PGAs, TIAs or Mixers. The voltmeter in the kit measures -30V to 30V of DC signals and includes an onboard thermocouple that is used as a low-noise voltage input. More information on the kit is available at www.cypress.com/go/cy8ckit-007.

 

PSoC 3 and PSoC 5 devices extend the world’s only programmable analog and digital embedded design platform, delivering unmatched time-to-market, integration, and flexibility across 8-, 16-, and 32-bit applications. The platform is powered by the revolutionary PSoC Creator IDE, which introduces a unique schematic-based design methodology along with fully tested, pre-packaged analog and digital peripherals easily customizable through user-intuitive wizards and APIs to meet specific design requirements.

 

“The new Voltmeter Demo kit provides a practical application of the powerful precision analog capabilities of the PSoC 3 architecture,” said Matt Branda, director of marketing for PSoC products at Cypress. “With the kit, designers get a feel for the high-level of analog integration enabled by PSoC 3, along with the simplicity of analog design through our PSoC Creator IDE.”

 

The PSoC 3 Precision Analog Voltmeter Demo Kit contains:


• The PSoC 3-based voltmeter
• Test leads
• USB battery pack with two AA batteries
• Quick Start Guide
• Kit CD, which includes: PSoC Creator, PSoC Programmer, sample projects and documentation.

 

Availability and Photo


The CY8CKIT-007 PSoC 3 Precision Analog Voltmeter Demo Kit is priced at US $79 and is available on the Cypress eShop at www.cypress.com or through authorized distributors. A high-resolution photo of the CY8CKIT-007 kit is available at www.cypress.com/go/VoltmeterKitphoto.

 

About PSoC 3 and PSoC 5


The new PSoC 3 and PSoC 5 architectures include high-precision programmable analog capability (up to 20-bit resolution for an Analog to Digital Converter) and expanded programmable digital resources integrated with powerful, industry-standard MCU cores and ample memory and communications peripherals. The PSoC 3 devices are based on a new, high-performance 8-bit 8051 processor, while the PSoC 5 devices include a powerful 32-bit ARM CortexTm-M3 processor. The new products provide designers with a seamless, programmable design platform, enabling easy migration from 8 to 32 bits. The robust features of these new solutions dramatically expand the applications and markets that PSoC can address, including automotive, portable medical, industrial and many more. More information about PSoC products is available at www.cypress.com/psoc and free online training is at www.cypress.com/psoctraining.

 

About Cypress


Cypress delivers high-performance, mixed-signal, programmable solutions that provide customers with rapid time-to-market and exceptional system value. Cypress offerings include the flagship PSoCRegistered programmable system-on-chip families and derivatives such as PowerPSoCRegistered solutions for high-voltage and LED lighting applications, CapSenseRegistered touch sensing and TrueTouchTm solutions for touchscreens. Cypress is the world leader in USB controllers, including the high-performance West BridgeRegistered solution that enhances connectivity and performance in multimedia handsets. Cypress is also a leader in high-performance memories and programmable timing devices. Cypress serves numerous markets including consumer, mobile handsets, computation, data communications, automotive, industrial and military. Cypress trades on the NASDAQ Global Select Market under the ticker symbol CY. Visit Cypress online at www.cypress.com.

  • lighting
  • sp:cypress
  • pt:led
  • tc:events
  • at:press_release