Intel
  • Products & Partners
  • Manufacturers
  • Intel
  • More
  • Cancel
Intel
Forum Win an Intel Edison: Simply Share Your Idea Here
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Intel to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 61 replies
  • Subscribers 44 subscribers
  • Views 7170 views
  • Users 0 members are here
  • competition
  • giveaway
  • projects
  • dev kit
  • contest
  • iot
  • intel edison
Related

Win an Intel Edison: Simply Share Your Idea Here

jwatson
jwatson over 9 years ago

FIVE lucky element14 Members will each receive an IntelRegistered Edison board to build a cool IntelRegistered project...and it's so simple to win!

 

How to Win

In the comments section below, give an idea of what you would create with the Intel Edison Kit ...and if you win, post a blog about your project in the Intel  space.

 

Your comment could contain:

  • a simple description of your idea
  • diagrams, schematics or sketches
  • a short video message
  • ...basically, anything to get across your idea

 

 

Need inspiration?  See Nine Awesome Intel Edison Projects.

 

 

Comment by midnight (GMT) on January 6, 2017 for a chance to win an IntelRegistered Edison development kit.

 

Winners will be announced on January 10, 2017.

 

Full Terms & Conditions >

image

Buy Intel Edison NowBuy Intel Edison Now

 

The IntelRegistered Edison is a Development Platform designed as a low-cost entry board for start-up product designers and pro-makers; with the Edison you can rapidly prototype and produce IoT and wearable computing products.

  • Sign in to reply
  • Cancel

Top Replies

  • sandeepdwivedi17
    sandeepdwivedi17 over 9 years ago +7
    Automated car parking assistance for difficult spaces according to following GIF
  • rsc
    rsc over 9 years ago +6
    I just finished adding insulation and weather seal to my greenhouse for extending the growing season through winter. I have some controls, sensors, and camera system installed, but they are not all connected…
  • jwatson
    jwatson over 9 years ago +5
    Congratulations to our 5 lucky Intel Giveaway winners! You've just won an Intel Edison Kit for Arduino to bring to life your ideas poised and post a blog about your project in the Intel space. Please direct…
Parents
  • vandia
    vandia over 9 years ago

    I got started on electronic engineering to make gadgets and props at comic conventions. I afterwards got into robotics for the same reason, to make a robot of a wolf from an anime. So far, I've yet to make that one but have made several other robots, from home security that target's faces when activated and emails them to me; to intelligent costume wings.

     

    I would use this for a project I've been designing for about two years, but have just recently found a reliable friend for a wielder: I plan to make an animal mech inspired by Zoids, a smaller model that you can ride inside. I have had the wiring and control panel schematics for a while, and started some of the programming, but I've lacked enough power to program things how I want them to be.

     

    I've been using a RasPi with an Arduino to control and collect system information, but the Arduino can only read and send one analog stream at once, unlike the PixAxe which I could stream multiple sources from, but am limited to 4 inputs per board. I also plan to connect it to screens for targeting programs, to be able to shoot airsoft or other projectiles. Another problem I face with my current systems is that the current boards may not be powerful enough to properly coordinate sensors fast enough to properly identify and target by quadrants, as I plan to install a voice-command system for targeting at some point. Bottom line is, programming is more limited on these boards, with mostly only Python easily accessible on one, and Basic on the other.

     

    Part of the reason for me starting to build this is because I have an undying love for Zoids and want to ride in one. I wanted to make a multiplayer Zoids fan game, but am building one inspired by it instead as a tribute in a sense, because of copyright; and the mech I make will be in that game. I'm heavily tied into several local fan groups, including the Louisiana Airship and Steampunk Society (LASS), the Star Wars Rebel Legion, and a few others; if all goes as planned with this, it could change the standard for props and even mechs in this area, which is starting to grow in popularity.

     

    Also, Element14 will be listed as a contributor for this project anywhere relevant, including at conventions and on the local community site for these things, once that site's relaunch is complete.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • spannerspencer
    spannerspencer over 9 years ago in reply to vandia

    Zoids?! image Those were soooo awesome, and well overdue for a reboot/re-release!

     

    Although you might be showing your age a bit there, same as me  image  I remember buying the red mammoth one from Harrods, of all places, on a rare trip to That London when I was a kid.

     

    Check out my awesome Zoids poster that I still have (and intend to get framed and put up on the wall):

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jlangbridge
    jlangbridge over 9 years ago in reply to spannerspencer

    You must have an awesome office image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jlangbridge
    jlangbridge over 9 years ago in reply to spannerspencer

    You must have an awesome office image