Intel
  • Products
  • Manufacturers
  • Intel
  • More
  • Cancel
Intel
Forum Win an Intel Edison: Simply Share Your Idea Here
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Intel to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 61 replies
  • Subscribers 44 subscribers
  • Views 6799 views
  • Users 0 members are here
  • competition
  • giveaway
  • projects
  • dev kit
  • contest
  • iot
  • intel edison
Related

Win an Intel Edison: Simply Share Your Idea Here

jwatson
jwatson over 9 years ago

FIVE lucky element14 Members will each receive an IntelRegistered Edison board to build a cool IntelRegistered project...and it's so simple to win!

 

How to Win

In the comments section below, give an idea of what you would create with the Intel Edison Kit ...and if you win, post a blog about your project in the Intel  space.

 

Your comment could contain:

  • a simple description of your idea
  • diagrams, schematics or sketches
  • a short video message
  • ...basically, anything to get across your idea

 

 

Need inspiration?  See Nine Awesome Intel Edison Projects.

 

 

Comment by midnight (GMT) on January 6, 2017 for a chance to win an IntelRegistered Edison development kit.

 

Winners will be announced on January 10, 2017.

 

Full Terms & Conditions >

image

Buy Intel Edison NowBuy Intel Edison Now

 

The IntelRegistered Edison is a Development Platform designed as a low-cost entry board for start-up product designers and pro-makers; with the Edison you can rapidly prototype and produce IoT and wearable computing products.

  • Sign in to reply
  • Cancel

Top Replies

  • sandeepdwivedi17
    sandeepdwivedi17 over 9 years ago +7
    Automated car parking assistance for difficult spaces according to following GIF
  • rsc
    rsc over 9 years ago +6
    I just finished adding insulation and weather seal to my greenhouse for extending the growing season through winter. I have some controls, sensors, and camera system installed, but they are not all connected…
  • jwatson
    jwatson over 9 years ago +5
    Congratulations to our 5 lucky Intel Giveaway winners! You've just won an Intel Edison Kit for Arduino to bring to life your ideas poised and post a blog about your project in the Intel space. Please direct…
  • joga95
    joga95 over 9 years ago

    i would build a distribuited IA system with intel edison to help peoples with disabilities to control their houses, computers, etc

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • isaacary
    isaacary over 9 years ago

    My idea is to connect a touch screen to the device then make a wall fitting for the device and connect it to the power in the house ( so it's actually flush in the wall ) I would like to then connect a few speakers into the ceiling in each room which is then Connected to the Edison and have the Edison boot and Spotify open immediately. That way I can have music throughout my house :).... (it would be handy to have toggles beside the device for each room to switch on and off speakers e.g. Kids are asleep in there rooms so music isn't heard in there room but is in the rest of the house

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jlangbridge
    jlangbridge over 9 years ago

    My idea doesn't count for this competition, I mean it has already been done and isn't the coolest idea ever, especially compared to some of the ideas I've read above, but oh well! My idea is simple, I'd write a tutorial series on the board, small projects to help get people up and running (similar to what I've done with mbed and the Silicon Labs BGM111 module). Good luck with the competition, everyone, and many thanks to Jane Watson for an awesome competition.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • satyavrat
    satyavrat over 9 years ago

    My idea for the Intel Edison is to use it as a Cognitive Server for IoT Sensor Networks.

     

    Data will remain just data unless it is used to come to a certain conclusion. Nowadays, with low-cost IoT sensor nodes generating huge amounts of data, we rely

    on off-site servers and corresponding cloud platforms for analytics. What if you could have a personal, dedicated computation device to make sense out of the data  being generated by the nodes which are of relevance only to you, say, your house?

     

    Enter the Intel Edison. I plan to leverage the Intel Edison's wealth of communication avenues and sheer computing horsepower to introduce the element of artificial intelligence to the conventional architecture of wireless sensor networks.

     

    With data generated from household devices, such as when a person switches on the lights or at what temperature does he switch off the fan, the Edison will learn the preferences of an individual and optimize the power usage of such resources by only switching them on when they are needed. It will also show the usage of said resources on a dedicated web server accessible via a browser like Chrome on devices on the same network.

     

    The procedure is fairly simple.

     

    1. Data is generated by household sensors, including when the resources are in use and when they aren't.
    2. This data is relayed to the Edison via BLE or WiFi (TCP stack)
    3. The received data is stored in an SQL table locally on the Edison
    4. A separate machine learning script, running continually on the Edison regularly queries the database and maps the temporal and sensor value dependency of these values (eg : At what time does the user switch on the lights? What is the ambient light value when he does?)
    5. Using this trend, the Edison trains itself to use the resources only when the values of environmental parameters are within the constraints.
    6. Using relays, it will control the resources as needed.
    7. The values of stored sensor data from all data sources as well as the state of the resources will be displayed on a web page hosted on the Edison.

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • diegoc
    diegoc over 9 years ago

    Hi, I'd like to prototype on it an hardware synthesizer, probably with touch interface

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • vishwasn
    vishwasn over 9 years ago

    An equipment to log the data of automobile(On Board Diagnostics ) and using that for user profiling to increase the experience of driving. Also the accident and drowsiness warning system.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mclaughlin7
    mclaughlin7 over 9 years ago

    i would build an intelligent reef aquarium controller with closed loop instrumentation.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • crsky
    crsky over 9 years ago

    I am interested to build a smart irigation system

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • kyawminnaing
    kyawminnaing over 9 years ago

    I want to create a autonomous drone with pixhawk 2 and intel board with object or human tracking and obstacles avoiding drone.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • nomade1999
    nomade1999 over 9 years ago

    Aren't you tired of having to manually select which phone connect to your handsfree system in your car due to lack of support by your manufacturer?

     

    Well, I would create a bluetooth "bridge" to address this issue.

     

    Basically, my Toyota Sienna 2013 has bluetooth support but it required you to manually select the device each time the driver change, this gets annoying and we keep forgetting..

     

    With this Intel Edison board I would create a small device that would listen on bluetooth after the car started and connect to the first (or prioritized) device found and bridge it to the car audio system.

     

    That way the car will always be connected to the Intel Edison board  and the board would then connect to a device, All traffic will then be passed on to the car audio system, no more need to manually select the device.

     

    And much more safety for everyone on the roads!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>