KEYSIGHT TECHNOLOGIES
  • Products & Partners
  • Manufacturers
  • KEYSIGHT TECHNOLOGIES
  • More
  • Cancel
KEYSIGHT TECHNOLOGIES
Forum 9v from modern ATX PSU for Ethernet Switch
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join KEYSIGHT TECHNOLOGIES to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 21 subscribers
  • Views 4614 views
  • Users 0 members are here
  • dc-dc
  • 12v
  • 9v
  • ethernet
  • psu
  • atx
  • switch
  • dc-to-dc_converter
Related

9v from modern ATX PSU for Ethernet Switch

ats1995
ats1995 over 11 years ago

Hi

 

Long time reader, first time poster. I've over time found it handy having a switch around since I often tinker with Raspberry Pis, among other things. Since most desktop computers have way more volume inside the case than needed, I think it would be ideal to permanently mount it inside (to avoid clutter etc.) and draw power from its PSU instead of having yet another wall adapter.

My switch has the id TL-SG108. The adapter is rated at 9v at 0.85A. Intuitively I think this should be easy, but after extensive googling (my knowledge on electricity is too limited to figure something out myself) I have yet to find a solution.

Any help and suggestions are appreciated!

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago in reply to ats1995 +1
    Hi Aslak, the LM 2596 does not come in a fixed 9 volt unit. You can get a variable version but then you will have to install external resistors to set the output voltage at 9 volts. Here is a schematic…
  • ats1995
    ats1995 over 11 years ago in reply to jw0752 +1
    I hope a late reply is a lot better than no reply: I ended up using a R-78B9.0-1.0. From the info I found it was very similar. It works without a problem. I measured the output voltage on the original…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Alask Tegle Sande,

    There are a couple of good reasons not to put the switch inside the cabinet. While there seems to be a lot of wasted room you will potentially hamper air flow and cooling of boards and parts. Most of the boards in the computer are exposed and if they touch or bump the outer case of the switch it might short out. You will also loose easy access to the ports of the switch and the LAN wires will need to be routed through the computer case. If space is a premium you might consider mounting the switch on the outside of the case.

     

    As far as drawing power from the ATX this is certainly possible with the appropriate DC to DC converter or regulator. For example in the power supply wiring of the computer (if it is standard) the Yellow wire will have + 12 volts and will be capable of sourcing power to the switch. The ground wire of the power supply is the black one. The next trick is we have to convert the +12 of the Yellow to Black wire voltage down to the 9 volts required for the Switch. We can use a small device like the Recom R-78C9.0-1.0 (Best Choice) or a linear regulator LM7809. I can draw up  the schematic of the circuit if you want to pursue this option. Since you say you lack experience you may want to think it over. You would have to test voltages, the first being the Yellow to Black power wire to verify that it is in fact 12 volts. Next you would have to build the little converter on a circuit board and use the wire from your wall wart to run the power to the switch. This would involve soldering and design so that connections are insulated and not allowed to short out. The connections to the black and yellow wires inside the computer would have to also be done properly and safely. The voltage of the wire to the switch would also have to be checked for proper 9 volts and for proper + / - polarity.  I do not know if this is a consideration but the switch would also turn on and off with the computer.

     

    Let me know if you want a schematic for the converter.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ats1995
    0 ats1995 over 11 years ago in reply to jw0752

    Thanks for super quick help John!

     

    I think I've thought the logistics of placing inside the cabinet pretty well, but I'll comment on it anyways:

    Airflow will not be a problem. My fans doesn't come close to max speed before keeping it cool enough even during heavy sessions. The switch is mounted on a solid rail quite far from the MoBo, so that's not a concern. Regarding accessing ports: It's placed flush against the back of the case. I've made a cutout for the ports, so this is neither a problem. From my understanding and experience (from an ancient PSU, shorting two pins (standby 5v and ground?) starts PSUs) the MoBo takes care of that.

     

    Sorry about my lack of accuracy: I'm not a total novice, but when it comes to currencies and voltages I find my knowledge surprisingly low (the physics classes had some theory on the subject). I'm familiar with the basics like polarity and measuring voltages. I'm also comfortable with a fair bit of soldering.

     

    I'm a bit tiny familiar with the LM7809. What would the benefits and differences be between a linear regulator and a switching one in this case? I notice that both of them requires a minimum of 12v. Voltages from computer PSUs are supposed to be quite accurate, but if not 100%, are there any tolerances on such components?

     

    The schematic shouldn't be necessary, but I would appreciate it! If you have a preferred or recommended place for buying components like this a recommendation would also be appreciated.

     

     

    Aslak

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ats1995
    0 ats1995 over 11 years ago in reply to jw0752

    Thanks for super quick help John!

     

    I think I've thought the logistics of placing inside the cabinet pretty well, but I'll comment on it anyways:

    Airflow will not be a problem. My fans doesn't come close to max speed before keeping it cool enough even during heavy sessions. The switch is mounted on a solid rail quite far from the MoBo, so that's not a concern. Regarding accessing ports: It's placed flush against the back of the case. I've made a cutout for the ports, so this is neither a problem. From my understanding and experience (from an ancient PSU, shorting two pins (standby 5v and ground?) starts PSUs) the MoBo takes care of that.

     

    Sorry about my lack of accuracy: I'm not a total novice, but when it comes to currencies and voltages I find my knowledge surprisingly low (the physics classes had some theory on the subject). I'm familiar with the basics like polarity and measuring voltages. I'm also comfortable with a fair bit of soldering.

     

    I'm a bit tiny familiar with the LM7809. What would the benefits and differences be between a linear regulator and a switching one in this case? I notice that both of them requires a minimum of 12v. Voltages from computer PSUs are supposed to be quite accurate, but if not 100%, are there any tolerances on such components?

     

    The schematic shouldn't be necessary, but I would appreciate it! If you have a preferred or recommended place for buying components like this a recommendation would also be appreciated.

     

     

    Aslak

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 11 years ago in reply to ats1995

    Hi Aslak,

    Sounds like you have the electronic experience to pull this off. The linear LM7809 will cost about a $1 but will have to be heat sunk. If we assume that your switch will consume 750 mA and there will be a three volt drop across the regulator it will need to dissipate about 2.25 Watts. The 12 volt power supply of the ATX will be fine for your application. If you decide to use the R-78C9.0-10 it will cost you about $9.00. I would normally tell you to get them from Newark but I see that they are out of stock right now. Check your parts suppliers to see who has one in stock. Since the R-78C is a DC / DC switching converter it will not need to be heat sunk. Be sure to follow the data sheet recommendations in either case for adding decoupling electrolytic capacitors on the input and output of the regulator/converter to maximize voltage stability. Most of the time you can find links to the data sheets on the sites of the Vendors like Newark. You probably don't need a schematic drawn by me but if you run into a bump let me know. I don't think I would mess with the on / off wire on the ATX. Turn it on and off with your normal computer switch. Hope this clarifies.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to ats1995

    Hi Aslak,

    Here is the schematic in case it will help clarify.

     

    image

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • ats1995
    0 ats1995 over 11 years ago in reply to jw0752

    Thanks a lot! Just one thing. What is the "c1" and c2"?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to ats1995

    These are the Decoupling capacitors for the different regulator/converters. For the 7809 C1 will be about 0.1 uF and C2 can be about 10uf. For the R-78C C1 should be about 22 uF and C2 can be 100 uF. The voltage ratings on the capacitors should be at least 25 volts DC. The data sheets for the part you decide to use may give slightly different recommendations. You probably can't go too wrong using their recommendations.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ats1995
    0 ats1995 over 11 years ago in reply to jw0752

    After a bunch of youtube videos (best one: https://www.youtube.com/watch?v=mk61DNz27FI ) and more, I think I have a good enough overview to make it, but I've stumbled upon cheaper switching regulators The R-78C was a bit difficult to find or get her in Norway. Is the LM2596 a viable option?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to ats1995

    Hi Aslak,

    the LM 2596 does not come in a fixed 9 volt unit. You can get a variable version but then you will have to install external resistors to set the output voltage at 9 volts.

     

    Here is a schematic for the LM 2596 that I got from the data sheet that shows how to calculate the value of the resistors.

     

    image

     

    Here is a link to the whole data sheet.

     

    http://www.ti.com/lit/ds/symlink/lm2596.pdf

     

    Because it comes prepackaged at 9 volts and doesn't need a lot of peripheral support I still think the Recom R-78C9.0-1.0 is the best. In lieu of the R-78 you might check ebay to see what is available in an inexpensive DC to DC adjustable converter. I do not know if you have access but I have purchased some good little converters from China for less than $5 US.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ats1995
    0 ats1995 over 11 years ago in reply to jw0752

    I hope a late reply is a lot better than no reply:

     

    I ended up using a R-78B9.0-1.0. From the info I found it was very similar. It works without a problem. I measured the output voltage on the original wall adapter. It was at about 9.5v! I guess that makes the R-78B9.0-1.0 overkill in terms of accuracy, but it's too late to change.

     

    A friend of mine is a lot more experienced in soldering, so after doing it myself with a standard DIY PCB. He recommended me to redo it with a stripboard (as shown in the picture. More pics at Switch in computer casemod - Album on Imgur ). I think it ended up perfectly. Measuring the output confirms that (reading 9.04v).

    imageimage

     

    Thanks a lot for the help! I learned a lot.

     

    Aslak

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to ats1995

    Hi Aslak,

    I really enjoyed the results that you posted and the pictures were great.

    John