• Products and Partners
    Products and Partners
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
Microchip
  • Products and Partners
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum Have a question? Ask our Microchip nanoWatt XLP expert!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 31 subscribers
  • Views 3200 views
  • Users 0 members are here
  • rishi_vasuki
  • low_power
  • security
  • microchip
  • xlp_mcus
  • smart_sensor
  • power_supplies
  • audio_expert
  • embedded
  • portable_music_player
  • extreme_low_power
  • motor_control
  • suny
Related

Have a question? Ask our Microchip nanoWatt XLP expert!

nlarson
nlarson over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Test & Measurement in the element14 Community Test & Measurement group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

 

RishiVasuki2.jpg

 

Rishi Vasuki

Rishi has been with Microchip Technology since 2001.  He has experience in developing portable music players and designing a wide variety of embedded applications (audio, security, motor control, power supplies and smart sensor).  His current focus includes PIC(R) XLP MCUs for eXtreme Low Power applications as well as Microchip's mTouch solutions using 8-bit PIC18 & 16-bit PIC24 MCUs.

  • Sign in to reply
  • Cancel
Parents
  • enrico.migchels
    enrico.migchels over 16 years ago

    Hi,

     

    I am considering a DSPic for a grid tied inverter. The inverter has a 400VDC input (input source solar DC/DC converter). Is the DSPic ever used for such an application? I know it has been used for AC induction motor control and AC/DC power supplies. My application will be a mix of both application. Grid Inverters have similar control loops (park - clark vector transformations) as motors and same circuits (full bridge) as power supplies. If anyone has information on the use of DSPic for these devices please share.

     

    Best regards,

     

    Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 16 years ago in reply to enrico.migchels

    Hi Enrico,

     

    There are 2 keys application targets in dsPIC30/33 families :

     

    * MOTOR control (references with "MC" at the end like DSPIC33FJ256MC710A-I/PF.DSPIC33FJ256MC710A-I/PF. : http://www.microchip.com/dscMOTOR

     

    * SMPS & energy conversion (references with "GS" at the end like  dsPIC33FJ64GS610 http://www.microchip.com/SMPS  . On this previous link you should find the information you're looking for.

     

    There are several applications notes showing implementation of Parke & Clarke transformation (Vector control).

    I recommend the use of dsPIC33 family which is more powerful (40MIPS) than dsPIC30 and especially some devices have on-chip DMA which reduces CPU load as peripheral read / write dual PORT RAM without CPU assistance.

     

    You may also want to ask precise questions on Microchip dsPIC dedicated forums : http://www.microchip.com/forums/tt.aspx?forumid=178

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • MicrochipRTCfr
    MicrochipRTCfr over 16 years ago in reply to enrico.migchels

    Hi Enrico,

     

    There are 2 keys application targets in dsPIC30/33 families :

     

    * MOTOR control (references with "MC" at the end like DSPIC33FJ256MC710A-I/PF.DSPIC33FJ256MC710A-I/PF. : http://www.microchip.com/dscMOTOR

     

    * SMPS & energy conversion (references with "GS" at the end like  dsPIC33FJ64GS610 http://www.microchip.com/SMPS  . On this previous link you should find the information you're looking for.

     

    There are several applications notes showing implementation of Parke & Clarke transformation (Vector control).

    I recommend the use of dsPIC33 family which is more powerful (40MIPS) than dsPIC30 and especially some devices have on-chip DMA which reduces CPU load as peripheral read / write dual PORT RAM without CPU assistance.

     

    You may also want to ask precise questions on Microchip dsPIC dedicated forums : http://www.microchip.com/forums/tt.aspx?forumid=178

     

    regards