• Products and Partners
    Products and Partners
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
Microchip
  • Products and Partners
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum 5v LCD on 3.3v board.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 28 subscribers
  • Views 880 views
  • Users 0 members are here
  • lcd
  • pic18f45k20
Related

5v LCD on 3.3v board.

JohnDSiviter
JohnDSiviter over 16 years ago
Ok I have ripped an old LCM-S01602DTR/M LCD off an old explorer board and now wish to put it on a Pickit demo board (18f45k20), however the LCD is 5V, whats the best Boost DC to DC regulator IC to use to step up from 3.3V?.
  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    John, do you already have a higher voltage supplying the Pickit?  Do you just need a 5V regulator, like a 7805 for the LCD.

     

    As far as interfacing, check the voltage level inputs for the LCDs to check if they'll work with 3.3V logic inputs.  Any signals from the LCD to the Pickit can be sorted with a resistor divider.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JohnDSiviter
    JohnDSiviter over 16 years ago in reply to e14 Contributor

    Hi Tony, I am aware of the 78xx range and I am not able to supply more than 3.3V, so will need to boost, to save the hassle I might just use a proper 3.3V LCD instead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • KennyMillar
    KennyMillar over 16 years ago in reply to JohnDSiviter

    How about one of these:

    http://uk.farnell.com/national-semiconductor/lm2623amm/dc-dc-converter-adj-powerwise/dp/8207445

     

    It's capable of doing 5v from a 3.3v source and is cheap, small an efficient.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JohnDSiviter
    JohnDSiviter over 16 years ago in reply to KennyMillar

    Thanks Again Kenny, you should work here in technical support!.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 16 years ago in reply to JohnDSiviter

    Hi,

     

    This 3V LCD  is currently used on EXPLORER16.

    It can be purchased here.

     

    regards