• Products and Partners
    Products and Partners
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
Microchip
  • Products and Partners
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum what is the difference between DM240001 and DM240002
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 27 subscribers
  • Views 884 views
  • Users 0 members are here
Related

what is the difference between DM240001 and DM240002

e14 Contributor
e14 Contributor over 15 years ago

i need to know the difference between DM240001 & DM240002.DM240002.

Does the DM240002.DM240002. support dspic as PIM or it  just for PIM PIC

 

if it does not support how i can use dspic with DM240002.DM240002.

 


  • Sign in to reply
  • Cancel
  • KennyMillar
    KennyMillar over 15 years ago

    The DM24001 is the 100 Pin Explorer 16 board and the DM24002 is the 44 Pin Explorer 16 board.

    The Explorer 16 100-pin features two interchangeable Plug-In Modules (PIMs), one each for the PIC24FJ128GA010 and the dsPIC33FJ256GP710 DSC. TheExplorer 16 44-pin features a Plug-In Module (PIM) for the PIC24FJ64GA004

     

    I hope this helps.

     

    More details here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to KennyMillar

    yes thanks

    but do i need to buy dsPIC33FJ256GP710 DSC or it comes with the board

     

    and does is it so hard if i buy the 44 pin and used an external dspic with it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • KennyMillar
    KennyMillar over 15 years ago in reply to e14 Contributor

    According to the page I linked to, the 100 Pin Explorer does come with the 2 pims, which are populated with the PIC Chips.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to KennyMillar

    Hi,

     

    All the descriptions of the various EXPLORER16 options are on this page : http://www.microchip.com/explorer16

    including all the optional processor modules (PIMs)

     

    regards