• Products and Partners
    Products and Partners
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
Microchip
  • Products and Partners
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum explorer 16 board and  AUDIO PICTAIL PLUS DAUGHTER BOARD
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 26 subscribers
  • Views 625 views
  • Users 0 members are here
  • pic32:microchip
Related

explorer 16 board and  AUDIO PICTAIL PLUS DAUGHTER BOARD

e14 Contributor
e14 Contributor over 15 years ago

how can i connect explorer 16 board to microphone or speaker

is there any method other than using the

 

AUDIO PICTAIL PLUS DAUGHTER BOARD

  • Sign in to reply
  • Cancel
Parents
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago

    Hi,

     

    As there is no specific HW for audio on the explorer16 board, the only alternative is to build your own audio on a pictail plus prototype board.

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to MicrochipRTCfr

    does the explorer 16 has A POWER supply to the entire board

    and if so can i use this power supply to the audio pictail or do i need an external power supply

    Direct 9 VDC power input that provides +3.3V and +5V (regulated) to the entire
    board

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to e14 Contributor

    Hi,

     

    There is a 9V power supply jack on explorer16 which goes into a couple of regulators which power the whole board. The Pictail plus connectors do get 5V and 3.3V from there regulators. As long as you don't exceed the current of these regulators for the whole board there is no issue.

    Actually Explorer16 can even power 2 pictail plus connectors (the second is optional and not soldered by default).

    The complete circuit of explorer16 can be seen in the User' manual of the borad which you can download here : http://www.microchip.com/explorer16

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to e14 Contributor

    Hi,

     

    There is a 9V power supply jack on explorer16 which goes into a couple of regulators which power the whole board. The Pictail plus connectors do get 5V and 3.3V from there regulators. As long as you don't exceed the current of these regulators for the whole board there is no issue.

    Actually Explorer16 can even power 2 pictail plus connectors (the second is optional and not soldered by default).

    The complete circuit of explorer16 can be seen in the User' manual of the borad which you can download here : http://www.microchip.com/explorer16

     

    regards