Moto Mods
  • Products & Partners
  • Manufacturers
  • Moto Mods
  • More
  • Cancel
Moto Mods
Forum Solar power source
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Moto Mods to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 57 subscribers
  • Views 779 views
  • Users 0 members are here
Related

Solar power source

pacobell
pacobell over 9 years ago

According to the Power Transfer Protocol documentation ( https://developer.motorola.com/explore/firmware/power-transfer  ), there are four defined power sources as enumerated by ptp_power_source: PTP_POWER_SOURCE_NONE, PTP_POWER_SOURCE_BATTERY, PTP_POWER_SOURCE_WIRED, and PTP_POWER_SOURCE_WIRELESS. Which one would a solar power mod fall under? I can understand that if the mod contained a battery in conjunction with the PV panel, it would probably be classified as just PTP_POWER_SOURCE_BATTERY. But what if it doesn't contain a battery? Would it be PTP_POWER_SOURCE_WIRED or PTP_POWER_SOURCE_WIRELESS? And what are the min/max electrical specifications for each power source?

  • Sign in to reply
  • Cancel

Top Replies

  • kingstu
    kingstu over 9 years ago +1
    I would guess that solar panels connected directly wouldn't generate enough power to be considered a power source for the moto z.
  • pacobell
    pacobell over 9 years ago in reply to kingstu +1
    I dunno about that. Some thin-film PV can generate up to 0.226W per 17x50mm cell. If you create a nine 5sx1p folding panel of these cells, you can get a 10W panel easily into a standard smartphone form…
Parents
  • kingstu
    0 kingstu over 9 years ago

    I would guess that solar panels connected directly wouldn't generate enough power to be considered a power source for the moto z.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pacobell
    0 pacobell over 9 years ago in reply to kingstu

    I dunno about that. Some thin-film PV can generate up to 0.226W per 17x50mm cell. If you create a nine 5sx1p folding panel of these cells, you can get a 10W panel easily into a standard smartphone form-factor. That's a compelling use-case.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • pacobell
    0 pacobell over 9 years ago in reply to kingstu

    I dunno about that. Some thin-film PV can generate up to 0.226W per 17x50mm cell. If you create a nine 5sx1p folding panel of these cells, you can get a 10W panel easily into a standard smartphone form-factor. That's a compelling use-case.