Moto Mods
  • Products & Partners
  • Manufacturers
  • Moto Mods
  • More
  • Cancel
Moto Mods
Forum Is it possible (project ideas)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Moto Mods to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 56 subscribers
  • Views 842 views
  • Users 0 members are here
Related

Is it possible (project ideas)

antp
antp over 9 years ago

If this all works I'd like to buy a z2 force to start this on or if there's anything like this out use it.

 

Would it be possible to dual boot moto z to run linux or linux arm or raspbian and have the phone act like a raspberry pi/sbc with the phone screen as a "monitor".

 

Also would it be possible to use the mod to take hdmi input and use phone screen as a monitor maybe also use as a capture card unsure if data flow allows signal to run to phone but the hdmi could maybe come in though the camera input and use a hdmi to 15pin camera ribbon and display on screen acting as a "camera mod" which would maybe allow a live view for monitor and recording like a camera would video.

 

If the hdmi input would work the you could have a raspberry pi or udoo x86 connected to it and have a extra battery to power it and also have the battery connect to the phone so it would all charger from phone port also maybe take touch input from screen?? like adafruit screens but higher definition so basically a mobile laptop converter mod thing or just a monitor and or capture card.

 

Is it also possible to add ram to the phone through a moto mod or use external cpu or gpu.

  • Sign in to reply
  • Cancel
Parents
  • kingstu
    0 kingstu over 9 years ago

    The Moto Mods System Architecture can give you a better idea about what is possible. https://developer.motorola.com/explore/system-architecture  Lots of ideas have come from participants of the Transform the Smartphone Challenge https://www.indiegogo.com/campaign_collections/transform-the-smartphone-challenge I am sure some of the ideas you have are possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • kingstu
    0 kingstu over 9 years ago

    The Moto Mods System Architecture can give you a better idea about what is possible. https://developer.motorola.com/explore/system-architecture  Lots of ideas have come from participants of the Transform the Smartphone Challenge https://www.indiegogo.com/campaign_collections/transform-the-smartphone-challenge I am sure some of the ideas you have are possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer