Moto Mods
  • Products & Partners
  • Manufacturers
  • Moto Mods
  • More
  • Cancel
Moto Mods
Forum USB3 powering device, but not enumeration
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Moto Mods to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 59 subscribers
  • Views 2544 views
  • Users 0 members are here
Related

USB3 powering device, but not enumeration

garengllc
garengllc over 9 years ago

I have an Ettus USRP (B205mini) that I can get to work fine with the usb2 project.  When I switches projects to compute (to take advantage of the USRP's USB3 capabilities), I cannot seem to get it to work.

 

When I plug the USRP into the middle USB port on the MotoMod, it powers it up, but I don't see the standard Android pop-up that a USB device was detected (which it does when I use the USBC port on the bottom of the phone).  I started adding debug statements into the fusb302.c file and can see the MotoMod recognizing a device being plugged in. 

 

I believe the issue is that in the decode_cc_termination function, it checks if (fusb302_regs.status0 & FUSB302_STATUS0_VBUSOK_MASK) (which is VBUS Valid), and it is coming up 0.  According to the FUSB302 datasheet, that bit it is checking is bit 7 of the status0 register and it describes it as going high (and interrupt occuring) when VBUS transitions through vVBUSthr. It also says that that bit typically is used to recognize port partner during startup.

 

So any idea what is going on here?  Any idea of further debug that I could try?

  • Sign in to reply
  • Cancel
Parents
  • garengllc
    garengllc over 9 years ago

    BTW, when the check gets done on status0 above, it has a value of 1 supposedly.  According to the datasheet (https://www.fairchildsemi.com/datasheets/FU/FUSB302B.pdf ), that means (among other things) that the device is drawing >200mA and <660mA.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dpwinkler
    dpwinkler over 9 years ago in reply to garengllc

    Hi Jason,

     

    Did you verify your A1 and A2 dip switch is set to "On, On" to enable USB3.1 support? Also, you may want to verify you are using a USB OTG(on the go) cable plugged into the MDK to ensure the device is properly recognized as a USB slave.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • garengllc
    garengllc over 9 years ago in reply to dpwinkler

    Sadly, i quadruple checked thise things!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dpwinkler
    dpwinkler over 9 years ago in reply to garengllc

    Have you been able to enumerate any other devices? I've had USB flash drives be recognized via the MDK using compute firmware in the past. I'm wondering if there is something specific to the device you are trying to connect which is causing an issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • garengllc
    garengllc over 9 years ago in reply to dpwinkler

    Funny you should say that, that was this morning mission.  Unfortunately, I haven't been able to find something here at work that is USB3 (besides other power hungry SDRs).  I was hoping to come up with a thumbdrive (or something simple like that), so I could prove to myself that the firmware is indeed OK.

     

    I also was on the hunt for a powered USB3 hub to rule out power supply issues to the device, but came up empty there as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • garengllc
    garengllc over 9 years ago in reply to garengllc

    A little more info on what my debugging has turned up.  It sees my device get plugged in and reports a togss of 0x02 which means toggle functionality has "settled on SRCon CC2", VBUSOK ==1 which means that a port partner was recognized (this was not working earlier but is now), and comp == 0 which means that the measured CC* input is lower than than reference level driven by MDAC.

     

    All that boils down to the MotoMod detecting USB ISR trigger for a USB 3.1 device on CC2B (and if I flip the USBC connector around that changes like it is supposed to).  I end up getting a "src -> src" in the fusb302_update_state function (meaning that when in the USB_STATE_ATTACHED_SRC state, we have a ATTACH_TYPE_SRC new attachment). 

     

    I can't for the life of me figure out where this is going wrong though. 

     

    Has anyone connected a USB3 device to the compute firmware for something more complicated than a thumbdrive (and I mean a direct-connect, not through a powered USB hub)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • garengllc
    garengllc over 9 years ago in reply to garengllc

    A little more info on what my debugging has turned up.  It sees my device get plugged in and reports a togss of 0x02 which means toggle functionality has "settled on SRCon CC2", VBUSOK ==1 which means that a port partner was recognized (this was not working earlier but is now), and comp == 0 which means that the measured CC* input is lower than than reference level driven by MDAC.

     

    All that boils down to the MotoMod detecting USB ISR trigger for a USB 3.1 device on CC2B (and if I flip the USBC connector around that changes like it is supposed to).  I end up getting a "src -> src" in the fusb302_update_state function (meaning that when in the USB_STATE_ATTACHED_SRC state, we have a ATTACH_TYPE_SRC new attachment). 

     

    I can't for the life of me figure out where this is going wrong though. 

     

    Has anyone connected a USB3 device to the compute firmware for something more complicated than a thumbdrive (and I mean a direct-connect, not through a powered USB hub)?