Moto Mods
  • Products & Partners
  • Manufacturers
  • Moto Mods
  • More
  • Cancel
Moto Mods
Forum FM Transmitter Mod
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Moto Mods to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 58 subscribers
  • Views 4946 views
  • Users 0 members are here
  • rapsberry-pi
  • audio
  • fm radio
  • gpio
  • moto mod
  • raspberry pi io
  • pifm
  • moto mdk
  • moto mods
  • raspberrypi_pifm_pitx_pisoftware
Related

FM Transmitter Mod

krobar14
krobar14 over 8 years ago

Hello,

 

I am currently undertaking a project on my own. To develop a mod for my Moto Z Play.

 

Just to give you some background into this. I tried implementing the PiFM GPIO project with the band pass filter feature recently on a raspberry pi. I expreienced great success with this endeavor, and thought that I would be able to do something similar for my Moto Z Play. I currently have all of the development tools, and the hardware, but I am just doing research, having implemented the Blinky Project already.

 

I am currently reading through some of the Nuttx instructions, and purposes. The information given seems to show that the firmware contains the possibility for Audio signals being processed.

 

What advice would you have for an Engineering student getting into this. I would like to have some input at where I should go from the Blinky project. I want to have a mod that takes my phone's audio, and sends it out over different FM frequencies. Is this even possible?

 

Thanks!

David

  • Sign in to reply
  • Cancel

Top Replies

  • motomodsdev
    motomodsdev over 8 years ago +1
    Very possible, I recommend starting with the Audio Personality Card example. This uses i2s to transfer digital audio from the Moto Z, and plays out a tiny mono speaker. It should be extremely easy to rip…
  • motomodsdev
    motomodsdev over 8 years ago in reply to krobar14 +1
    The MDK does generate clock and PWM outputs, so it appears it would be feasible to use the MuC in the same manner that they used the Pi. In this case the audio would be an analog signal out of the TFA…
  • motomodsdev
    motomodsdev over 8 years ago in reply to krobar14 +1
    Sorry for missing this update, I guess the TFA9890 is mono audio only, which the reason for the i2s stereo decoder. Did you look to see if there was anything in the TFA family that might make your firmware…
Parents
  • krobar14
    krobar14 over 8 years ago

    Will do. Thanks for your help. I'll post updates on this thread.

     

    Would another possibility be, building a GPIO board that would connect to the mod, and send out audio, the same way I did on the raspberry pi?

    I'm more specifically referring to the PiFM Project on the raspberry pi.

     

    David

    Raspberry Pi Radio Transmitter: 4 Steps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • motomodsdev
    motomodsdev over 8 years ago in reply to krobar14

    The MDK does generate clock and PWM outputs, so it appears it would be feasible to use the MuC in the same manner that they used the Pi.  In this case the audio would be an analog signal out of the TFA still, correct?  You would probably need to flywire a new circuit on the Perforated board, since the Audio card doesn't provide easy access to extra GPIO.

     

    If you run into issue configuring any MuC outputs, we're here to help.  As for how the user tunes the transmitter, than can be easily done with an Android app and pass the information to your Moto Mod using the Raw protocol.

     

    There's an interesting comment that this isn't really a good way to do FM since you "splash" out over other channels.  I thought your FM transmitter was a separate chip, controlled by i2c like the TFA is.  Pretty interesting just modulating a GPIO signal; not sure if that is easier or harder than a transmitter IC.

     

    Great documentation so far, really interesting to see this evolving!  But you confused me when you mentioned 2 knobs next to the speaker.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • krobar14
    krobar14 over 8 years ago in reply to motomodsdev

    So sorry for the confusion. The knobs are actually pins that push inward on the spk_out plates. If you have a spare Audio Personality card at home, take off all the screws, and lift the lid. You'll notice that the speaker is attached to the lid, and there are two little pins that press down on the spark plugs. Those are the "Knobs" I was talking about. What I was think about doing was using a Audio Amplifier, and a FM Transmitter both from adafruit.

    I've posted links to both below. Does this look like something that would be feasible?

     

    image

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • krobar14
    krobar14 over 8 years ago in reply to motomodsdev

    So sorry for the confusion. The knobs are actually pins that push inward on the spk_out plates. If you have a spare Audio Personality card at home, take off all the screws, and lift the lid. You'll notice that the speaker is attached to the lid, and there are two little pins that press down on the spark plugs. Those are the "Knobs" I was talking about. What I was think about doing was using a Audio Amplifier, and a FM Transmitter both from adafruit.

    I've posted links to both below. Does this look like something that would be feasible?

     

    image

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • krobar14
    krobar14 over 8 years ago in reply to krobar14

    https://www.adafruit.com/product/1958

    https://www.adafruit.com/product/987

     

    The main components I will use on my perforated board.

     

    David