NI
  • Products & Partners
  • Manufacturers
  • NI
  • More
  • Cancel
NI
Blog How to Turn a Button On with Python and mioDAQ
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NI to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: timifolayan
  • Date Created: 27 Jul 2026 7:53 PM Date Created
  • Views 962 views
  • Likes 7 likes
  • Comments 0 comments
Related
Recommended

How to Turn a Button On with Python and mioDAQ

timifolayan
timifolayan
27 Jul 2026

Hello, my name is Timi Folayan and I am a SDE intern here at NI. I've noticed most of the community's DAQ content assumes you're using LabVIEW, which makes sense - it's the flagship tool. But I come from a software engineering background, and I wanted to see how far I could get controlling a mioDAQ using nothing but Python and the official nidaqmx-python API.

This is the first post in a short series where I'll build up complexity one step at a time: this post just turns an LED on, the next will read a button press, and eventually I'll combine input and output into something interactive. Starting simple on purpose - if you're newer to hardware, this is meant to be a post you can follow along with on your own bench.

What you'll need

  • NI mioDAQ
  • Breadboard
  • 1x illuminated pushbutton (red)
  • 1x 10k Ω resistor
  • Jumper wires
  • Python 3.8+ with nidaqmx installed (pip install nidaqmx) and the NI-DAQmx driver installed

*A note on scope*

This post only turns the pushbutton's built-in LED on - it doesn't read the button press yet. I'm keeping input and output separate for now so each post in the series stays focused on one concept at a time.

Wiring it up

image

The LED lead from the pushbutton connects to P0.0 through a 10kΩ current-limiting resistor. The other LED lead ties into the mioDAQ's DGND. That's it for this post - the switch contacts on the pushbutton aren't wired yet.

image

image

Two ways to write to an mioDAQ: analog vs. digital

The nidaqmx-python examples repo includes both analog and digital output patterns. Since a pushbutton LED is a simple on/off device, digital output is the right fit here — but it's worth seeing the analog version too, since it's the same basic task/channel pattern applied to a continuous voltage instead of a binary line.

image

Analog output writes a specific voltage value (here, 10.0 V) to an analog channel - useful for things like driving a motor speed or simulating a sensor signal, where you need more than just on/off.

The digital output code (what I'm actually using)
image


Demo Video: 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


Reference

The examples I started from are in the official nidaqmx-python repo: github.com/ni/nidaqmx-python - worth a look if you want to see the full range of what the API covers beyond digital and analog output.

Up next

Post 2 in this series will read the pushbutton's actual switch state as a digital input - the first step toward making this interactive instead of just scripted.