Panasonic
  • Products & Partners
  • Manufacturers
  • Panasonic
  • More
  • Cancel
Panasonic
Forum HAVE A QUESTION ON CAPACITORS,ASK AN EXPERT!
  • Blog
  • Forum
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Panasonic to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 48 replies
  • Subscribers 32 subscribers
  • Views 8432 views
  • Users 0 members are here
  • capacitor
  • expert
  • panasonic
Related

HAVE A QUESTION ON CAPACITORS,ASK AN EXPERT!

Resistor+caps
Resistor+caps over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Passive in the element14 Community Passive group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


 

 


  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Greetings Mr. Setsuda

     

    I just replaced the capacitors in my Lincoln SP250 wire feed welder after they went off like volcanoes inside my machine while I was working on a project. While I was welding, I could hear them venting and stopped in the middle of my weld to witness this hideous cloud of white smoke fuming from my machine. I think I incorrectly made the assumption that since my machine was still working when this happened and the screw connections on the old capacitors exhibited signs of arching, I could get away with just replacing them. I was able to find replacements with similar specs from Newark except the new caps were physically smaller.

     

    Old:

    MEPCO/CENTRALABS

    S13490-120

    3120 EG303U050AMA5

    30000 UF -10 + 75%

    50 VDC 75 SURGE

    85 C MAX AMBIENT

    362 9016 56699

    2.0 OD X 5.12 LG

     

    New:

    UNITED CHEMI-CON

    E32D500HPN333MAB7ME32D500HPN333MAB7M

    33000 UF +-20%

    50V

    105 C MAX AMBIENT

    1.38 OD X 4.60 LG

     

    After I put the new caps in the machine, I went to tack a couple of pieces of metal togeter and noticed the output of the welder was much lower than it should have been for the machine setting. After the third tack, one of the new caps vented and I shut the machine off.

     

    Being that I'm just a mechanical designer, my electrical skills are pretty weak (obviously) and I'd like to get some advice from someone with more experience. I'm wondering if there are any components in the circuit I should test (rectifier/diodes, transformer, block, etc.) that could be the source of the trouble or did I just completely miss the mark on using these caps as a replacement. Any help would be greatly appreciated.

     

    Dave Buckalew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Hello Dave san

     

    Thank you for your question,

    But Unfortunately I can not find out MEPCO web and MEPCO Capacitor SPEC in Web site.

    It seems that MEPCO SPEC and UNITED CHEMI-CON SPEC is not same.

     

    MEPCO

    30000 UF -10 + 75%

    50 VDC 75 SURGE

    Maximum ESR (mΩ) at 25deg,120Hz

    UNITED CHEMI-CON

    33000 UF +-20%

    50V

    Maximum ESR (mΩ) at 25deg,120Hz

    12.5

    Rated Ripple Current (A rms) at 85deg,120Hz

    17.22

     

    In case of such kind of big capacitance and big current capacitor

    You should use completely same SPEC capacitor as MEPCO.

    Unfortunately

    Panasonic does not have screw type capacitor.

     

    Thank you for your understanding.

     

    Thanks

    Setsuda

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Thanks for taking the time to respond to my question so quickly. It looks like I still have some more work to do.

     

    -Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Dear Mr Setsuda

     

    Pulse discarge capacitor

     

    I have an application where I need to charge a large capacitor to 96V and then discarge it across a low resistance soleniod, this will not happen very often.

    I am thinking of using a Panasonic capacitor EETUQ2C272EA (2700uF, 160V).

    Is there a different capacitor that would be more suitable for this kind of pulse discharge application?

    Kind regards

    Nico Rotolo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MAKeller
    MAKeller over 16 years ago

    Hiroshi,

     

    I am looking for a way to measure some fuel quantity probes.

    This would an AC capacitance measurement of 30 pF, with a tolerance of +/- .3 pF and resolution of .05 pF.

     

    Do you have any recommendations on a LCR to make this measurement in a manufacturing enviroment.

     

    Thank you,

     

    MA.Keller

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Resistor+caps
    Resistor+caps over 16 years ago in reply to e14 Contributor

    Hi Nico

     

    Thank you for your mail, Snap in capacitors are generally the best solution  for charge/discharge application and the question might be, which capacitance, Ripple, etc. you require?

     

    Kind regards

     

    Setsuda

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to Resistor+caps

    Hi Nico san

     

    I am waiting for your detail information.

     

    Thanks

    Setsuda

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to MAKeller

    Hello Keller san

     

    Unfortunately

    Panasonic capacitor does not have MLCC now due to business transfer to Another company.

    So we do not have such kind of pF capacitor products as of today.

    I will try to chase former My MLCC engineer.

    Give me more time.

     

    Sorry for inconvinient.

     

    Thanks

    Setsuda

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Hello Setsuda

    Sorry for my delay in replying.

    I have a very simple application and I would like some advice on what type of capacitor to use.

    My application needs a 2700uF capacitor that is charged to 96V. Once charged, the capacitor is discharged (using a fast thyristor) into a very low resistance (almost a short circuit).

    This 'firing' of the capacitor will only happen occasionally.

    I understand that some types of capacitors have a very short lifetime if they are used in this way, is an electrolytic capacitor suitable for this application?.

    Regards

    Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi Mr. Setsuda,

     

    I am designing a power supply circuit which will use supercapacitors for backup.

     

    I was wondering if supercapacitors have discharge current ratings? This pdf below (on bottom of page 3) seem to imply that there are limits on operating currents for supercaps, but there was nothing on the product page or data sheet itself regarding current.

     

    Also, I am thinking of using a supercapacitor charger in the circuit. Is it safe to set up the charge voltage limit at exactly the maximum voltage rating of the supercap, or is it a bad idea? For example, setting maximum voltage limit to 2.5V on 2.5V supercaps. Will they blow / degrade quickly if they are cycled to maximum capacity regularly?

     

    Thank you,

     

     

    Irving

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>