Panasonic
  • Products & Partners
  • Manufacturers
  • Panasonic
  • More
  • Cancel
Panasonic
Forum Panasonic Capacitor 1000uf, 200V, failure concern
  • Blog
  • Forum
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Panasonic to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 28 subscribers
  • Views 2624 views
  • Users 0 members are here
Related

Panasonic Capacitor 1000uf, 200V, failure concern

e14 Contributor
e14 Contributor over 15 years ago

Hi,

 

I am at a manufacturer that has experienced failures on the rectifier board with the capacitor venting or bulging.  There are three issues.  Is the issue a likely failure, Is this  real or fake panasonic part,  have other failures been reported ?

1.  We found the damaged part is a 1000 uf, 200 volt, capacitor part EETED2D102CAEETED2D102CA with a date code of 0921 (M).  Our analysis was that the capacitor has corrosion on the leads which causes the capacitor to fail then the imbalanced capacitors on the rectifier board causes a voltage spike that ruins the electronics.  Is it possible or a likely root cause to have corrosion on a lead ?

 

2.  I attached a photo.  Is the 0921 (M) code a real panasonic part date code and if so what does it mean.  We are finding other panasonic 1000uf, 200V capacitors that are slightly different in height and diameter and plastic cover print font.

 

3.  Are there any other field reports of problems on this capacitor.

 

Thanks

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hello Thomas 123 san

     

    This is Setsuda,

    Panasonic Industrial Europe located in Muenchen Germany.

    I am Capacior Guy.

    1) Could you send your picture which shows corrosion on a lead?

    2)Lot# 0921M means 2010 Sep/21st or 2000 Sep/21st.

       But This product Lot# should be 2010 Sep/21st.

     

       Please let me know below.

       1)When you bought this capacitor?

       2)From Which Disty you bought this capacitor? Farnell or other Disty?

       3)What is your mesurement of this capacotor?

          Give me Diameter length and Hight length

          EEEED2D102CA should be Diameter 25mm x Height 45mm.

     

    3) As of now I do not have information of problem about this capacitor.

     

    Thanks

    Setsuda

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ahaustin77
    ahaustin77 over 9 years ago in reply to e14 Contributor

    Hello Hiroshi,

     

    I have these Panasonic capacitors that have been bulging from the top. Could you help tell me if these are counterfeit or legitimate Panasonic capacitors? Any help would be great. Thanks.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ahaustin77
    ahaustin77 over 9 years ago in reply to e14 Contributor

    Hello Hiroshi,

     

    I have these Panasonic capacitors that have been bulging from the top. Could you help tell me if these are counterfeit or legitimate Panasonic capacitors? Any help would be great. Thanks.image