STMicroelectronics
  • Products & Partners
  • Manufacturers
  • STMicroelectronics
  • More
  • Cancel
STMicroelectronics
Forum How to get STM32F105 into DFU mode?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STMicroelectronics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 28 subscribers
  • Views 1481 views
  • Users 0 members are here
  • stm32f105xx
  • st products
  • dfu
Related

How to get STM32F105 into DFU mode?

e14 Contributor
e14 Contributor over 10 years ago

Hi!

 

I got a custom board and having problem to get F105RCT6 MCU into DFU mode when connected to USB-cable and PC. Is there anyone the have some suggestions that can help me?

 

I also tried to get connected using USB to TTL with no success. Then I tried PA9/PA10 for USART1_TX and USART1_RX..

 

All help is appriciated

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to gadget.iom +1
    Hi Paul! Thanks for the reply. No, I have not tested PA9. I will give this a try and is hopeful. I have a question regarding if Nreset pin 7 always should be connected to Vdd? On my custom board this is…
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    Have you tried connecting PA9/OTG_FS_VBUS to +3.3V?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to gadget.iom

    Hi Paul!

     

    Thanks for the reply. No, I have not tested PA9. I will give this a try and is hopeful.

     

    I have a question regarding if Nreset pin 7 always should be connected to Vdd? On my custom board this is the case and I wonder if this can cause the problem due to I cannot physically do a reset with a switch as it is right now. But I can do a modification if needed to cut the line for Nreset so this is not connected to Vdd if this could help. Hope you can understand my description.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to gadget.iom

    Hi Paul!

     

    Thanks for the reply. No, I have not tested PA9. I will give this a try and is hopeful.

     

    I have a question regarding if Nreset pin 7 always should be connected to Vdd? On my custom board this is the case and I wonder if this can cause the problem due to I cannot physically do a reset with a switch as it is right now. But I can do a modification if needed to cut the line for Nreset so this is not connected to Vdd if this could help. Hope you can understand my description.