STMicroelectronics
  • Products & Partners
  • Manufacturers
  • STMicroelectronics
  • More
  • Cancel
STMicroelectronics
Forum How to get STM32F105 into DFU mode?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STMicroelectronics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 28 subscribers
  • Views 1481 views
  • Users 0 members are here
  • stm32f105xx
  • st products
  • dfu
Related

How to get STM32F105 into DFU mode?

e14 Contributor
e14 Contributor over 10 years ago

Hi!

 

I got a custom board and having problem to get F105RCT6 MCU into DFU mode when connected to USB-cable and PC. Is there anyone the have some suggestions that can help me?

 

I also tried to get connected using USB to TTL with no success. Then I tried PA9/PA10 for USART1_TX and USART1_RX..

 

All help is appriciated

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to gadget.iom +1
    Hi Paul! Thanks for the reply. No, I have not tested PA9. I will give this a try and is hopeful. I have a question regarding if Nreset pin 7 always should be connected to Vdd? On my custom board this is…
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    Have you tried connecting PA9/OTG_FS_VBUS to +3.3V?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 10 years ago

    Have you tried connecting PA9/OTG_FS_VBUS to +3.3V?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to gadget.iom

    Hi Paul!

     

    Thanks for the reply. No, I have not tested PA9. I will give this a try and is hopeful.

     

    I have a question regarding if Nreset pin 7 always should be connected to Vdd? On my custom board this is the case and I wonder if this can cause the problem due to I cannot physically do a reset with a switch as it is right now. But I can do a modification if needed to cut the line for Nreset so this is not connected to Vdd if this could help. Hope you can understand my description.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to gadget.iom

    I read in AN2606 regarding DFU.

    https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Attachments/18225/AN2606.pdf

     

    Your correct, PA9 should have +5V.

     

    However there is one statement that I dont understand on p14 of 55:

    USART1_RX (PA10), USART2_RX (PD6) and CAN2_RX (PB5) pins must be kept at a high or low level during the detection phase

     

    I dont have PD6 on my 64 pin F105RCT6 MCU.

     

    Does this mean that USB DFU does not work or what do you think?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    Maybe this can help http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4370.pdf . But this explains more https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32F%20MEMS%20%20iNEMO/Flat.aspx?RootFolder=https%3a%2f%2fmy%2est%…

    Clem