TT Electronics
  • Products & Partners
  • Manufacturers
  • TT Electronics
  • More
  • Cancel
TT Electronics
Blog Adaptable Optical Sensors vs. Fixed Legacy Systems: A Guide for Industrial Engineers
  • Blog
  • Forum
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join TT Electronics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: william.walsh
  • Date Created: 30 Apr 2026 7:42 PM Date Created
  • Views 951 views
  • Likes 4 likes
  • Comments 2 comments
  • industrial
  • sensors
  • tt electronics
  • sensors_group
  • automation
Related
Recommended

Adaptable Optical Sensors vs. Fixed Legacy Systems: A Guide for Industrial Engineers

william.walsh
william.walsh
30 Apr 2026

In the landscape of industrial automation, the debate between maintaining fixed legacy systems and migrating to adaptable optical sensors is not just about technology; it is about operational philosophy. For decades, fixed optical systems—standard logic photocells, basic LED emitters, and fixed-gain optoisolators—have been the backbone of manufacturing. They are reliable, understood, and inexpensive.

However, the shift toward Industry 4.0 has exposed the limitations of these rigid systems. Engineers are now tasked with integrating components that can self-calibrate, communicate status, and adapt to environmental degradation. This article provides a transparent comparison between fixed legacy systems and modern adaptable optical sensors, covering Fibre Optics, Optoisolators, Photologic assemblies, and VCSEL technologies.

The Core Definition: Fixed vs. Adaptable

Fixed Legacy Systems

A fixed system operates on binary logic or set parameters defined at the hardware level. Once installed, its behaviour is static. For example, a standard infrared emitter paired with a phototransistor will trigger a signal when a light beam is broken. If dust accumulates on the lens, the signal degrades until the system fails. To fix it, a technician must physically clean the sensor or adjust a potentiometer.

Adaptable Optical Sensors

Adaptable sensors utilise intelligent circuitry and superior materials (like VCSELs) to adjust to their environment. A programmable Photologic sensor, for instance, might dynamically adjust its hysteresis threshold to account for signal drift caused by temperature changes or debris. These systems prioritise data continuity and predictive maintenance over simple binary switching.

The Argument for Fixed Legacy Systems

We must acknowledge why legacy systems remain prevalent. They are not without merit.

Lower Upfront BOM Cost – A standard fixed-gain optoisolator or a simple LED-based interrupter is significantly cheaper than a programmable alternative.

Simplicity of Replacement – If a fixed sensor fails, you pull it out and plug in an identical part. There is no firmware to update and no calibration software to run.

Zero Latency – Purely analogue fixed systems often have faster response times than smart sensors that require processing cycles to interpret data.

Technology Comparison: Fixed vs. Adaptable Optical Sensors

1. VCSEL vs. Standard LED Emitters

Legacy systems rely on standard LEDs. While functional, they suffer from beam divergence and lower power efficiency. Adaptable systems utilise Vertical-Cavity Surface-Emitting Lasers (VCSELs). VCSELs offer a narrow, coherent beam that requires less power and provides higher accuracy for position sensing. In adaptable systems, the VCSEL current can be modulated dynamically to maintain constant output power as the component ages.

2. Photologic® vs. Discrete Components

A fixed system usually employs a discrete photodiode and a separate amplifier circuit. Adaptable Photologic sensors integrate the sensor, amplifier, and logic gate into a single package. The benefit is not just space; it is consistency. These adaptable units often feature internal voltage regulation and temperature compensation that fixed discrete circuits lack.

3. Flexible Fibre Optics vs. Hardwired Connections

In high-EMI environments, copper is a liability. While legacy systems try to shield copper, adaptable systems switch to fibre optics. Modern industrial fibre optic links are adaptable because they provide complete electrical isolation and can be routed through hazardous areas where electrical sparks are prohibited. They are immune to the electromagnetic interference that plagues fixed copper legacy systems.

Decision Matrix: When to Switch to Adaptable Optical Sensors?

Engineers should consider migrating to adaptable sensors if:

  • Environmental variation is high – Varying light levels, dust, or temperature swings require sensors that can auto-calibrate.

  • Downtime is expensive – If stopping a line to wipe a sensor lens costs thousands of pounds, an adaptable sensor that compensates for occlusion is worth the investment.

  • Precision is critical – If you are moving from simple object detection to precise position sensing, VCSEL-based adaptable systems are required.

Conclusion

Fixed legacy systems are not obsolete, but they are becoming niche. For simple, cost-constrained applications where downtime is manageable, they remain a valid choice. However, for industrial engineers building systems for longevity, reliability, and Industry 4.0 integration, adaptable optical sensors offer a superior return on investment despite the higher upfront cost. By eliminating manual calibration and reducing failure points related to environmental stress, adaptable sensors future-proof manufacturing lines.

Written by TT Electronics

  • Sign in to reply
  • geralds
    geralds 6 months ago

    Hi  william.walsh 

    I agree with the arguments you've explained here.

    The biggest problem I've had in over 50 years of working in electronics was programming the appropriate algorithms and transmission protocols.

    Electronic hardware and materials physics were less of a problem for me; I'm a "walking encyclopedia" of data.
    I remember physical properties more easily than source codes.

    Well, on top of that, other people are programming too, and then you eventually run into trouble because
    someone suddenly says, "You can't do that without certifications. Have you a license for this? Are you even qualified? Are you... etc ..."

    THAT'S the real problem: instead of all of us working together, there's fierce competition against you.

    Well, and now... now I'm retired (physically, but mentally I feel young).

    It all boils down to "who's paying for it?"...
    Money greed and lust for power are the fundamental problems of human society.
    Summary, it's not a problem of technology (Ind. 4, Ind. 5, Ind. 6, ...), it's a problem of human society.   

    We'd already be on Mars if we ALL truly worked together and didn't deliberately destroy anything.

    Best Regards
    Gerald
    ---

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB 6 months ago

    Throughout my career, I have always had to deal with legacy systems.

    It has always been a cottage industry to go in and extend the life of working systems, that just need a little upgrade to keep them useful.

    One of my biggest upgrades involved an existing FLIR system on an older helicopter.

    We replaced an old box with some new hardware and software to provide the user with a significant upgrade for a search and rescue system.