Weller
  • Products
  • Manufacturers
  • Weller
  • More
  • Cancel
Weller
Forum I purchased a Weller reflow set
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Weller to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 10 subscribers
  • Views 7529 views
  • Users 0 members are here
Related

I purchased a Weller reflow set

Jan Cumps
Jan Cumps over 3 years ago

The title says it all. I have a Weller solder station. They have IC reflow gizmos that work together with its hot air gun.

image
image source: sinuss.nl, the element14 retailer in Belgium and the Netherlands

These are little ovens, that you put on top of the IC you want to rework. Then you put the hot air pencil inside, to flow the solder.
There's a chip lifter (think: coal mine headframe) that can then lift the IC.
It can also be used to place ICs. Should help me with BGA designs.

It may be over-fancy. Paul Daniels and Louis Rossmann do all of this with just a heat gun. But I'm not that skilled - don't do it enough to be repeatedly successful.
My kit is also expensive. The one I bought, with support for 10x10 mm to 33x33 mm (with 6 steps in between), costs 500 €. An amount that I do not easily give away for tools.

Here's a video from Weller:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I have now burned my budget for the next two years (three years actually, but last year I didn't buy anything). It 'd better work as promised.
Send me your old PCBs, so that I can practice.

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 3 years ago in reply to scottiebabe +4
    Yes, so is the Metcal one of similar design. There's always a justification lurking somewhere though, you just aren't looking hard enough!
  • Jan Cumps
    Jan Cumps over 3 years ago +4
    Customer Action Video: https://youtu.be/-oNphHi_tUk The video is real time, raw footage. No comments or talk. End result: no pads ripped, no pins bent.
  • Jan Cumps
    Jan Cumps over 3 years ago +4
    Test 2, with a bigger IC and one of the bigger ovens. This was more eventful. Not because of the kit, but because of me, learning while on video. https://youtu.be/lWrsRHoDSZM The editing is very…
  • shabaz
    shabaz over 3 years ago

    Really nice! Also looks perfect to lift off ICs for reuse - great for being environmentally friendly : ) 

    I don't fully understand, is the chamber unit unheated, and then hot air is blown in? Or is the chamber heated too? Is the tube on top of the chamber for sucking fumes?

    Also, is the hot air unit part of your Weller solder station. or separate?

    I have a solder station (JBC) but it doesn't have a hot air system as part of it. Instead, I have a separate Metcal hot air unit (model HCT2-120), but it's only 120W power so it's very limiting. I need to get a new hot air tool someday, but I wanted to avoid the low-cost ones (I had one which was about $50 before the Metcal one, and it was loud, and died. I know there's recommendations from youtube people to use the Quick 861DW, but it doesn't look well-built on the inside (this is just speculation based on what it looks like to me, I could be very wrong; I just don't want to spend the several hundred $$$ on it and discover it won't last long. There are comments on the internet about it's unreliability for some people, so that didn't give a warm feeling).

    The Metcal unit is really quiet (turbine type blower I guess) but due to the low power I end up using it for non-soldering tasks (like heat-shrink). It just about manages to reflow solder on small parts, if I also use a pre-heater. It's been working great for several years, I use it regularly, just not much for actual soldering/desoldering tasks : (

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago

    That is definitely a significant investment.

    It looks like the metal frame conducts heat from the air gun to the pins.

    Are chips lifted with a vacuum?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to dougw

    The solder is heated with the hot air directly. The housing spreads the heat over the IC's surface.

    The lifting works with my station's pick-and-place vacuum pump. It has 3 air connections. For the hot air pencil, for the desoldering sucker, and the pick-and-place one.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to Jan Cumps

    It’s an interesting tool Jan.  I’d always read that one should try and uniformly heat up a PCB with the hot air tool to avoid localised hot spots and I took that to mean try to avoid keeping the hot air in one place too long but keep it “moving around” the part.  This looks like a way of evenly heating up the area around the chip: I bet it works well with the board on a hot plate.

    How much clearance around the IC is required?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to Andrew J

    Also, if I think about it, €500 doesn’t sound like a lot for a Weller station albeit a big investment.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to dougw

    baldengineer shows it in this video, at 3'10"

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    I created some training material
    image

    I took apart a Pioneer car stereo (barely used, but aged and no one wanted to buy it on the 2nd hand forum here the last 7 years). I've used the long board yesterday evening to practice small parts recovery, and SMD many-pins-plastic-connector removal.

    The rectangle SMDs will be my training blocks when the rework kit arrives.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago
    Andrew J said:
    €500 doesn’t sound like a lot for a Weller station

    It's just for this:
    image

    No station included. It's made to work with the station I have though.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to Jan Cumps

    Blimey!  In that case, I take it back: it is standard expensive Weller pricing.  At least it will be a quality kit.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago

    Congrats! You deserve it!

    I would like to buy a Weller preheater but cant justify the price....

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
>