Würth Elektronik
  • Products & Partners
  • Manufacturers
  • Würth Elektronik
  • More
  • Cancel
Würth Elektronik
Documents ANR010_Range Estimator Application Note
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Würth Elektronik to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: sandro93
  • Date Created: 27 Jan 2020 9:58 AM Date Created
  • Last Updated Last Updated: 6 Oct 2021 10:16 PM
  • Views 715 views
  • Likes 3 likes
  • Comments 0 comments
Related
Recommended

ANR010_Range Estimator Application Note

   

 

    image

 

 

 

 

 

 

RANGE ESTIMATOR APPLICATION NOTE

 

 

 

 


 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

VERSION 1.0

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

DECEMBER 2, 2019

   

 

 

 
   

1 Introduction

 

When a radio connection is planned the given circumstances define largely the requirements for radio range, operating temperature and available space. To ease the challenge of choosing a suitable RF-module regarding the radio range Würth Elektronik eiSos makes freely available the Range Estimator to find on the website http://www.we-online.com/redexpert . With this tool the modules can be sorted and selected by their attributes. After selecting a module and maybe changing the radio profile and antenna height it shows the calculated range for the Friis model and for the two ray ground reflection model. This application note explains the theory behind the two models, the requirements, differences and the reasonable use.

 

 

image

 

 

Figure 1: RedExpert

 

 

 

 

 


image

 


Figure 2: Range Estimator Overview

   
   

2    Graphical User Interface

 

In order to use the Range Estimator properly, a basic understanding of the selectable attributes is required. The first step is to select a module which is suitable for the application. This will preconfigure the input boxes to a default set of values for the Range Estimator Tool corresponding to the specific data sheet These presets are typical conditions, and may need  to be adjusted by the user.

 

For example, the antenna height has to be adjusted to the utilized height, as this impacts the two ray radio range. Equally the use of an other radio profile with for example a higher data rate would degrade the receiver sensitivity and consequently the radio range.

 

 

 

image


Figure 3: Range Estimator GUI

   


   

3    Fresnel zone

 

 

 

 

image

 

Figure 4: Fresnel zone ideal simplified

 

 

 

 

 

Character

Description

Unit

c0

speed of light in vacuum

[m/s]

dtotal

distance from transmitter to receiver

[m]

f

the frequency of the transmitted signal

[Hz]

Fn

radius of the n-th Fresnel zone

[m]

 

Fnmax

maximum radius of the n-th Fresnel zone between transmitter and receiver

 

[m]

λ

wavelength of the transmitted signal

[m]

n

number of the Fresnel zone

x

point on the line of sight between transmitter and receiver

[m]

 

 

 

The Fresnel zones are ellipsoids around the line of sight between the transmitter Tx and the receiver Rx with the antennas in its focal point. There are multiple Fresnel zones around the line of sight. If an object is within the Fresnel zone in a matter, that a 2-segment path from Tx to Rx deflects off a point within that border. This corresponds to a time-of-arrival difference between the line of sight and the reflected signal from objects, for the primary Fresnel zone of between 0°and 90°, for the second between 90°and 270°, for the third between 270°and 450°and so on. The primary Fresnel zone is the most important to keep free, because most of the signal power will be transmitted in this area.

 

The radius of the any Fresnel zone at any chosen point on the line of sight x is calculated by the equation                                     

   
  (1)image

 

so the equation for the radius on any chosen point on the line of sight is

 

(2)
image

 

this formula makes the assumption, that x and dtotal x both are much longer than n λ,  for the first Fresnel zone this means that x and dtotal x have to be much longer than the wavelength of the signal.

Due to this restriction the radius will not be accurate for distances close to the Tx- or Rx- antenna.

 

 

  image

 

 


  Figure 5: The changing radius of the Fresnel zone for different frequencies with a dtotal of 1000 meters

 

 

   
   

The Fresnel zone shows the largest diameter for x = dtotal x - x = dtotal x /2 , which is actually right in the middle between Transmitter and Receiver.

To get an impression on which objects may cause power loss of the signal, it is often useful to know at least the maximum diameter of the first Fresnel zone. Which according to (1) is.

   
 

image(3)

   

The dependency of the maximum radius from the frequency and the transmission distance is shown in this graph.

Obviously the radius of the Fresnel zone will increase for longer distances between Transmitter and Receiver. But also the frequency of the transmitted signals has a major influence  to the radius of the Fresnel zone. 

A 2.44 GHz Signal will have  an 8.5 meters maximum radius for a line of sight distance of 2350 meters. Will the signal be transmitted with a frequency of 868 MHz a maximum radius of 8.5 meters will only allow a line of sight distance below 850 meters. As a short reminder, any object within the first Fresnel zone will damp the transmitted signal and reduce the range of the transmission.

   
 

 

    image

 

Figure 6: Radius of the Fresnel zone

 

 

 


   

4    Calculation models

 

Depending on the application it is often not possible to keep the Fresnel zone free of objects. So it is essential to understand, that this has high influence on damping of the transmission and therefore maintaining the range of a RF-module. But to estimate its range, a look on the specific datasheet is mandatory. There are several methods to calculate the range of a RF- transmission, but these equations are often very complex and unhandy for  practical usage,  so simplification is needed. The results of the simplified equations are only approximations, but experience shows that the discussed equations are able to deliver reliable estimations  for the transmission range, when applied correctly. As a convention all symbols are in metric units, if not otherwise declared. To improve understanding of basic equations metric units are mandatory, but because logarithmic values are commonly used in radio communication, it is purposeful to also use the logarithmic units for the range calculation.

 

 

 

Character

Description

Unit

λ

wavelength of the signal

[m]

2RPL

path losses of the 2-ray ground reflection model

[dB]

c

speed of light in vacuum (299 792 458)

[m/s]

d

distance from transmitter to receiver

[m]

f

frequency of the signal

[m]

hT x

height of the transmitter antenna over ground

[m]

hRx

height of the receiver antenna over ground

[m]

FSPL

path losses of the free space model

[dB]

LM

link margin (safety to ensure a received signal)

[dB]

PT x

total power emitted by the transmitting antenna

[W] or [dBm]

PRx

total power received by the receiving antenna

[W] or [dBm]

Rxsens

sensitivity of the receiving RF module

[dB]

   
   

 

 

4.1    Friis transmission for free space

 

image


Figure 7: Free space model

 

 

 

Friis transmission for Free  Space is a model to calculate the path loss, to estimate the range of a radio link in a free space environment.

 

This model makes the assumption, that the emitted power is radiated equally in every direction (isotropic) and calculates the power loss only taking into account the decreasing power density of the wavefront with increasing distance to the origin, without any reflection, absorption or attenuation.

   
    image(4)

 

this leads to the free space path loss

   

    image(5)   

expressed in decibel this means,

 

  image

 

 

 

To determine the maximum range of a Wurth Elektronik eiSos RF-module, the path losses

   

    image

 

Figure 8: Wave amplitude depending on the distance to the Tx antenna

 

 

 

of the transmission are equaled to the ratio of the received power to the emitted power:

 

  image

 

     

   

 

  image

 

Figure 9: Path losses for different frequencies

   
   

4.2    Two-ray ground reflection

 

 

 

 

  image

Figure 10: Two ray ground model

 

The two-ray ground reflection model is applied, when transmitter and receiver are in line of sight but the first Fresnel zone is not free ob objects. So the calculation consideres the received power of the direct line of sight path and in addition the power of the reflection path with slight phase difference. In the following a simplified formula is shown, giving suitable results for the precondition of long distance between receiver and transmitter compared to their antenna heights, d » ht + hr.:

 

image(8)

Which translates to

 

  image(9)

and in decibel

image

 

A very interesting aspect now is, that the formula depends on the heights of both antennas but not on the frequency.

 

To determine the maximum range of a module, the path losses of the transmission are equaled to the ratio of the received power to the emitted power:

 

(10)

image
   

(11)image

   

 

 

image

 

Figure 11: Path losses for different antenna heights

   
   

5 Conclusion

 

In a lot of cases there is the need of long distances with regard to the antenna height, so usually the two ray ground model is a good fitting estimation. Only for some special cases with the free space condition fulfilled the Friis model is useful.

 

Having a closer look to the models there are several interesting points to mention.

 

•   One point is the dependency of the frequency. Often it is mentioned in general, that the lower the frequency is, the higher the range is. We have learned, that this is only the case when free field conditions are met.  But there other      effects of the frequency, as the fact, that for higher frequencies smaller objects will cause reflections, or that for low frequencies it might be hard to find an antenna with acceptable size and efficiency.

 

•  An other important point is the influence of the antenna height on the range. The higher the antennas can be placed, the longer is the range that can be reached.  Placing an antenna directly above ground reduces the range so radical, a layman could hardly imagine.

 

 

Often there is stated the free field range for radio modules. This might be useful to compare modules as the two ray ground model would differ depending on the chosen antenna height. But the risk is to underestimate the     difference between this model and the practical reached range.

 

To illustrate, that the Friis model range can diverge extremely from the real accomplish able range, we compare the range estimations of the 2 models. Therefore we pick a module, from which we know, by empirical values and costumer feedback, that the 2-ray ground reflection model is very close to the real accomplished range. Our pick is the Thebe-II, a proprietary radio module at 869 MHz. We adjust the antenna heights to some realistic values, 6m for the transmitter and 6m for the receiver and use radio profile 3, which is one of the long range modes of Thebe-II. In the following screen shot ( 12) we can clearly see in this example, that the range estimation with the Friis model is almost up to twenty times higher, than the range that will be achieved in a real application.

 

Comparing the two models one point catching attention is the often large difference in the resulting range. This is easy explained by the formulas, as in the Friis model the distance is entered by the power of two, in the two ray model by the power of four.

 

 

 

By using the the Range Estimator on Redexpert tool range calculations can be cut, because the range estimation of the 2 ray ground model is pretty accurate.

   
   

 

  image

 

 

Figure 12: Range estimations for Thebe-II

       

 

 

 

 

USEFUL LINKS:

Full PDF

Application Notes

Farnell Shop

HF-Modules

 

 

 

 

Contact:

 

Würth Elektronik eiSos GmbH & Co. KG Division Wireless Connectivity & Sensors

 

Gottbillstr. 22

 

54294 Trier

 

Germany

 

Tel.: +49 651 99355-0

Fax.: +49 651 99355-69

  • radio modul
  • wireless comunication
  • hf modules
  • data communication
  • würth elektronik
  • wifi range
  • range estimator application
  • iot
  • Application Notes
  • wireless
  • range
  • bluetooth modul
  • frequency