Xsens
  • Products & Partners
  • Manufacturers
  • Xsens
  • More
  • Cancel
Xsens
Blog mikroBUS (transceiver) compatibility of the MTi 1-series Development Board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Xsens to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: xsenssupport
  • Date Created: 7 Jan 2022 2:33 PM Date Created
  • Views 11250 views
  • Likes 2 likes
  • Comments 0 comments
  • ins
  • xsens
  • inertial sensors
  • mikroe
  • imu
  • mti 1-series module
Related
Recommended

mikroBUS (transceiver) compatibility of the MTi 1-series Development Board

xsenssupport
xsenssupport
7 Jan 2022

When testing or evaluating the MTi 1-series we highly recommend purchasing a Development Kit, such as the MTi-3 Development Kit or the MTi-7 Development Kit. The Development Board included in this Kit features many different options to communicate with your MTi 1-series device, such as a micro-USB interface and Arduino-compatible headers for UART, SPI and I²C communication.


In addition to this, the Development Board features two mikroBUS extension sockets, one for connecting an external GNSS receiver (MTi-7-DK only) and one for regular communication purposes. This latter communication port can be found on headers P202 and P203 as indicated in the figure below. For the exact pin descriptions, refer to the MTi 1-series DK User Manual.

image

Figure 1: MTi 1-series Development Board. P202 and P203 (bordered in red) together follow the mikroBUS header standard.


The mikroBUS communication extension socket allows users to further extend the communication capabilities of the MTi 1-series Development Board. Because of the mikroBUS standard there are various off-the-shelf "click boards" available that can be mounted here, including boards for serial and wireless communication. Refer to Mikro Elektronika's webshop for a large range of available click boards.

The table below shows a list of transceiver click boards that have been tested with the MTi 1-series Development Board. For some click boards, additional configuration is necessary; see the configuration column.

 

Board Vendor link Compatibility Configuration
RS232 Click

Mikro Elektronika

Farnell

Verified compatibility Full-duplex: Set PSEL0/PSEL1 to 0/0.
RS232 2 Click

Mikro Elektronika

Farnell

- Hardware flow control not supported; RTS/CTS pins reversed.
RS485 Click 3.3V*

Mikro Elektronika

Verified compatibility Half-duplex: Set PSEL0/PSEL1 to 1/0.
Bluetooth Click

Mikro Elektronika

Verified compatibility RST functionality needs to be disabled**.
Can be configured to act as a serial bridge in Windows ("Standard Serial over Bluetooth Link (COM)"), making it fully compatible with the MT Software Suite.


Notes:

*The extension sockets of the MTi 1-series Development Board do not offer a 5V power supply! Click boards can only be supplied at 3.3V.
**Pay attention to the RST pin functionality of mikroBUS click boards. The MTi 1-series Development Board has an active pull-down on this pin, which may conflict with click boards that feature an active-low (nRST) pin.
***The extension socket of the MTi 1-series Development Board will be disabled if the Board is powered at 5V (e.g. through micro-USB)! In order to enable the extension socket you will need to power the board at max. 3.6V. Refer to this page for more information.



If you have any questions regarding this list, please do not hesitate to contact our product specialists.