PCB Design, Prototyping and Production
  • Products
  • More
PCB Design, Prototyping and Production
PCB Blogs KiCAD 8: RX23E-B kit - serial comms schematic
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 2 Nov 2024 10:22 AM Date Created
  • Views 1638 views
  • Likes 8 likes
  • Comments 8 comments
  • kicad
  • rx23E-B
  • renesas
Related
Recommended

KiCAD 8: RX23E-B kit - serial comms schematic

Jan Cumps
Jan Cumps
2 Nov 2024

I'm building a PCB for Renesas' RX23E-B microcontroller. In this post: the UART / serial communications design

image

I've taken over the design of the Renesas Solution Starter Kit for RX23E-B, without the FTDI serial-to-USB. 

image

I'm not sure yet if I will keep the same uart peripheral. It shares its pins with the lcd segment outputs. And I may want to use those too. But if I change the uart, I can't reuse the Renesas out-of-box software ...

  • Sign in to reply
Parents
  • shabaz
    shabaz over 1 year ago

    Hi Jan,

    One idea could be to stick a flat-flex connector footprint on the board, so that the problem is pushed away to another day : ) i.e. a separate LCD PCB could be attached optionally one day. And maybe bringing out two UART options, so that one can be avoided if the LCD were utilized.

    40-pin LCDs are quite common, but they consume a lot of the microcontroller pins : ( I've not tested the symbol/layout below, but when I created it, I noticed that some of the 40-pin LCDs had a slightly larger row spacing than others, hence the reason why there are extra pads along one row in the footprint. There are fewer-pin multiplexed LCDs so they could be a better choice (if the microcontroller supports that).

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to shabaz

    One idea could be to stick a flat-flex connector footprint on the board, so that the problem is pushed away to another day : )

    That's what Renesas did. 

    image

    Maybe I do the same, with the same footprint ...

    Part of the RX23E-B starter kit is a patch bay, where you can select the intended function with 0R resistors

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to shabaz

    One idea could be to stick a flat-flex connector footprint on the board, so that the problem is pushed away to another day : )

    That's what Renesas did. 

    image

    Maybe I do the same, with the same footprint ...

    Part of the RX23E-B starter kit is a patch bay, where you can select the intended function with 0R resistors