PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Blogs KiCAD 8: RX23E-B kit - serial comms schematic
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 2 Nov 2024 10:22 AM Date Created
  • Views 2237 views
  • Likes 8 likes
  • Comments 8 comments
  • kicad
  • rx23E-B
  • renesas
Related
Recommended

KiCAD 8: RX23E-B kit - serial comms schematic

Jan Cumps
Jan Cumps
2 Nov 2024

I'm building a PCB for Renesas' RX23E-B microcontroller. In this post: the UART / serial communications design

image

I've taken over the design of the Renesas Solution Starter Kit for RX23E-B, without the FTDI serial-to-USB. 

image

I'm not sure yet if I will keep the same uart peripheral. It shares its pins with the lcd segment outputs. And I may want to use those too. But if I change the uart, I can't reuse the Renesas out-of-box software ...

  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to dougw

    With this 100 pin controller, and up to 9 pin functions, I need to put some limits. In order to get the job done.

    Here's the design that I'm using as inspiration: Renesas' starter kit.

    image

    I don't plan to make a like-for-like. I'm cherry-picking what I'd like to have. And then expose as much of the other pins as doable.

    USB, PMODs and CAN will go.
    The 4 - 20 mA transmitter and AC excitation driver will go on separate PCBs. 
    Thermocouple connector, RDC and related resistor network will mostly go on a separate little board too.

    All power provisions external. Maybe I make a convenience PCB for that ...

    I plan to keep debug access, (maybe) LCD, UART and all analogue options.

    My design will end up to be more expensive than the Renesas kit (and that isn't cheap either). But I figured that, for that budget, I'd rather have some fun and experiments ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago

    I would tend to include footprints for all variants of solutions I'm interested in, so that I could populate each particular solution when needed. I always buy several PCBs, so I could even assemble multiple versions, each populated in a different way. Sometimes it is worth routing some signals to jumper selectable pins to allow resolution of conflicts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago

    Hi Jan,

    One idea could be to stick a flat-flex connector footprint on the board, so that the problem is pushed away to another day : ) i.e. a separate LCD PCB could be attached optionally one day. And maybe bringing out two UART options, so that one can be avoided if the LCD were utilized.

    40-pin LCDs are quite common, but they consume a lot of the microcontroller pins : ( I've not tested the symbol/layout below, but when I created it, I noticed that some of the 40-pin LCDs had a slightly larger row spacing than others, hence the reason why there are extra pads along one row in the footprint. There are fewer-pin multiplexed LCDs so they could be a better choice (if the microcontroller supports that).

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<