PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Blogs PCB Art:  The Scream
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 24 Jan 2020 3:07 AM Date Created
  • Views 4255 views
  • Likes 13 likes
  • Comments 19 comments
  • pcb_art
  • kicad
  • photoshop
  • pcb
  • art
Related
Recommended

PCB Art:  The Scream

fmilburn
fmilburn
24 Jan 2020

I decided to give PCB art a try and will be basing my attempt on methods described by Andrew Sowa.  Andrew uses Adobe Illustrator for the art work and KiCad for the PCB design.  I will also use KiCad but will use my trusty pre-subscription version of Photoshop for the artwork.  Inkscape is another possibility.  Andrew's process is described in this video from which my work is derived.  The detail behind many of the steps won't be described in this post - watch the video for that.

 

The goal is to take a photograph, painting, etc. and place it on a PCB using the FR4, copper layer, solder mask, and silk screen to make the palette.  My PCB will feature the famous work by Edvard Munch, The Scream which has always fascinated me.  So, how to turn a masterpiece into a PCB facsimile?image

 

Palette

 

The limited palette is a challenge.  For this exercise the focus will be on the central figure in order to reduce board size (and thus cost) of the experiment.  The OSHPark purple solder mask will hopefully give the dark colors desired.  Andrew also used OSHPark in his example, and helpfully provided a palette which has been modified here to help describe how the layers translate to color and are stacked for conversion in KiCad.

image

Different colors will be obtained for different layer transparencies and tints from other board houses.

 

Photoshop Workflow

 

The five colors in the palette must be separated into different layers in the software of choice.  My workflow in Photoshop is as follows:

  1. Create a B&W layer
  2. Create a working layer from the background / B&W layer
  3. Using the Magic Wand Tool (adjust tolerance as needed) select the darkest layer (#5 in the palette) from the working layer
  4. Create a new layer using only the selected area and give it a name (e.g. #5_Mask_on_bare for the darkest layer)
  5. Select the current color (#5 for the darkest layer) from the color picker or palette above and fill the selected area with the color
  6. Delete the selected area from the working layer
  7. Repeat steps 3 - 6 above for the next lighter area until all colors in the palette are selected and all areas of the image are filled with colors from the palette.

 

When these steps are completed the individual layers in Photoshop look something like this:

{gallery} Photoshop Layers

image

Silk Layer

image

Copper Layer

image

Bare FR4 Layer

image

Mask on Copper Layer

image

Mask on bare FR4 Layer

 

The full image with all layers showing as it appears in Photoshop is shown below.

image

 

Next prepare the layers that will be used in KiCad.  The layers are copper (both bare and covered by other layers), mask, and silk.  To do this, combine the layers as shown at the bottom of the palette and convert them to a B&W image.   I used png file format set to 400 DPI and roughly the size I wanted (1 x 1.5 inches).  The resulting images are shown below.

 

{gallery} Layer Images Converted for KiCad

REPLACE THIS TEXT WITH YOUR IMAGEimage

Silk

image

Mask

image

Copper

The work flow in Illustrator demonstrated by Andrew is much different and judging from the video has advantages.  However, my method proved quite workable.

 

KiCad Conversion Workflow

 

From this point on everything is the same as in Andrew's video.  KiCad has a learning curve and the details are beyond the scope of this post.  But here it is in outline form...

 

  • Pull the three B&W images from the last step one at a time into the KiCad Bitmap to Component Converter.
  • Adjust resolution if necessary but not much higher than 400 DPI
  • Set the radio button to Pcbnew (.kicad_mod file)
  • Set Black / White Threshold to 63
  • Set Board Layer for Outline as follows:
    • Front silk screen for silk screen layer
    • Front solder mask for mask and copper layers
  • Export someplace it can be found with meaningful names like Silk, Copper, and Mask

 

The conversion panel will look something like this:

image

 

If named as I did there will be three resultant files:  Copper.kicad_mod, Mask.kicad_mod, and Silk.kicad_mod.  Follow the following steps:

  • Copy the file named Silk to a new file which will be combined with the mask and copper ones to make a footprint in KiCad (I named my file scream.kicad_mod)
  • Open up the Mask.kicad_mod file and copy all sections with fp_poly in the leader to just below the last closing parenthesis ")" in the combined file.  Don't copy the header with fp_text and don't copy the closing parenthesis in the Mask file.
  • Open up the Copper.kicad_mod file in Notepad++ or other text editor and replace all instances of Mask with Cu
  • Copy all sections of Copper.kicad_mod with fp_poly in the leader to just below the last closing parenthesis ")" in the combined file of Copper.kicad_mod.  Don't copy the header with fp_text and don't copy the closing parenthesis in the Copper file.

 

There will now be a combined file which can be used to create a footprint in KiCad which has the layers defined in the 5 colors of the palette.

 

KiCad Pcbnew Workflow

 

Inside of Pcbnew, open up the footprint editor and from the File pulldown select Import Footprint from KiCad file... Navigate to the location of the combined file (in this case the file scream.kicad_mod) and select it.  The footprint will appear as shown below:

image

If desired, view it in the 3D Viewer to make sure it looks right.  Save it in the appropriate library.

 

Now select the Add Footprints tool and place the newly generated footprint in the work area.  Layers can be turned off and on to make sure things look correct.  Draw the boundaries of the PCB on the Edge.Cuts layer.  The 3D viewer in KiCad renders it like this:

image

Finally, use Plot to create the gerber files and it is ready to go to the board house.  Below is what the render from OSHPark looks like.

image

Summary

 

I won't know how good it really looks until the boards come back but for now I am holding off sending it in.  The primary reason is I would like to add an actual circuit to it. It would be possible to build a simple single layer board with the art on the opposite side but it would be nice if the components somehow enhanced the art.

 

The process may seem complicated but it took longer to document than it did to figure out how to create the PCB.  Hopefully by documenting the process it will be even quicker next time.  Thanks for reading.  Comments and suggestions are always welcome!

 

Other posts in this Series

 

PCB Art:  Screaming LM386

Screaming LM386:  An Audio Amplifier with PCB Art

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 6 years ago +5
    Hi Frank, It seems to me that inside every electronics engineer there is a frustrated, or maybe not so frustrated, artist. My attempts have always been very frustrated but I do believe you have a winner…
  • Fred27
    Fred27 over 6 years ago +5
    Some very nice work. It'll be interesting to see how the physical board looks when you get it back. I've been tempted at times to do a PCB business card. One of the things that has held me back is the…
  • Andrew J
    Andrew J over 6 years ago +4
    Brilliant! I’d never even considered the possibility of this, even seeing that people put logos and other images on their boards. I suppose it takes an artist to think of these things... I do like the…
  • 14rhb
    14rhb over 6 years ago in reply to dubbie

    Those diamond blades really are a great invention image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to 14rhb

    I am sure that somewhere on the mitre saw there is something that can be used to adjust the 0 degree click stop. Maybe I'll havev to go and look in the manual.

     

    Yes, a diamond blade is needed when cutting the concrete brick pavers. Plus a good vacuum to take care of all the dust, or do it outside like I do. Not sure what the neighbours think as it is really noisy but no one has complained yet. I do dunk the brick pavers in water before cutting and this does help with the dust level.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 6 years ago in reply to dubbie

    Hopefully there is a screw adjustment or similar that allows you to ensure the 90 degree marking or 'positive click stop' can actually be at 90 degrees. I'll try and look at my saw later to see what I've got - perhaps it will help you.

     

    I note you mention it is for cutting brick pavers - perhaps it is less accurate than a wood saw. I'm assuming you change the blade to do wood?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to Andrew J

    Andrew,

     

    Yes, my local B&Q has a similar box of scrap offcuts, some of which have become resident at my house. I will have to be on the lookout for appropriate parts. Sometimes they even have units and carcasses, which may well be more suitable (that is, easier!). Maybe one day when the sun is shining.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to 14rhb

    It is a powered mitre saw. I have never actually calibrated it as I assumed that it would come from the factory calibrated. It took me over a year to realise that at 90 degrees it wasn't actually making a 90 degree cut as two pieces cut on the saw didn't make a 90 degree joint - it is something like 88 or 89 degrees. It was also only this summer that I realised that it would cut at an angle as well although I haven't tried that out yet. I mostly bought it to cut brick pavers for my patio and 88 or 89 degree cuts are distinguishable from 90 degree cuts, disappointingly.

     

    Using an existing draw carcass is a great idea, I hadn't thought of that, I'll have to see what I can find.

     

    I must also admit to daydreaming about what the draw would do should I ever be able to make. My vision was of opening the draw and the contents slowly unfolding to display all my electronic bits in an accessible way, maybe playing music as well as lights/LEDs. However, the reality is it will probably just be a simple draw that I pull open and then scrabble about in looking for 'bits'.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>