PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum Is there such a PCB construction technique?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 162 subscribers
  • Views 4354 views
  • Users 0 members are here
  • pcb manufacture
  • pcb prototyping
  • pcb fabricating
Related

Is there such a PCB construction technique?

colporteur
colporteur over 3 years ago

image

Is there a PCB construction that creates an area of the board that can easily be broken?

In the sketch the dotted section could be easily broken to reduce the size PCB. My design would have each breakout section containing a button(s) that wire back to a single edge connector. Breaking off pieces of the PCB reduces the number of buttons. 

I was wonder if such a technique is used and what it might be called when constructing a PCB?

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +4
    Yes, there is several techniques that can be used to make divisible PCBs. One is to use V-scoring to cut a channel - this results in a cut line which can be snapped to divide the PCB but nothing can…
  • Gough Lui
    Gough Lui over 3 years ago in reply to Andrew J +2
    Andrew J said: panelling This is when you want to create multiple identical PCBs but have them all attached together as a single "large" board. This is usually done for reasons of easier automated population…
  • Andrew J
    Andrew J over 3 years ago in reply to Gough Lui +2
    If that is the case, it would be even more cost effective than to have them made individually with some form of edge connectors - e.g. as beacon-Dave mentions. It’s something crazy like $1.50 per up to…
Parents
  • shabaz
    0 shabaz over 3 years ago

    Also, if you don't mind ordering thinner PCBs, then it's possible to cut with some scissors, with no slots or holes necessary. You can just draw on the silkscreen layer, a line to guide the scissors visually : ) 

    This was a 0.8mm board I think, and it costs about the same (or very little extra).

    image

    The faint grid dots are 1mm spaced in the screenshot below, to get an idea of the size of the board (it is a 7mm wide strip basically). I added a few tiny holes (yellow) on the silkscreen line, but they were not necessary, but no harm to add them to make it a bit easier.

    image

    This was an LED strip board, where I just wanted a couple of different options to snip off a few LEDs. I guess a similar idea to the buttons you mention.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago

    Also, if you don't mind ordering thinner PCBs, then it's possible to cut with some scissors, with no slots or holes necessary. You can just draw on the silkscreen layer, a line to guide the scissors visually : ) 

    This was a 0.8mm board I think, and it costs about the same (or very little extra).

    image

    The faint grid dots are 1mm spaced in the screenshot below, to get an idea of the size of the board (it is a 7mm wide strip basically). I added a few tiny holes (yellow) on the silkscreen line, but they were not necessary, but no harm to add them to make it a bit easier.

    image

    This was an LED strip board, where I just wanted a couple of different options to snip off a few LEDs. I guess a similar idea to the buttons you mention.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 3 years ago in reply to shabaz

    (In case anyone's curious, the scissors are these ones, they are more like snips, with the short cutting blades but with large handles. The blades are finely serrated, I think that is helping provide good board grip during cutting too. 

    I got them from Workshopshed  choosing a fiber-optic toolkit for me, during a secret Santa event, and these scissors were part of the kit. They're really nice.