PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum Good PCB design practices
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 161 subscribers
  • Views 3526 views
  • Users 0 members are here
  • kicad
  • pcb
  • pcb prototyping
  • pcb design
Related

Good PCB design practices

rsjawale24
rsjawale24 over 3 years ago

I'm working on an oscillator design using an off the shelf integrated circuit-based oscillator.

I have made two large gnd planes in the PCB, the top layer as well as the bottom layer. 

Is this a good practice esp. for making PCBs for applications like oscillators?

I have also added plenty of vias to connect the two layers. 

I just wanted suggestions (if any) before I send the PCB for fabrication. 

image

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +2
    If you have top and bottom ground plane, it is essential to stitch them together with a lot of vias, so that is good. They should be positioned all the way up to the edge of the board. Also more vias at…
  • shabaz
    shabaz over 3 years ago in reply to shabaz +2
    EDIT: In fact, it looks like your project is doing a similar thing to mine, except for the sharper edges. Also, I'm using a multi-position slide-switch instead of a DIP switch, but it's all fairly similar…
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +2
    Some more ideas: 1) If you rotate C2 clockwise 90deg and move it closer to pins 1,2 of U2, the power trace could stay on the top layer. Also the power trace should be much thicker, 1mm (25 mil) as a…
Parents
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago

    Some more ideas:

    1) If you rotate C2 clockwise 90deg and move it closer to pins 1,2 of U2, the power trace could stay on the top layer. Also the power trace should be much thicker, 1mm (25 mil) as a ballpark.

    2) Moving U2 closer to J2 and making the trace from pin5 to the connector center pin a straight line.

    3) SW: the traces connecting pins 1, 2, and 3 routed on the outside of the footprint would make the design more obvious when looking at the PCB and easier to cut if needed. Same for U1 pins1 and 3.

    4) If SW1 is a regular DIP8 footprint, the 2 jumpers J1 and J3 look like a pin distance of 1.27mm (50mil), which is half the size of a regular 0.1" jumper. I once had an eval board with those tiny bastards, they were terrible to handle (2nd picture on the linked post).

     Vishay microBUCK SiC461 Eval Board 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago

    Some more ideas:

    1) If you rotate C2 clockwise 90deg and move it closer to pins 1,2 of U2, the power trace could stay on the top layer. Also the power trace should be much thicker, 1mm (25 mil) as a ballpark.

    2) Moving U2 closer to J2 and making the trace from pin5 to the connector center pin a straight line.

    3) SW: the traces connecting pins 1, 2, and 3 routed on the outside of the footprint would make the design more obvious when looking at the PCB and easier to cut if needed. Same for U1 pins1 and 3.

    4) If SW1 is a regular DIP8 footprint, the 2 jumpers J1 and J3 look like a pin distance of 1.27mm (50mil), which is half the size of a regular 0.1" jumper. I once had an eval board with those tiny bastards, they were terrible to handle (2nd picture on the linked post).

     Vishay microBUCK SiC461 Eval Board 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 3 years ago in reply to wolfgangfriedrich

    1.27mm pin headers are the worst! : ) The board size looks spacious so normal 0.1" would fit anyway. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 3 years ago in reply to wolfgangfriedrich

    Thank you for the ideas!

    I'll modify the power trace.

    SW1 is a DIP switch. J1 and J3 will not be populated and I'll just solder wires to the PCB.