PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum Easy Front Panels with KiCad
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 160 subscribers
  • Views 6595 views
  • Users 0 members are here
  • step
  • kicad
  • 3d
  • dxf
  • Front Panel
  • kicad 6.0
  • pcb design
Related

Easy Front Panels with KiCad

shabaz
shabaz over 3 years ago

I really like using extruded aluminium enclosures, such as this one from Farnell/Newark. They are great because they come in different lengths, so if the project doesn't fit, I can just choose a longer enclosure!

image

Another great benefit is that the front panels can be made of either PCB material (FR4), or aluminium, since a lot of the prototype PCB manufacturers provide cheap metal core circuit boards too. By using these services, I do not need to do any drilling. The PCB manufacturer does all the hard work for me, milling/drilling out any shapes required.

image

I just spent an hour painstakingly drawing the front panel for this enclosure. And then realized I could have done it in five minutes if I'd thought about it!

The solution was, to search out the DXF file for the enclosure, and then import it into KiCad : )

The screenshot below shows my hour-long effort at the top, and the immediate DXF import below! 

image

In the past, I've found it time-consuming, manually pulling measurements from drawings in the enclosure datasheet. The one below took me ages (it is quite old, it was done with EAGLE at the time).

image

In KiCad 6, it was as easy as going to the PCB Editor, and clicking on File->Import->Graphics and selecting the DXF file. The file has all graphic elements grouped, so you can right-click on the content and select Grouping->Ungroup, and then get rid of any superfluous DXF content. I imported the content on a drawing layer, so then I can simply trace out the actual shape I want using the Edge.Cuts layer as normal, and use the drawing layer to see precisely where the PCB will be inserted, so that I can create connector/LED/display cut-outs exactly where they are needed.

I'm going to be doing this a lot more in future since it opens up the opportunity to have extremely nice front panels, done right-first-time.

Note that you can take this to the next level by then saving your front panel in STEP format (click on File->Export->Step) and then importing it into FreeCAD, along with your actual project PCB, plus the STEP file for the enclosure (if it exists), and then assemble it all virtually : )

For instance, here's a different project, where I put the project PCB into an enclosure (non-extruded in this case). This project doesn't have a front panel, but I could easily make one if needed, using the method described.

image

Thanks for reading!

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 3 years ago +4
    I created 4 different panels in this way following your earlier effort. It’s such a good idea and the finished results look great. Range of colours with JLCPCB too. I have two tips if using JLCPCB; …
  • shabaz
    shabaz over 3 years ago in reply to Andrew J +3
    Found it here .. I'm going to remember is as 4 JLC's ... also need to click on " Specify a Location ". I wish they would optionally accept a file (e.g. JSON, YAML or whatever) with all their config settings…
  • baldengineer
    baldengineer over 3 years ago +2
    I usually import SVG instead of DXF in KiCad. In the past, I had trouble with it not handling curves very well. SVG hasn't been perfect either, however. I sometimes have to apply a scaling factor. So…
Parents
  • dougw
    dougw over 3 years ago

    Presumably the entire drawing could be done as a DXF, including text.

    It brings up the age old question - should the mechanical design accommodate the electrical design or should the electrical design fit the mechanical design?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to dougw

    Hi Doug,

    I believe it could, and would be a better way for those familiar with (say) Inkscape or any CAD package.

    In my case, I don't have any 2D CAD package that I know how to use (and I can barely do anything with FreeCAD or Inkscape) so preferred to do as much in the KiCad editor, i.e. just use the enclosure manufacturer's DXF file imported in as a drawing layer and overlay with my own cut lines and silkscreen where needed.

    I liked old AutoSketch and old AutoCAD, and the excellent Generic CADD (it was a DOS application) but I've forgotten how to use them (and don't have copies of them any longer).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to dougw

    Hi Doug,

    I believe it could, and would be a better way for those familiar with (say) Inkscape or any CAD package.

    In my case, I don't have any 2D CAD package that I know how to use (and I can barely do anything with FreeCAD or Inkscape) so preferred to do as much in the KiCad editor, i.e. just use the enclosure manufacturer's DXF file imported in as a drawing layer and overlay with my own cut lines and silkscreen where needed.

    I liked old AutoSketch and old AutoCAD, and the excellent Generic CADD (it was a DOS application) but I've forgotten how to use them (and don't have copies of them any longer).