PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum KiCad 7.0.0 Is Here!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 161 subscribers
  • Views 33529 views
  • Users 0 members are here
  • eda
  • kicad
  • schematic capture
  • kicad 7.0
  • ecad
  • pcb
  • pcb design
Related

KiCad 7.0.0 Is Here!

baldengineer
baldengineer over 3 years ago

game gear schematic drawn in KiCad 7

Just slightly over a year since releasing version 6, the development team has released KiCad 7.0!

Something like 1200 (reported) issues were addressed in this update. And an ASIC-load (get it? instead of boat-load...) of new features. You can start the KiCad 7.0 download here. While that chonker downloads, you can read the full announcement or check out my longer KiCad 7 write-up on the release.

My Favorite Two New Features (so far)

Colorizing nets in the Schematic editor was the last thing I played with before the official release. The above image is my version of the Game Gear schematic. (It's in the Bit Preserve GitHub repo.) To help keep the various buses straight, I assigned the bus and its nets to a custom color. I love using this colorization for address, data, and power rails. It really helps things to pop when looking at the schematic.

My other favorite feature is the properties panel in PCB. As the name implies, it brings the properties of an element to the top of the UI. First, it saves you from having to "edit" a footprint to adjust its settings. And second, it lets you group multiple similar elements together and change common properties. So, for example, you can grab multiple graphic elements and move them to a different layer without opening any other dialogs!

So, those were the two stand-out features that I really liked. But there are so many more.

Have you used it yet? If so, what do you like (or not like!) about KiCad 7.0?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago in reply to baldengineer +4
    who will make the first Comic Sans board?
  • shabaz
    shabaz over 3 years ago +3
    I decided to edit a KiCad 6.0 version board with version 7.0, and happened to use the font capability. The font here looked too informal, so I reverted back to the KiCad standard font after this screenshot…
  • shabaz
    shabaz over 3 years ago +3
    I tried the Pack-and-Move ('P' key) on an older Kicad 6 schematic. It's going to save a HUGE amount of time!
Parents
  • shabaz
    shabaz over 3 years ago

    I've installed it too, (in parallel with existing KiCad 6, with backed-up projects and custom libraries) and it all went well, although I will need to manually locate 3D files for some of the custom library footprints, but I had expected to do that, and it's not a big issue. I'm probably not going to make a PCB with it until a V7 dot-release is available, but I figured it's still a good time to use it to try the new features.

    Several of the new features are super-helpful, especially in the PCB Editor area; the properties pane feature and the 'P' pack-and-move will both save a _lot_ of time.

    The quick line-finish tool (pressing F) in the PCB editor could same some time too. Also, the inverted ('knockout') text is great to see, although it would be nicer if you could draw any filled shape and have the text cut out the filled shape if the text is placed on top. Maybe that's very difficult to implement though, and there are other workarounds anyway.

    The only disappointment for me is that the footprint editor didn't see any properties pane-like functionality at all. It's a pain having to edit each pad one at a time, if a slight tweak needs to be made. Some CAD packages allow for a pad definition to be created separately (I don't like that method, but I can see why they do that). It would be nice to see some sort of solution for rapidly changing all similar pads in one go. Maybe there is a way to do this, but I've not found it yet, and I didn't see anything to indicate that the properties pane will eventually make its way to the footprint editor. 

    My current workaround is to delete all the pads and re-do them all if I need to tweak many pads, but it's not great.

    One other thing that would be nice to see is a way of truncating or splitting lines (e.g. PCB edge cuts, or silkscreen lines) where they intersect. Quite minor, but would be helpful occasionally.

    In summary, using V7 is just as easy as using V6, and from my perspective, it was great to see the new V7 features, particularly in the PCB Editor area,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to shabaz

    The only disappointment for me is that the footprint editor didn't see any properties pane-like functionality at all.

    I did not realize it was missing from the footprint editor until someone asked in the KiCad Discord this morning. Currently, the only way I can think to bulk-edit pads is to copy/paste them into a text editor, then paste back. Less than ideal, but at least faster than going through each pad one at a time.

    I strongly suspect we'll see the Properties panel get implemented through the suite. It's current form feels more like a "let's see how to make this work" and then the next iteration will be more integrated throughout.

    Hopefully V7 is the start of the trend. An update of this size in about year will make version 8 very interesting to see.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to baldengineer

    Ah, great idea to text-edit it. I keep forgetting that option exists and is very viable.

    Also, the yearly release is fantastic, I hope they always have such a schedule! : ) That would be the best KiCad feature : )

    On a product group I worked on, customers loved that releases were at fixed (almost guaranteed) dates. They would only slip by a week or so under extreme circumstances. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to baldengineer

    Ah, great idea to text-edit it. I keep forgetting that option exists and is very viable.

    Also, the yearly release is fantastic, I hope they always have such a schedule! : ) That would be the best KiCad feature : )

    On a product group I worked on, customers loved that releases were at fixed (almost guaranteed) dates. They would only slip by a week or so under extreme circumstances.