PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum The magic of Tin cans!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 159 subscribers
  • Views 2757 views
  • Users 0 members are here
Related

The magic of Tin cans!

battlecoder
battlecoder over 2 years ago

I've been learning more about electromagnetic interference for a while now, and in the process improving my tools and my understanding on how to measure, counter and prevent EMI, noise, crosstalk, etc. And this weekend I had the opportunity to put some of that knowledge in practice (although admittedly the most basic things).

I had this small switching module that takes 2.8-5.5V as input, and outputs ±12V, which is very useful for op-amps and other circuits, and it was supposed to be used connected to another module; a low-noise, 10x gain differential amplifier.

There were two problems with the board. The first one was that the voltage output itself was a bit noisy. This was to be expected since it is a switching supply with not a lot of filtering at the output stage. I fixed this with 79XX and 78XX regulators and a couple of capacitors.

But the other problem is that the module itself emits a crazy amount of EMI, which was very undesirable, given that this module was going to sit very close to a low-noise amplifier board.

To solve that problem I tried putting the board inside a small tin box, and here's the result:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I already knew that "tin cans" (or generally speaking; metal shielding) was an effective way of blocking EMI, but I wasn't expecting THIS much of a difference with a repurposed "hand cream sample" tin can Stuck out tongue

I've used "buck-boost" converters and other switching supplies modules in the past. To the point that they have become an essential "tool" to power electronics in my projects, especially when there's a very specific voltage requirement that can't be easily met with a battery pack or power adapter, or when using a linear regulator would dissipate too much heat, or won't be able to take advantage of the full voltage range of the batteries.

But I wasn't aware of how much EMI they can emit. I'm sure as hell going to be placing them all inside metal enclosures if they are going to be sitting next to noise-sensitive electronics or sensors, from now on.

As I always wonder about other people's experiences, I'd love to ask the community if you have ever needed to put a circuit inside a metal-shielded box in order to fix an issue caused by EMI (or to prevent it from ever happening) ?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +4
    Not a top quality shielding method, but cheap, I've been sanding the ends of aluminium extruded boxes from AliExpress etc. The idea being that the end panels (sanded on the inside) will make the electrical…
  • jc2048
    jc2048 over 2 years ago +4
    I've used actual tin cans for temporary screening in blogs here on e14. Here's one where I was trying mainly to keep out mains noise, but also a low-level nuisance signal (a sawtooth between 40 and 50kHz…
  • michaelkellett
    michaelkellett over 2 years ago +3
    For an example of tin-cannery to the max try: https://www.eevblog.com/forum/blog/eevblog-1256-most-gorgeous-test-gear-teardown-ever!/ Modern scope and spectrum analysers tend to use multi compartment…
Parents
  • shabaz
    shabaz over 2 years ago

    Not a top quality shielding method, but cheap, I've been sanding the ends of aluminium extruded boxes from AliExpress etc. The idea being that the end panels (sanded on the inside) will make the electrical connection between the two halves.

    image

    Or, lazy approach, replace the metal end panels with PCBs. Saves effort sanding/drilling, and only costs £2 or so added to a PCB order.

    image

    The inner side has no solder mask.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 2 years ago

    Not a top quality shielding method, but cheap, I've been sanding the ends of aluminium extruded boxes from AliExpress etc. The idea being that the end panels (sanded on the inside) will make the electrical connection between the two halves.

    image

    Or, lazy approach, replace the metal end panels with PCBs. Saves effort sanding/drilling, and only costs £2 or so added to a PCB order.

    image

    The inner side has no solder mask.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • battlecoder
    battlecoder over 2 years ago in reply to shabaz

    I love those small boxes from Aliexpress. Ironically I've only used *one* out of the couple I once bought, and I never bothered measuring whether it made any difference protecting the circuit from EMI (this was a long time ago, before I even got interested in this). I should sand the interior pieces to connect the whole shell as you did, though.

    I like the PCB idea too.