PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum The magic of Tin cans!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 159 subscribers
  • Views 2748 views
  • Users 0 members are here
Related

The magic of Tin cans!

battlecoder
battlecoder over 2 years ago

I've been learning more about electromagnetic interference for a while now, and in the process improving my tools and my understanding on how to measure, counter and prevent EMI, noise, crosstalk, etc. And this weekend I had the opportunity to put some of that knowledge in practice (although admittedly the most basic things).

I had this small switching module that takes 2.8-5.5V as input, and outputs ±12V, which is very useful for op-amps and other circuits, and it was supposed to be used connected to another module; a low-noise, 10x gain differential amplifier.

There were two problems with the board. The first one was that the voltage output itself was a bit noisy. This was to be expected since it is a switching supply with not a lot of filtering at the output stage. I fixed this with 79XX and 78XX regulators and a couple of capacitors.

But the other problem is that the module itself emits a crazy amount of EMI, which was very undesirable, given that this module was going to sit very close to a low-noise amplifier board.

To solve that problem I tried putting the board inside a small tin box, and here's the result:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I already knew that "tin cans" (or generally speaking; metal shielding) was an effective way of blocking EMI, but I wasn't expecting THIS much of a difference with a repurposed "hand cream sample" tin can Stuck out tongue

I've used "buck-boost" converters and other switching supplies modules in the past. To the point that they have become an essential "tool" to power electronics in my projects, especially when there's a very specific voltage requirement that can't be easily met with a battery pack or power adapter, or when using a linear regulator would dissipate too much heat, or won't be able to take advantage of the full voltage range of the batteries.

But I wasn't aware of how much EMI they can emit. I'm sure as hell going to be placing them all inside metal enclosures if they are going to be sitting next to noise-sensitive electronics or sensors, from now on.

As I always wonder about other people's experiences, I'd love to ask the community if you have ever needed to put a circuit inside a metal-shielded box in order to fix an issue caused by EMI (or to prevent it from ever happening) ?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +4
    Not a top quality shielding method, but cheap, I've been sanding the ends of aluminium extruded boxes from AliExpress etc. The idea being that the end panels (sanded on the inside) will make the electrical…
  • jc2048
    jc2048 over 2 years ago +4
    I've used actual tin cans for temporary screening in blogs here on e14. Here's one where I was trying mainly to keep out mains noise, but also a low-level nuisance signal (a sawtooth between 40 and 50kHz…
  • michaelkellett
    michaelkellett over 2 years ago +3
    For an example of tin-cannery to the max try: https://www.eevblog.com/forum/blog/eevblog-1256-most-gorgeous-test-gear-teardown-ever!/ Modern scope and spectrum analysers tend to use multi compartment…
  • michaelkellett
    michaelkellett over 2 years ago

    For an example of tin-cannery to the max try:

    https://www.eevblog.com/forum/blog/eevblog-1256-most-gorgeous-test-gear-teardown-ever!/

    Modern scope and spectrum analysers tend to use multi compartment "cans" machined form solid metal.

    You can buy nice kits for making pcb mounted screening cans and ready made ones:

    https://www.etch-tech.co.uk/products/screening-cans/

    https://www.digikey.co.uk/en/product-highlight/h/harwin/emc-rfi-shield-clips-and-shield-cans

    I often use diecast boxes for one-offs.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago

    Funnily enough I just bought a new wallet, and it came with a "RFID blocker" claimed feature. I didn't seek that feature particularly, it just happened to have it. But I am curious to give it a try, see how effective it is with NFC with a mobile phone. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 2 years ago in reply to michaelkellett

    I didn't knew there were ready-made kits for PCBs! I always assumed they were custom-made by the manufacturers and only sold in custom-ordered industrial quantities. Nice!

    Also: Wow that's a lot of cans!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 2 years ago in reply to shabaz

    Even if you don't need it, I truly hope it works and it's not a fake marketing claim. I kinda hate when products are advertised as having a feature or being able to do a thing, that they truly don't.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to battlecoder

    EEVBlog tested it. 10:12 in the video:

    https://youtu.be/EICbskk-0dM?si=hp3bruAI_y5x3WID&t=612

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 2 years ago in reply to Jan Cumps

    It works!

    My passport came with an rfid blocking envelope (might’ve been free with the passport photos), and at security they always instructed us to remove the passport from the envelope.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 2 years ago in reply to ntewinkel

    Nice! My last credit card also came in one of those envelopes now that I think of it. Will look for it and test it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago

    Understanding EMI is a very useful skill to have.

    In my early years I was working with high powered lasers that generated a lot of EMI.

    We used a copper screen room to house the beast for normal operation.

    One day they wanted to know just how sensitive our PDP-11-20 was to EMI, so they put the laser on a cart and began moving it towards the computer.

    When it got to within about twenty feet, the computer we down.

    In the EMI world, 20 feet is a huge distance, which gives you an idea of the magnitude of the EMI pulses coming from the laser.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 2 years ago in reply to DAB

    That's crazy. EMI power drops considerably over the smallest increases in distance. 20 feet is a whole universe apart for most electronics.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago

    Not a top quality shielding method, but cheap, I've been sanding the ends of aluminium extruded boxes from AliExpress etc. The idea being that the end panels (sanded on the inside) will make the electrical connection between the two halves.

    image

    Or, lazy approach, replace the metal end panels with PCBs. Saves effort sanding/drilling, and only costs £2 or so added to a PCB order.

    image

    The inner side has no solder mask.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
>