PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum First attempt at SMD soldering
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 166 subscribers
  • Views 6305 views
  • Users 0 members are here
Related

First attempt at SMD soldering

Andrew J
Andrew J over 7 years ago

I bought a practice kit that, in theory at least, lights up LEDs in some sequence.  I say in theory, but as all the instructions (presumably) are in Chinese, who knows??  Anyway, it has components in a number of sizes: 1206, 0805, 0603, 3528, not sure for the ICs.

 

I've spent the afternoon soldering away - 76 components - and what can I take away from the experience?  Well:

  1. forget 0603, I'm not going there again.  Just too small for hand soldering.  I did of course lose a 0603 capacitor to the God of Misery and the kit had no spares.  One day, I expect to find it. Or not.
  2. forget resistor arrays as well (I think that's what they are), especially in 0603.  Seriously, what sadist invents such a thing??
  3. 0805 is likely to be the minimum I go with.
  4. I need a microscope to do this stuff.  At my age, my eyes aren't good enough and I have a bit of handshake too.  See also (1)!
  5. I need more practice at (a) soldering; and (b) keeping care of my tip.
  6. 0.46mm solder is still a bit thick, but just about do-able.  I dare say if I was better at 5a then it would be ok
  7. Still unsure of the best tip to use.  I had a 1.2mm chisel tip which is the smallest that I have, bar a pointy one
  8. Solder wick (decent stuff) is very useful
  9. It's not clear what the markings on a LED are - there were two variants (green marks on one lot, cut corner on the other lot.)  I did search but found the information results confusing: I assumed the marks referred to the Cathode.
  10. The ICs weren't too bad: I can't detect bridging, solder wick helped
  11. I don't think I'd be too worried about it in the future, at least I've taken the plunge right!  I'm not convinced I'd do better with paste and a hot-air gun either.

 

Questions I have:

  1. Is 350c too hot?  I used leaded solder: Sn 62, Pb 36, 2Ag with 505 rosin cores from Multicore.  It has a melting temperature of 179C.
  2. Would I fair better with a thinner tip?
  3. I used flux but my experience was it burnt off immediately and seemed to do nothing - related to questions 1 and 2?

 

I suppose the question on everyone's lips is "did it do anything?"  Well, in short, no.  I tested the resistors and they seemed ok, the ICs were getting voltage to the correct pins so I know they are the right way around.  Perhaps the LEDs are on the wrong way, perhaps the soldering isn't right, perhaps components are not in the right place (no markings on the tapes so I may have deduced incorrectly), perhaps it doesn't do anything anyway, perhaps, perhaps.  I'm not too bothered: it was a test/practice of soldering SMDs which it achieved.

 

I could definitely do with more practice but I expect I'll get better over time.  I also think that these practice kits are a good idea and I would recommend one to someone whose not done this before.

 

Thanks for listening image

 

EDIT: I have a follow up thread as well - https://www.element14.com/community/message/275494/l/second-attempt-at-smd-soldering#275494

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 7 years ago in reply to Fred27 +9
    I can do you a photo, I'm not ashamed . Don't look too closely at the Capacitors though - those were (some of) the evil 0603s, one of which has gone on holiday. This was all done by eyesight as well.
  • jw0752
    jw0752 over 7 years ago +8
    Hi Andrew, I think you did a pretty good job too. With respect to the LEDs I always use a small analog multimeter set to R X 1 to test and verify polarity on small difficult LEDs. In the case of my analog…
  • Fred27
    Fred27 over 7 years ago +7
    No photos? Maybe best not for your first attempt! Of course you can now practice some rework until either the LEDs light up or you destroy it by lifting a track. It won't take long to get used to SMD.…
Parents
  • 14rhb
    14rhb over 7 years ago

    Hi Andrew,

     

    Well done for your exploits into the SMT field - I'm sure in time you'll get more confident and start to expand on your equipment required to make things a bit easier (like David suggests a microscope). To answer your questions:

     

         1.     Is 350c too hot?  I used leaded solder: Sn 62, Pb 36, 2Ag with 505 rosin cores from Multicore.  It has a melting temperature of 179C.

         Not in my opinion, but it will cause the tip to deteriorate quicker....not that you'll probably notice much if you only solder occasionally.

     

         2.     Would I fair better with a thinner tip? 

         Always handy to make sure you only get the heat onto the required pad, in which case keeping the tip temperature up is probably a good thing.

     

         3.     I used flux but my experience was it burnt off immediately and seemed to do nothing - related to questions 1 and 2?

         A flux pen does definitely help the solder flow; it cleans off impurities and helps prevent solder bridging between tracks.

     

    I find the best way to solder the smallest resistors is to:

    • apply flux to the pads
    • heat and apply the slightest dab of solder (a thin solder wire helps here)
    • if too much solder is applied then use de-soldering braid to remove the excess
    • holding the components on the long sides with some fine tweezers, position with one hand and heat the pre-tinned pad to make the initial solder joint
    • I then use the tweezers to push lightly on the top of the component and reheat that first joint to get the component to sit down flush onto the pad
    • I then apply solder to the second end
    • Once that has solidified I often give the first side another quick touch of the soldering iron to ensure a better joint

     

    As you have found, it can still go wrong: the tweezers ping the component off to oblivion, the 0603 gets wicked into the solder on the end of your iron, solder bridges remain hidden....all part of the fun image

     

    Rod

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • 14rhb
    14rhb over 7 years ago

    Hi Andrew,

     

    Well done for your exploits into the SMT field - I'm sure in time you'll get more confident and start to expand on your equipment required to make things a bit easier (like David suggests a microscope). To answer your questions:

     

         1.     Is 350c too hot?  I used leaded solder: Sn 62, Pb 36, 2Ag with 505 rosin cores from Multicore.  It has a melting temperature of 179C.

         Not in my opinion, but it will cause the tip to deteriorate quicker....not that you'll probably notice much if you only solder occasionally.

     

         2.     Would I fair better with a thinner tip? 

         Always handy to make sure you only get the heat onto the required pad, in which case keeping the tip temperature up is probably a good thing.

     

         3.     I used flux but my experience was it burnt off immediately and seemed to do nothing - related to questions 1 and 2?

         A flux pen does definitely help the solder flow; it cleans off impurities and helps prevent solder bridging between tracks.

     

    I find the best way to solder the smallest resistors is to:

    • apply flux to the pads
    • heat and apply the slightest dab of solder (a thin solder wire helps here)
    • if too much solder is applied then use de-soldering braid to remove the excess
    • holding the components on the long sides with some fine tweezers, position with one hand and heat the pre-tinned pad to make the initial solder joint
    • I then use the tweezers to push lightly on the top of the component and reheat that first joint to get the component to sit down flush onto the pad
    • I then apply solder to the second end
    • Once that has solidified I often give the first side another quick touch of the soldering iron to ensure a better joint

     

    As you have found, it can still go wrong: the tweezers ping the component off to oblivion, the 0603 gets wicked into the solder on the end of your iron, solder bridges remain hidden....all part of the fun image

     

    Rod

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Andrew J
    Andrew J over 7 years ago in reply to 14rhb

    All those things happened Rod! 

     

    The approach you you laid out is, essentially, what I did except the 5th bullet (press on top), I shall remember that.  I did use a flux pen but it just seemed to burn off immediately.  I also think I could do with some thinner solder which is a shame as it isn’t cheap.

     

    if I give it another go (get another practice kit), I may try a smaller tip and experiment with the temperature.  If only it was as easy as they make it look on YouTube image

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 7 years ago in reply to 14rhb

    Rod,

     

    I would second all of your suggestions (almost like you looked over my shoulder when I was soldering.

     

    Gene

    • Cancel
    • Vote Up +7 Vote Down