PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum Second attempt at SMD soldering
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 164 subscribers
  • Views 2876 views
  • Users 0 members are here
Related

Second attempt at SMD soldering

Andrew J
Andrew J over 7 years ago

Following on from this discussion where a lot of tips came my way, I thought it only right to give it another go:  https://www.element14.com/community/thread/72152/l/first-attempt-at-smd-soldering  I really feel like I've joined the club now I burnt the end of one of my fingers image  On the plus side, none of the parts went pinging off.

 

In no particular order...

 

Following Antonio Tajeda's advice, I got hold of a DS3231 kit to have a play with - more on that later!  I did look up a 900M-T-3CM900M-T-3CM tip for my Hakko FX-888DFX-888D but couldn't find any in the UK and HK Wentworth wanted £20+ and £5 P+P for one which they'd get from Japan.  I'll keep my eye open but decided to try with the tips I had - the T18-D12T18-D12 worked very well.  I also re-watched the videos linked to on YouTube - they make it look VERY easy but I expect technique comes with practice.

 

Following Gene Breniman's and Luis Ortez's advice on a magnifier I have been looking at microscopes but I also tried a head magnifier in the first instance - I got one with swappable glass lenses.  The 2x was great for a bit of through hole soldering I did yesterday, and I managed pretty well on the DS3231 kit with the 3.5 magnification.  My only real issue was having to get so close to see in focus - I was around 4 inches away.  I used a PCB holder and that raised the board up so it wasn't too uncomfortable.  I think I'll persevere with that for a while and save the money.

 

Following Shabaz's advice I got hold of some thin solder - 0.274mm.  It was significantly easier to work with at this size than my 0.46mm.  The two sizes together are great for both through hole and SMD.  I also dropped the temperature down to 300C and had no problems - I suspect with some of the larger pads I should go a bit higher but it all worked.

 

There were a bunch of other tips as well, from many others who I haven't named, in respect to flux, tinning one pad first and so on - these work very well so anyone picking up on this thread could do worse than follow them.

 

Someone, somewhere on a different thread suggested the use of blu-tack (or similar) for through hole - it might have been Shabaz - I can confirm that it is an excellent tip!

 

So, here are some photos.

 

The LED Side

image

 

The other side - mix of SMD and through hole:

image

 

Close ups:

image

 

image

(I honestly thought I'd cleaned that up with IPA - couldn't see the mess by eye!)

 

And, finally:

image

 

As for the kit.  The PCB looks well made, exceptionally 'skiddy' surface.  However there were NO instructions with it which for the most part wasn't a problem, but placing the resistors was really an educated guess - one I got right based on everything lighting up.  There's a couple of dodgy LEDs: in the photo they are lit but will only colour blue.  Also, it isn't possible to actually set a time, date etc as the touch buttons (which I didn't have to do anything with) don't work.  As there's no schematic I can't tell if it's a soldering problem with one of the chips or just a dodgy board: there are no bridges that I can spot under my x5 magnifying glass.  Perhaps the buttons need the battery, who knows??

 

I think there is some scope here for Element 14 to create some quality practice kits, with instructions and troubleshooting hints.

 

Anyway, it was enjoyable doing it and great practice.  Given that it's my fourth or fifth time picking up a soldering iron I'm really pleased with myself.  Time for a celebratory beer.

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 7 years ago in reply to Fred27 +6
    Ha! Can I recommend blu-tack, or white tack. Yesterday I soldered a 4x1 header and a 4x2 header perfectly perpendicular with that stuff holding it down. And because it's stuck on solder mask it lifts right…
  • Andrew J
    Andrew J over 7 years ago in reply to shabaz +6
    Thanks Shabaz. I had looked for some wipes but they are expensive in this country. I mean to buy a brush, just haven't gotten around to it yet. I mostly used my flux pen although I do have some flux paste…
  • shabaz
    shabaz over 7 years ago in reply to Andrew J +6
    Hi Andrew, That's great that you're taking these precautions (many newcomers don't I bet : ). From what you say, and seeing the quality of the soldering, I bet it's 99% likely the cause is ESD-related…
Parents
  • Fred27
    Fred27 over 7 years ago

    Nice work. Very neat.

     

    I don't know about everyone else but I find that even though I'll now happily solder 0.4mm pitch LQFP and QFN, I can still make a right mess of a simple 0.1" through hole header if it suits me. image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fred27
    Fred27 over 7 years ago

    Nice work. Very neat.

     

    I don't know about everyone else but I find that even though I'll now happily solder 0.4mm pitch LQFP and QFN, I can still make a right mess of a simple 0.1" through hole header if it suits me. image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Andrew J
    Andrew J over 7 years ago in reply to Fred27

    Ha!  Can I recommend blu-tack, or white tack.  Yesterday I soldered a 4x1 header and a 4x2 header perfectly perpendicular with that stuff holding it down.  And because it's stuck on solder mask it lifts right off.  DO NOT stick it over vias, it doesn't come out image

    • Cancel
    • Vote Up +6 Vote Down