Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog A second helping of Pumpkin Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fustini
  • Date Created: 25 Oct 2012 6:44 AM Date Created
  • Views 5199 views
  • Likes 1 like
  • Comments 20 comments
Related
Recommended
  • halloween
  • pumpkin_pi
  • raspberry_pi
  • rpiexpert
  • adafruit

A second helping of Pumpkin Pi

fustini
fustini
25 Oct 2012
imageWant to build this project?
View Parts

 

In my last post, I introduced the Pumpkin Pi: a Raspberry Pi project for Halloween.  It puts a Raspberry Pi inside a jack-o'-latern to provide web-controlled lights and sound:

image

(click to enlarge; screenshot of latest version as of 2012-Oct-26)

 

The Pumpkin Pi software was written in Python with generous assistance from Bonnie King and can be found on GitHub under my account "pdp7" in the punkin_pi repository.

 

 

Install dependencies:

To run punkin_pi on your Rasperry Pi, you'll first need to install these dependencies.  The following commands were run on the current Raspbian 2012-Sept-18 image:

sudo apt-get update

 

sudo apt-get install git-core mplayer python-setuptools


sudo easy_install bottle

 

sudo easy_install RPi.GPIO

If running an earlier image, then you may encounter an error on when installing the RPi.GPIO in that last step ("couldn't find Python.h").  To resolve the error, run this command:  sudo apt-get install python-dev and then sudo easy_install RPi.GPIO again.  Thanks to Joel Dunn for the advice!

 

 

Install sound clips:

Next, sounds clips that the pumpkin will play need to be installed.  I downloaded a few .wav files from a site with a nice collection of Halloween sound clips and placed in /home/pi/files as punkin_pi expects:

pi@raspberrypi ~ $ mkdir files

 

pi@raspberrypi ~ $ cd files

 

pi@raspberrypi ~/files $ wget http://www.countessbloodshalloweenhorror.com/sounds/howl.wav

 

pi@raspberrypi ~/files $ wget http://www.countessbloodshalloweenhorror.com/sounds/scream.wav

 

pi@raspberrypi ~/files $ wget http://www.countessbloodshalloweenhorror.com/sounds/ghostgigl.wav

 

Any files that mplayer can play can be put into /home/pi/files such as .wav, .mp3 & .ogg.

 

 

Install & run punkin_pi:

Next, I installed the punkin_pi software project via git:

pi@raspberrypi ~ $ git clone https://github.com/pdp7/punkin_pi.git

 

The web server (built on the bottle framework) can be started via:

pi@raspberrypi ~ $ cd punkin_pi


pi@raspberrypi ~/punkin_pi $ sudo python ./control.py

 

It will be available at the Pi's IP address on port 8081.  Here is a video of the web interface in action:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

(The LEDs happen to be connected to the Raspberry Pi via the Adafruit Pi Cobbler in this video clip as my Adafruit Pi Plate featured in my previous post wasn't handy at the time)

 

 

Audio troubleshooting:

If you want to check if punkin_pi will be able to play a particular file in /home/pi/files, then try to play it with mplayer:

mplayer /home/pi/files/howl.wav

Sometimes the sound system may become unstable and produce errors. Restarting ALSA should resolve this:

sudo /etc/init.d/alsa-utils restart

If your speakers lack a volume control, then the ALSA mixer can be used to adjust volume:

alsamixer

 

 

Cheers,

Drew

 

 

element14
Product Name*DescriptionBuy All Parts
Raspberry Pi Model B with SD Card Raspberry Pi model B and 8GB SD Card with NOOBS preinstalled
Optical mouse Basic USB optical mouse
Keyboard Basic USB keyboard
Adafruit Pi Plate Breakout and expansion board for Raspberry Pi
Tiny Breadboard Small breadboard sized to fit Pi Plate
Adafruit Pi Box Clear acrylic enclosure for Raspberry Pi
(2) NPN BJT NPN bipolar transistor
(2) 1k ohm resistor 1k ohm, 250mW carbon film resistor
(4) Red LED 5mm red LED
(4) 220 ohm resistor 220 ohm, 250mW carbon film resistor
(4) 180 ohm resistor 180 ohm, 250mW carbon film resistor
(4) Yellow LED 5mm yellow LED
20AWG Red Hook Up Wire 20AWG solid copper hook up wire - red
20AWG White Hook Up Wire 20AWG solid copper hook up wire – white
Additional Parts
Product Name*Description
Rechargeable USB Battery Pack4000 mAh Li-Ion battery pack with USB outputs and included cables
Mini SpeakerSmall rechargeable mono speaker with integrated amplifier

 

*Products and resources listed are listed to help members build their own Pi Projects. They are suggestions and listed for educational purposes. For substitutions of any parts, please post a question asking the original author.
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 13 years ago +2
    I am running an August 2012 Raspbian image. When I went to install the software for this, I found that when I got to the step to install "RPi.GPIO" the compile failed (couldn't find Python.h). I'm not…
  • fustini
    fustini over 13 years ago in reply to e14 Contributor +1
    Thanks for the tip! I'll add it to the instructions above and to the readme in the github repository.
  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Well, my soldering skills are suspect ;-), and I've not been able to blink a light yet. Guess the two us need to put our Pi's in the same pumpkin...I have sound and no lights, and you have lights and no…
  • fustini
    fustini over 13 years ago in reply to ralph_shade

    Hi Ralph, that is great to hear!  Merry Christmas to you, too!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralph_shade
    ralph_shade over 13 years ago

    It's a little late for Halloween image, but my board is now ready for next year!   Drew and Bonnie, thank you very much for all the work you put into this and for helping many of us bring our work to fruition.  This is the first project like this that I have tackled in, um..., 50 years.  Having it work was extremely gratifiying and should open me up to new hardware projects.

     

    Merry Christmas to all,

    Ralph

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 13 years ago in reply to e14 Contributor

    I'm very happy that the project interested you in the GPIO capabilities.  The circuit and software could definitely be adapted for other holiday displays.  The Pi is a great solution for adding web control to interactive lighting and sound.  The Raspberry Pi Foundation posted some other Pumpkin Pi projects earlier this week which might give you some more ideas, too: http://www.raspberrypi.org/archives/2282

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 13 years ago in reply to e14 Contributor

    Thanks for the tip.  What SD card image were you using?    I'm guessing there must be some additional package that was installed when I did "sudo apt-get install git-core mplayer python-setuptools" on the Raspbian 2012-09-18 image.  I also ran through my install instructions on new 2012-10-28 image last night, and wav files played ok with mplayer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I had the same problem:

    Playing howl.wav.

    libavformat version 53.21.0 (external)

    Mismatching header version 53.19.0

    Audio only file format detected.

     

    I disconnected hdmi, and downloaded some .mp3 files. Then "mplayer some.mp3", it works fine.

    So I removed all .wav files in the 'files' dir, and put some .mp3 files I found on internet, the web interface shows all .mp3 files, each with a button.

    Works fine.

    Hope it helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>