Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Cirrus Logic Audio Card 2015 Update
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 16 Jan 2015 3:12 PM Date Created
  • Views 5443 views
  • Likes 4 likes
  • Comments 62 comments
Related
Recommended
  • raspberry_pi
  • raspeberry_pi_accessories

Cirrus Logic Audio Card 2015 Update

e14 Contributor
e14 Contributor
16 Jan 2015

Introduction to the Cirrus Logic Audio Card

With the launch of the Model B+ there was one significant, yet highly appreciated change which meant the existing audio card with the P5 pogo pins was no longer compatible with the Model B+. This is a mechanical limitation and unfortunately it wasn't possible to find a neat solution for the existing card.

To deliver the same audio experience we have updated and created a new audio card for Model B+, called the Cirrus Logic audio card. For anyone who may have missed it Wolfson Microelectronics was acquired by Cirrus Logic in the summer of 2014, hence the name change for the audio card.

This short blog introduces the new Cirrus logic audio card and provides some background on hardware and software developments.

 

Hardware

From a hardware perspective if it isn't broke then don’t mess with it - that was the simple approach we took to the hardware design.

So the updated audio card uses the same core components (WM5102 and WM8804) and has the same core architecture as the original card. From a features perspective there is no significant change however we have listened to the feedback and made some minor improvements. This is mainly around a back powering option, changing the expansion header to 2.54mm pitch, increasing the expansion header to make the unused GPIO pins from the Raspberry Pi accessible and adding the option to connect external stereo ECM microphones to the line input.  

This ensures that users can experience the same high quality audio experience using Model B / B+ or A+.

 

Please refer to the table on the main Cirrus Audio card community page, this provides a good summary of the feature comparison between cards.

 

The key take away on hardware is that the same primary functions remain on both audio cards with only minor changes in hardware design.

 

Software

From a software perspective we continue to update and improve.

Firstly the software for Model B and Model A+/B+ is exactly the same, automatic detection and pin mapping is included so there is no need for different compiled software kernels for the two boards. You can use the Cirrus 3.12 kernel image on either the Wolfson or Cirrus boards with no manual configuration or setup required.

 

What is currently available from a software perspective

  • A Raspbian image is available for download from the E14 community website using kernel 3.12. This will support the Model B,  B+ and A+ using either the Wolfson or Cirrus audio cards.
  • We have also published our source code for the 3.12 kernel on our own newly created github repository. You can find details and the source code here - https://github.com/CirrusLogic/rpi-linux/wiki

 

From the existing Raspberry Pi pull request we received good feedback on issues that users discovered, we have where possible addressed the issues and these are incorporated in the Cirrus github.


With regards to upstreaming into the Raspberry Pi kernel and in particular Kernel 3.12, we have encountered issues relative to how the kernel operates when the card is not connected, there are also issues which impact other audio cards. We have tried to find a solution to this but unfortunately the effort is not insignificant and reaches further than our own drivers. Therefore we are currently unable to support inclusion into the official Raspberry Pi 3.12 kernel.

We have discussed this with the maintainer and he is in support of this limitation and also with regards to our plans going forward.

 

What is our current plan going forward

Integration into the Raspberry pi kernel and in turn the Raspbian distribution remains our end goal. With the issues we have encountered integrating into the 3.12 kernel we are now focusing our efforts on integration to the latest kernel (3.18). The 3.18 kernel in particular adds support for device tree, this in turn provides support for add on modules and in particular will allow the issues with multiple I2S audio cards in 3.12 to be addressed. The Raspberry Pi kernel is planning to move from the current 3.12 kernel in the future so this provides an opportunity to add future support as part of the standard distribution.

 

 

There are now two audio cards available for the appropriate model of Raspberry Pi, both cards use the same software and most importantly both will deliver the same HD audio experience for both capture and playback.

 

We hope you find the new audio card a worthwhile addition to your Raspberry Pi Model B+ experience.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +1
    It's unfortunate that we all have to engage in wishful thinking when it comes to looking for driver updates. Right now we're all scouring the internet, hoping to find things like updated drivers, better…
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor +1
    bob p wrote: It's CirrusLogic's responsibility to fix their hardware/software problems. A minor point, but legally, that is likely not the case in most jurisdictions. I guess you mean some moral responsibility…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to timg73

    Here you can find all the changes. With this you can make your own patch files. But please don't publish them. This should be the work of the engineers of Cirrus Logic. Don't do their job.

     

    https://github.com/CirrusLogic/rpi-linux/compare/raspberrypi:rpi-3.12.y...rpi-3.12.y

    Have fun.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • timg73
    timg73 over 11 years ago in reply to e14 Contributor

    To the best of my knowledge the Cirrus audio card does not work with the RPi 2B, contrary to the information in the Farnell catalogue.  This is because the only kernel available for the RPi 2B is v3.18 and Cirrus Logic have not yet released a patch-set for that kernel.  We can hope that the RPi 2B will be supported if/when the patches promised above are released.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to fujg1980

    Have you got the card working with the Pi 2? I've got one of the new 2 B models, and not had any luck with the Cirrus card. Hmm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks Andrew. Yes, someone else mentioned Runeaudio and told me they'd got it working with the Cirrus card and were impressed by its interface. I must take a look. I've had the hardware nearly a fortnight now, and not yet found time to have a proper play with it - and I'm supposed to be retired!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Although not exactly what you are looking for, have you tried Runeaudio.  I currently have it working with my Raspberry pi and Wolfson audio card.  I spent some time working with Volumio, but found Runeaudio much easier to configure and the folks in the forum are very helpful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>