• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Essential Raspberry Pi Peripherals #2 (annex 2): 7" LCD touch screen display installation notes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 1 Oct 2015 2:30 PM Date Created
  • Views 4411 views
  • Likes 3 likes
  • Comments 20 comments
Related
Recommended
  • tutorial
  • installation_note
  • raspberry-pi2
  • touch_screen
  • raspberry_pi
  • setup
  • raspberry-pi
  • lcd_screen
  • 7_inches_touch_screen_display
  • configuration

Essential Raspberry Pi Peripherals #2 (annex 2): 7" LCD touch screen display installation notes

balearicdynamics
balearicdynamics
1 Oct 2015

Introduction

image

There is a considerable number of places on the Internet, including the Element14 site, showing useful information on the installation and settings of this brand new device; in the meantime a number of doubts and questions has raised about the touch screen settings, the on-screen keyboard installation and more. The goal of these notes is to depict a setup scenario as much complete as possible. The Raspberry PI 7" LCD Touch Screen display is the perfect replacement of a dedicated screen, with the plus of the optional on-screen keyboard.

 

To use this device in a Raspberry PI project requiring User Interaction it sounds almost difficult in applications like robotics, machines control, informative point, web access, sensors gauges etc.

A reliable solution exists and its name is Kivy: open source, not too difficult to install and is based on Python.

 

Note: the frame assembly of the Raspberry PI LCD Touch Screen display shown in the images of this post is available on the Drobott site. Don't forget to apply the Element14 discount code W0E49MYQ (10% off) reserved to the community users!

 

What raspbian release?

image

The first thing to do it to decide what raspbian image should be installed on the PI. If you have already a Raspberry PI with an existing raspbian version on it, you should install the hardware then power on the system and proceed with the software.

 

If you should start from scratch instead, I suggest to download the last raspbian updated image (2015-05-05-raspbian-wheezy.img at the date) from the raspberry.org site to create a bootable microSD card; you  can choose between two different flavours: raspbian based on Debian wheezy or Debian jessie; this choice is up to you. At the actual date it seems that the Raspberry PI porting of the Jessie distribution has again some issues.

 

In both cases, the next step is an update/upgrade of the system.

 

$sudo apt-get update
$sudo apt-get upgrade
         

 

You should have noted that the system, also on first-boot will recognise the new display device without any special setting or display drivers to be installed.

 

Showing full HD videos on the screen

If you plan to use the screen to show full HD videos (1080x1920 pix) the better performances can be obtained reserving 128 Mb of shared memory to the video card. The amount of shared memory (64 Mb by default) can be changed with the raspi-config command and selecting the menu options shown below.

image

Select Advanced Options from the main menu.

image

Select Memory Split from the next screen.

image

Then, write 128 instead of 64 (the default settings). Confirm and exit, reboot.

 

On-Screen keyboard

Installing the on-screen keyboard is not the solution to develop software or write long text documents on the Raspberry PI, but it is a must-to-have to make complete the user interaction options. Installing the keyboard is a very simple operation that can be done with a single command from the terminal:

 

sudo apt-get install matchbox-keyboard
      

 

just as it is explained in the product document page on Element14. The documentation says that the keyboard (after installation and reboot) is accessible on-screen from the Menu->Accessories->Keyboard. Doing several installations I have verified that the keyboard is not always listed as a new menu option; one of the reasons depends on the previous presence of a physical keyboard connected to the Raspberry or not. To be sure that the on-screen keyboard is added to the desktop menu after installation the better choice is to manage the Raspberry PI from remote via SSH.

 

The on-screen keyboard can be shown by your applications or bash scripts with the command

 

matchbox-keyboard
     

 

Enabling the touch-screen

Depending on the current status of the linux settings, maybe you don't see the mouse pointer on the screen and the touch screen is unresponsive; the touch screen uses SPI to communicate with the Raspberry PI so it should be enabled, while by default the SPI kernel modules are not loaded.

 

From the terminal launch the command

 

sudo raspi-config
    

 

then from the character graphic menu follow the steps shown below.

image

Select Advanced Options from the main menu.

image

Select the SPI menu option.

image

Confirm to enable the SPI module and the next screen to load the SPI kernel modules on boot by default. Then, exit and reboot the system.

 

Congratulations!

Now your system is ready to use the full features of the 7 inches LCD display and touch screen.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 11 years ago +1
    That bezel and stand look really good! The gloss/slightly translucent white finish looks nicer than the default black border! I did wonder why the official RPI case was one style, and the official 7" screen…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to shabaz +1
    Thank you Shabaz! Maybe because the previous designer was fired ? BTW, this support has been designed by me with the specific aim to solve the problem when - in some cases - the touch slide scroll down…
  • shabaz
    shabaz over 11 years ago in reply to balearicdynamics +1
    Looks like two-week lead-time currently : (
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to fvan

    I have tested on PI2 and it works perfectly. The documentation of Kivy is not complete and a bit outdated.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago in reply to balearicdynamics

    I tried the A+, because the Kivy website stated that it hadn't been tested with the Pi 2, but worked properly on the original A/B. Not sure how they managed to install Cython, unless something's wrong with my A+ ...

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to fvan

    Was ok the tutorial? I wrote it following the installation and I hope I have not forgot something.

    If go out of memory installing I have serious doubts to see it running on A image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago in reply to balearicdynamics

    Kivy is finally installed on the Pi2. On the A+, the Cython installation would hang as the Pi ran out of memory and desperately started swapping.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to fvan

    That is should happen (IMO, as far as I see, that is the right orientation. I saw this happening on a old version of the Raspbian also after setting the SPI on the raspi-config.

     

    I have found no doc on the Internet about... Too simple things come complex without explanation why are so simple image Satisfact of this new device? Try with Kivy, it's incredible!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>