Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Quick SD to SSD on the pi 4
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gam3t3ch
  • Date Created: 30 Aug 2019 3:54 PM Date Created
  • Views 14280 views
  • Likes 11 likes
  • Comments 12 comments
Related
Recommended

Quick SD to SSD on the pi 4

gam3t3ch
gam3t3ch
30 Aug 2019

See quite a few tutorials on hooking up a hard drive to the pi for and just want to give my quick and easy version cause I tried a few and they didn't work.

 

 

install buster on sd card :  https://www.raspberrypi.org/downloads/

 

insert into your pi and boot up do the first time setup and updates.

 

plug in your ssd drive

 

go to the pi menu and then to accessories

image

click on SD Card copier

 

copy from device:  your SD Card

copy to device:      your ssd or hdd

 

image

 

Before clicking on start make sure you check the box to create New Partition UUIDs

 

once complete close that out.

 

Open terminal:  ctrl+alt+t

 

type sudo blkid

 

image

 

open another terminal:  ctrl+alt+t

 

first we want to back up the cmdline.txt file just in case it doesn't work we

can take it back to our computer and re-enable the working one.

 

sudo cp /boot/cmdline.txt /boot/cmdline.txt.bak

 

type: sudo nano /boot/cmdline.txt

 

So now we are going to look at the "PARTUUID="somenumbers"

 

now in the terminal you typed in the other window you should see 2 rootfs

one should be the same as in the cmdline.txt file grab the one from sda1 or sda2 with

the label rootfs.

 

image

 

replace the cmdline.txt with the new uuid

 

hit ctrl+x then press y hit enter

 

type sudo reboot

 

once booted up open your file folder the yellow file and look in the bottom right and see

if its picked up your ssd or hdd should show the size you may have to adjust volume sizes.

 

That's it you should be now running on the ssd or usb storage drive.

 

---------------------------------------------------------------

update:

So I finally got around to doing a video on it.  Now bear with me its certainly interesting recording and editing on the raspberry pi 4 but I managed to get through it will have to update my other post about using the pi 4 as a desktop in my other blog post.   takes just over a hour to render a 10 minute video but its doable.  getting the setting and codecs correct took some time tho. I think it took me about 2 days to finally get everything edited and uploaded.  But now I have the process down next time it won't take so long.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • gam3t3ch
    gam3t3ch over 6 years ago in reply to clem57 +3
    From what I read before out of the box only pi3 and lower versions were able to do so. I think at some point they will update this like they did for those versions. I have my ssd on the usb 3.0 connection…
  • gam3t3ch
    gam3t3ch over 6 years ago in reply to grondak +2
    Thanks grondak I got some cool pi stuff in the works so lots more tips and tricks will be coming soon.
  • grondak
    grondak over 6 years ago +1
    My SSD was auto-resized as I finished this operation. Thank you gam3t3ch !
  • gam3t3ch
    gam3t3ch over 6 years ago in reply to clem57

    From what I read before out of the box only pi3 and lower versions were able to do so.   I think at some point they will update this like they did for those versions. 

    I have my ssd on the usb 3.0 connection and wow its night and day I was confused why my pi3 with ssd was running better then the pi4 and it was 100% the SD card

    causing the slow down.  So upgraded and ran some benchmarks now I am happy with the outcome.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 6 years ago

    gam3t3ch understand using it storage, but is there an option to boot from the SSD? That would be great given the new USB 3.0 connection.

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<