Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog RP2040 SD Card SPI Benchmark
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 17 Mar 2022 4:43 AM Date Created
  • Views 15144 views
  • Likes 10 likes
  • Comments 9 comments
Related
Recommended
  • rp2040
  • sd-card

RP2040 SD Card SPI Benchmark

ralphjy
ralphjy
17 Mar 2022

When I posted earlier about the SparkFun RP2040 mikroBUS Development Board for Happy Pi Day, DAB had mentioned that he was curious as to the SD card size and write rates.

I have to admit that I've never run a speed test on an SD card setup with a microcontroller.  

image

I'm going to do a quick test using the method that I normally use - the SPI interface with the Arduino SDFat library.  The library includes a simple write/read benchmark example.  Unfortunately, SparkFun doesn't have a dedicated Board library for this board, so I am going to use the Raspberry Pi Pico Mbed library and modify the SPI pins in the variant.h file.

For this test I'm using a SanDisk Ultra 16GB UHS-I card rated at a max speed of 80MB/s.  The SPI interface will be substantially slower than that.  The SPI Clock frequency in the program is set to 50MHz.

Here is the program for reference:
RP2040_MikroBUS_SDcard_bench.ino

/*
 * This program is a simple binary write/read benchmark.
 */
#include "SdFat.h"
#include "sdios.h"
#include "FreeStack.h"

// SD_FAT_TYPE = 0 for SdFat/File as defined in SdFatConfig.h,
// 1 for FAT16/FAT32, 2 for exFAT, 3 for FAT16/FAT32 and exFAT.
#define SD_FAT_TYPE 0
/*
  Change the value of SD_CS_PIN if you are using SPI and
  your hardware does not use the default value, SS.
  Common values are:
  Arduino Ethernet shield: pin 4
  Sparkfun SD shield: pin 8
  Adafruit SD shields and modules: pin 10
*/
// SDCARD_SS_PIN is defined for the built-in SD on some boards.
#ifndef SDCARD_SS_PIN
const uint8_t SD_CS_PIN = SS;
#else  // SDCARD_SS_PIN
// Assume built-in SD is used.
const uint8_t SD_CS_PIN = SDCARD_SS_PIN;
#endif  // SDCARD_SS_PIN

// Try max SPI clock for an SD. Reduce SPI_CLOCK if errors occur.
#define SPI_CLOCK SD_SCK_MHZ(50)

// Try to select the best SD card configuration.
#if HAS_SDIO_CLASS
#define SD_CONFIG SdioConfig(FIFO_SDIO)
#elif ENABLE_DEDICATED_SPI
#define SD_CONFIG SdSpiConfig(SD_CS_PIN, DEDICATED_SPI, SPI_CLOCK)
#else  // HAS_SDIO_CLASS
#define SD_CONFIG SdSpiConfig(SD_CS_PIN, SHARED_SPI, SPI_CLOCK)
#endif  // HAS_SDIO_CLASS

// Set PRE_ALLOCATE true to pre-allocate file clusters.
const bool PRE_ALLOCATE = true;

// Set SKIP_FIRST_LATENCY true if the first read/write to the SD can
// be avoid by writing a file header or reading the first record.
const bool SKIP_FIRST_LATENCY = true;

// Size of read/write.
const size_t BUF_SIZE = 512;

// File size in MB where MB = 1,000,000 bytes.
const uint32_t FILE_SIZE_MB = 5;

// Write pass count.
const uint8_t WRITE_COUNT = 2;

// Read pass count.
const uint8_t READ_COUNT = 2;
//==============================================================================
// End of configuration constants.
//------------------------------------------------------------------------------
// File size in bytes.
const uint32_t FILE_SIZE = 1000000UL*FILE_SIZE_MB;

// Insure 4-byte alignment.
uint32_t buf32[(BUF_SIZE + 3)/4];
uint8_t* buf = (uint8_t*)buf32;

#if SD_FAT_TYPE == 0
SdFat sd;
File file;
#elif SD_FAT_TYPE == 1
SdFat32 sd;
File32 file;
#elif SD_FAT_TYPE == 2
SdExFat sd;
ExFile file;
#elif SD_FAT_TYPE == 3
SdFs sd;
FsFile file;
#else  // SD_FAT_TYPE
#error Invalid SD_FAT_TYPE
#endif  // SD_FAT_TYPE

// Serial output stream
ArduinoOutStream cout(Serial);
//------------------------------------------------------------------------------
// Store error strings in flash to save RAM.
#define error(s) sd.errorHalt(&Serial, F(s))
//------------------------------------------------------------------------------
void cidDmp() {
  cid_t cid;
  if (!sd.card()->readCID(&cid)) {

    error("readCID failed");
  }
  cout << F("\nManufacturer ID: ");
  cout << hex << int(cid.mid) << dec << endl;
  cout << F("OEM ID: ") << cid.oid[0] << cid.oid[1] << endl;
  cout << F("Product: ");
  for (uint8_t i = 0; i < 5; i++) {
    cout << cid.pnm[i];
  }
  cout << F("\nVersion: ");
  cout << int(cid.prv_n) << '.' << int(cid.prv_m) << endl;
  cout << F("Serial number: ") << hex << cid.psn << dec << endl;
  cout << F("Manufacturing date: ");
  cout << int(cid.mdt_month) << '/';
  cout << (2000 + cid.mdt_year_low + 10 * cid.mdt_year_high) << endl;
  cout << endl;
}
//------------------------------------------------------------------------------
void clearSerialInput() {
  uint32_t m = micros();
  do {
    if (Serial.read() >= 0) {
      m = micros();
    }
  } while (micros() - m < 10000);
}
//------------------------------------------------------------------------------
void setup() {
  Serial.begin(115200);

  // Wait for USB Serial
  while (!Serial) {
    yield();
  }
  delay(1000);
  cout << F("\nUse a freshly formatted SD for best performance.\n");
  if (!ENABLE_DEDICATED_SPI) {
    cout << F(
      "\nSet ENABLE_DEDICATED_SPI nonzero in\n"
      "SdFatConfig.h for best SPI performance.\n");
  }
  // use uppercase in hex and use 0X base prefix
  cout << uppercase << showbase << endl;
}
//------------------------------------------------------------------------------
void loop() {
  float s;
  uint32_t t;
  uint32_t maxLatency;
  uint32_t minLatency;
  uint32_t totalLatency;
  bool skipLatency;

  // Discard any input.
  clearSerialInput();

  // F() stores strings in flash to save RAM
  cout << F("Type any character to start\n");
  while (!Serial.available()) {
    yield();
  }
#if HAS_UNUSED_STACK
  cout << F("FreeStack: ") << FreeStack() << endl;
#endif  // HAS_UNUSED_STACK

  if (!sd.begin(SD_CONFIG)) {
    sd.initErrorHalt(&Serial);
  }
  if (sd.fatType() == FAT_TYPE_EXFAT) {
    cout << F("Type is exFAT") << endl;
  } else {
    cout << F("Type is FAT") << int(sd.fatType()) << endl;
  }

  cout << F("Card size: ") << sd.card()->sectorCount()*512E-9;
  cout << F(" GB (GB = 1E9 bytes)") << endl;

  cidDmp();

  // open or create file - truncate existing file.
  if (!file.open("bench.dat", O_RDWR | O_CREAT | O_TRUNC)) {
    error("open failed");
  }

  // fill buf with known data
  if (BUF_SIZE > 1) {
    for (size_t i = 0; i < (BUF_SIZE - 2); i++) {
      buf[i] = 'A' + (i % 26);
    }
    buf[BUF_SIZE-2] = '\r';
  }
  buf[BUF_SIZE-1] = '\n';

  cout << F("FILE_SIZE_MB = ") << FILE_SIZE_MB << endl;
  cout << F("BUF_SIZE = ") << BUF_SIZE << F(" bytes\n");
  cout << F("Starting write test, please wait.") << endl << endl;

  // do write test
  uint32_t n = FILE_SIZE/BUF_SIZE;
  cout <<F("write speed and latency") << endl;
  cout << F("speed,max,min,avg") << endl;
  cout << F("KB/Sec,usec,usec,usec") << endl;
  for (uint8_t nTest = 0; nTest < WRITE_COUNT; nTest++) {
    file.truncate(0);
    if (PRE_ALLOCATE) {
      if (!file.preAllocate(FILE_SIZE)) {
        error("preAllocate failed");
      }
    }
    maxLatency = 0;
    minLatency = 9999999;
    totalLatency = 0;
    skipLatency = SKIP_FIRST_LATENCY;
    t = millis();
    for (uint32_t i = 0; i < n; i++) {
      uint32_t m = micros();
      if (file.write(buf, BUF_SIZE) != BUF_SIZE) {
        error("write failed");
      }
      m = micros() - m;
      totalLatency += m;
      if (skipLatency) {
        // Wait until first write to SD, not just a copy to the cache.
        skipLatency = file.curPosition() < 512;
      } else {
        if (maxLatency < m) {
          maxLatency = m;
        }
        if (minLatency > m) {
          minLatency = m;
        }
      }
    }
    file.sync();
    t = millis() - t;
    s = file.fileSize();
    cout << s/t <<',' << maxLatency << ',' << minLatency;
    cout << ',' << totalLatency/n << endl;
  }
  cout << endl << F("Starting read test, please wait.") << endl;
  cout << endl <<F("read speed and latency") << endl;
  cout << F("speed,max,min,avg") << endl;
  cout << F("KB/Sec,usec,usec,usec") << endl;

  // do read test
  for (uint8_t nTest = 0; nTest < READ_COUNT; nTest++) {
    file.rewind();
    maxLatency = 0;
    minLatency = 9999999;
    totalLatency = 0;
    skipLatency = SKIP_FIRST_LATENCY;
    t = millis();
    for (uint32_t i = 0; i < n; i++) {
      buf[BUF_SIZE-1] = 0;
      uint32_t m = micros();
      int32_t nr = file.read(buf, BUF_SIZE);
      if (nr != BUF_SIZE) {
        error("read failed");
      }
      m = micros() - m;
      totalLatency += m;
      if (buf[BUF_SIZE-1] != '\n') {

        error("data check error");
      }
      if (skipLatency) {
        skipLatency = false;
      } else {
        if (maxLatency < m) {
          maxLatency = m;
        }
        if (minLatency > m) {
          minLatency = m;
        }
      }
    }
    s = file.fileSize();
    t = millis() - t;
    cout << s/t <<',' << maxLatency << ',' << minLatency;
    cout << ',' << totalLatency/n << endl;
  }
  cout << endl << F("Done") << endl;
  file.close();
}

Here is the Serial Console output:

image

So, looks like write and read are about 140KB/s.  The SD card interface is wired for SDIO, so that may be an option if I need more speed in the future.  I haven't used SDIO yet, but I think the current library available for it is 4 bit read and 1 bit write.

image

  • Sign in to reply
  • LeScherd
    LeScherd over 4 years ago

    Hi,
    I ran similar tests a few months ago using the MBed Arduino core, the MBed SDFat lbrary and the standard SPI pins MISO 4, MOSI 3, SCK 2 and CS 5.
    I set the SPI clock to 30MHz.
    The results I got were significantly faster:
    PicoPi 125MHz clock: W/R: 1450.54 KB/s / 1249.06 KB/s
    PicoPi 250MHz clock: W/R: 1938.74 KB/s / 1774.31 KB/s
    I didn't write down my results for the Philhower core... I must have run into issues.
    I would be willing to try to set this experiment up again if you are interested.
    I was never able to figure out a way to get SDIO working within the Arduino environment.
    Thanks, Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • LeScherd
    LeScherd over 4 years ago

    Hi,

    A couple of months ago I ran a similar test using the Arduino Mbed core and SDFat library, using the standard MBed SPI pins: MISO 4, MOSI 3, SCK 2, CS 5.

    I set the SPI clock rate at 30MHz.

    I got the following data rates:

    125MHz (PicoPi clock): W/R: 1450.54 KB/s / 1249.06 KB/s

    250MHz clock: W/R: 1938.74 KB/s / 1774.31 KB/s

    I would be willing to set up the experiment again to see if I get the same results. These results seem significantly faster than what you got... and I don't know why.

    I never figured out how to implement SDIO in the Arduino environment, I would be very interested in hearing about that.

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 4 years ago

    Cool experiment. I wonder if it is possible to calculate.

    140KB/s = 1,120kbits/s or 1.12 Mbits/s which is a long way from 50 Mbits/s. So how to calculate the overhead? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 4 years ago

    Thank you for running the test.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<