Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Win a Raspberry Pi 5 from the element14 Community!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 28 Sep 2023 6:24 AM Date Created
  • Views 25576 views
  • Likes 17 likes
  • Comments 251 comments
Related
Recommended
  • competition
  • raspberry pi 5
  • raspberry pi 5 giveaway
  • win a raspberry pi 5

Win a Raspberry Pi 5 from the element14 Community!

e14phil
e14phil
28 Sep 2023

image

Win a Raspberry Pi 5!

We have just announced the release of the amazing Raspberry Pi 5, with its 2.4GHz quad-core, 64-bit Arm Cortex-A76 CPU, VideoCore VII GPU, LPDDR4X-4267 SDRAM (4GB and 8GB SKUs available at launch), 2.4 GHz and 5.0 GHz 802.11ac Wi-Fi, and Bluetooth 5.0 / Bluetooth Low Energy (BLE).

This Competition is now Closed.

Congratulations JWx our team has selected you as the winner of our Raspberry Pi 5 Give away!
We hope to see your experiments with the PCI-E functionality.  
/products/raspberry-pi/b/blog/posts/win-a-raspberry-pi-5-from-element14-community?CommentId=0f1e6de3-ee46-457b-bc91-71acc33df059 

Check out our Raspberry Pi 5 announcement blog here:

 Introducing The New Raspberry Pi 5 - 3x Faster, 2.4GHz, VideoCore VII GPU, RTC, Gigabit Ethernet, 1GB, 2GB, 4GB, 8GB RAM  

If you would like to win a Raspberry Pi 5, all we want to know is ... "What would you build with a Raspberry Pi 5?"

How to Enter:

Comment on this blog below, answering the question: What ould you build with a Raspberry Pi 5? We will send our favorite commenter a Raspberry Pi 5.

End Date: 30th November 2023 at 23:59 

Click here for Terms & Conditions.

Note: When selecting winners, if we discover that your name and address details are not correct on your Community account profile, we will choose a different winner.

Make sure your profile information is correct and up to date.

  • Sign in to reply

Top Comments

  • misaz
    misaz over 3 years ago +4
    In last years I used most time used Raspberry Pi for some kind of long-term automation. For example, last few months two of my Raspberry Pies was running experiments (one Rpi 4B and one 3B+) to evaluate…
  • ItsZephyrOne
    ItsZephyrOne over 3 years ago +3
    I already have a Raspberry Pi Zero; I tried desktop on it, but Zero doesn't have processing power, which is why I need a Raspberry Pi 5.
  • draq357
    draq357 over 3 years ago +3
    I would probably set this up as a server to receive weather information, and display it on a smart mirror. It would get weather info from the home built station in my backyard.
  • Hrichik
    Hrichik over 3 years ago

    I plan to build an autonomous submarine with initial guidance taking weather measurements with intervals, with the RPI 5's processing capabilities, it would be able to achieve such a feat. Also, it could run AI models and send data with much more information, such as trash belts, chemical levels, wave turbulence, etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Sol5689
    Sol5689 over 3 years ago

    I would finish porting some OpenFrameworks (C++) sketches and use it to control two other RPIs with small e-paper displays, synchronized via BLE. These are running a generative art system which is neither converting nor diverging based on particles flowing in a perturbed noise field. Each particle is an agent, with a specific behaviour, trying to be near other particles, but not too near, and if by chance they get propelled to near, they randomly explode outwards, similar to flocking behaviour. The system updates slowly, so the e-paper display is perfectly suitable. BLE synchronizes the framed displays - think of a painting or an engraving, in a wood frame, but slowly mutating, with the center "painting" getting input via its camera (placed strategically so as to not be too visible), and warping the noise field upon which the particles flow. No sound yet, i'm unsure if to add sound. It's a demanding task. Now with FLOSS drivers perhaps i could add (a LOT) more particles via Vulkan. The RP1 chip dealing with I/O seems to be promising to alleviate the CPU workload, so the Bluetooth BLE being handled separately would be good. The system seems more CPU bound that RAM bound, but of course, 8GB, 2 per core, would be great. Perhaps assigning cgroups to make 2 virtual "nodes", one pinned to the system, and the others to the user tasks would, specially with the new CPU, could allow more finer grained flow and noise fields. So many possibilities to explore....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelsit91
    michaelsit91 over 3 years ago

    Low Latency audio router, using hifiberry to send PC audio input to multiple endpoints simultaneously

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • huntz47
    huntz47 over 3 years ago

    Ooooh yeah.
    its Finally here.
    I am building an exoskeleton suit which is capable of defending the user from any kind of attacks.
    also it can be used by anyone, whether they are disabled or not. It will be just like the Tuxedo suit. you dnt have to do
    Anything. all my software part is complete. all i need is the RPI5.
    I have been Waiting for This one. I was using my laptop to test my codes. Now i dont have to worry anymore.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Diveshdon
    Diveshdon over 3 years ago

    Considering the power of pi 5 with cryptograpic support I would like to make a all in one open source AI powered home assistant hub with touch screen & camera, mediacenter for locally stored music video playback on tv, all using llama language model for interaction and control all smart devices with voice assistant locally inside the network, improved home network security & local DNS. with the help of high speed i/o support & power full SoC with LPDDR4x ram, i think all things can works smoothly and a scope of incuding more functionality with upcoming pcie 2.0 peripherals. Hope my dreams come true.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>