Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Evaluate GNU Radio application performance on Pi4(2G)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 40 replies
  • Subscribers 703 subscribers
  • Views 10201 views
  • Users 0 members are here
  • raspberry_pi
Related

Evaluate GNU Radio application performance on Pi4(2G)

colporteur
colporteur over 6 years ago

The results after using a Raspberry Pi 3B+ to run a GNU Radio flow graph were unacceptable. The audio outputed from the Pi was distorted. I speculate the SBC doesn't have the performance specification to support GNU Radio.

 

I am trying to determine if the Raspberry Pi (version ?) is capable of supporting a GNU Radio flow graph. My current assessment is no. The hardware performance is not sufficient to handle the digital signal processing requirements.

 

It was suggested I make a forum post while some testing was done, so other interested could follow.

 

My objective was to write a tutorial for the GNU Radio application using a Raspberry Pi. After successfully building two GNU Radio flow graphs on my Ubuntu 18.04 i7 processor desktop, I ported the flow graphs to a Pi3B+ connected to an HDMI with audio monitor. One flow graph is an audio signal generator outputed to a speaker. The second is an FM receiver. Both flow graphs work in the sense they produce audio but with distortion and in the case of FM broadcast, unreadable.

 

The audio flow graph requires a GNU Radio software installation. The FM flow graph requires an SDR dongle to gather a broadcasted signal to feed the GNU Radio FM radio receiver flow graph. The test will be using the audio flow graph since no additional hardware is required.

 

image

cstanton  has agreed to use his Pi4(2G) to run the test. Before starting the exercise, I will ask Christopher to review review the procedures and provide feedback. I'm keeping the the verbiage terse, assuming a higher level of understanding. If more details are required or feel something is more appropriate or missing please let me know.

 

A zip file of two flow graphs is attached. The file with basic is minimal as it gets. The second file provides a test module. I experienced a problem with both.

 

 

Test Procedure:

Fresh install of Raspbian Buster Full, current release.

Apply O/S updates/upgrades & Install GNU Radio

 

///CODE START///

sudo apt-get update -y;sudo apt-get upgrade -y

sudo reboot

sudo apt-get install gnuradio

///CODE END///

 

Take screen shots of htop screen at the following milestones.

1. O/S idle, no application running on the GUI desktop other than what is defaulted.

2. GNU Radio started, no flow graph

3. GNU Radio flow graph loaded.

4. GNU Radio flow graph started.

5. Evaluate audio coming from speaker and advise.

 

Depending on results, i would like to expand the test Ginny pig agreed.

 

Sean

 

Message was edited by: sean conway I have uploaded the two audio flow graphs for GNU Radio. The current version of GNU Radio encourages development in QT widgets verses the WX widgets. Three is discussion in the community support for WX will disappear. The flow graphs provided are QT. Sean

Attachments:
gnuradio.zip
gnuradio_FM.zip
  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    Gough Lui over 6 years ago

    I have not tried it, but the Pi is relatively low powered so I wouldn't be surprised if there were issues.

     

    One suggestion I have is to use a sample rate of 48kHz as many sound cards and outputs expect 48kHz output. Feeding in lower sample rates sometimes will resample correctly, but other times not, resulting in crackles and underflow (i.e. U being printed in the console).

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to Gough Lui

    Interesting observations today. GNU Radio audio flow graph worked! I used an existing Pi setup with bluetooth speakers and the GNU Radio audio flow graph shown worked. No distortion. No intermittent audio. What changed?

     

    The issue may be related to audio configuration.

    • GNU Radio installation by itself will error out trying to run a flow graph. The error message suggests something to do with ALSA configs.
    • Installing gqrx enables GNU Radio flow graphs to work but audio distorted.
    • GNU Radio installation with bluetooth speaker configured, flow graphs work and audio not distorted.

     

    Raspbian Buster has made big strides with Buster in fixing bluetooth issues. One major leap is integration to ALSA using bluealsa services. I used a Pi install that had bluetooth speakers configured as part of another project. I merely used the install to test GNU Radio and discovered it worked.

     

    gam3t3ch did a post Alsa no audio (glitch) issue Pi 4 fix to share his process for resolving audio issues. The post discusses ALSA and how configuration appear to change as software is installed. The order of software installs is what twigged me to a possible audio issue with GNU Radio.

     

    I'm not sure my supposition that a Pi lacks the performance to support GNU Radio is valid. It appears the audio distortion issue is related to Pi's audio configuration and not performance. Further investigation is required.

     

    cstanton Christopher if you are monitoring this post, be aware of these findings before starting your Pi4 testing. I expect the instructions provided will give you a GNU Radio install that fails to run the flow graph because of ALSA issue. I haven't resolved that issue only I stumbled on the work around to get it working using bluetooth.

     

    Sean

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 6 years ago in reply to Gough Lui

    Interesting observations today. GNU Radio audio flow graph worked! I used an existing Pi setup with bluetooth speakers and the GNU Radio audio flow graph shown worked. No distortion. No intermittent audio. What changed?

     

    The issue may be related to audio configuration.

    • GNU Radio installation by itself will error out trying to run a flow graph. The error message suggests something to do with ALSA configs.
    • Installing gqrx enables GNU Radio flow graphs to work but audio distorted.
    • GNU Radio installation with bluetooth speaker configured, flow graphs work and audio not distorted.

     

    Raspbian Buster has made big strides with Buster in fixing bluetooth issues. One major leap is integration to ALSA using bluealsa services. I used a Pi install that had bluetooth speakers configured as part of another project. I merely used the install to test GNU Radio and discovered it worked.

     

    gam3t3ch did a post Alsa no audio (glitch) issue Pi 4 fix to share his process for resolving audio issues. The post discusses ALSA and how configuration appear to change as software is installed. The order of software installs is what twigged me to a possible audio issue with GNU Radio.

     

    I'm not sure my supposition that a Pi lacks the performance to support GNU Radio is valid. It appears the audio distortion issue is related to Pi's audio configuration and not performance. Further investigation is required.

     

    cstanton Christopher if you are monitoring this post, be aware of these findings before starting your Pi4 testing. I expect the instructions provided will give you a GNU Radio install that fails to run the flow graph because of ALSA issue. I haven't resolved that issue only I stumbled on the work around to get it working using bluetooth.

     

    Sean

    • Cancel
    • Vote Up +3 Vote Down