• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Raspberry Pi Forum Evaluate GNU Radio application performance on Pi4(2G)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 40 replies
  • Subscribers 703 subscribers
  • Views 10232 views
  • Users 0 members are here
  • raspberry_pi
Related

Evaluate GNU Radio application performance on Pi4(2G)

colporteur
colporteur over 6 years ago

The results after using a Raspberry Pi 3B+ to run a GNU Radio flow graph were unacceptable. The audio outputed from the Pi was distorted. I speculate the SBC doesn't have the performance specification to support GNU Radio.

 

I am trying to determine if the Raspberry Pi (version ?) is capable of supporting a GNU Radio flow graph. My current assessment is no. The hardware performance is not sufficient to handle the digital signal processing requirements.

 

It was suggested I make a forum post while some testing was done, so other interested could follow.

 

My objective was to write a tutorial for the GNU Radio application using a Raspberry Pi. After successfully building two GNU Radio flow graphs on my Ubuntu 18.04 i7 processor desktop, I ported the flow graphs to a Pi3B+ connected to an HDMI with audio monitor. One flow graph is an audio signal generator outputed to a speaker. The second is an FM receiver. Both flow graphs work in the sense they produce audio but with distortion and in the case of FM broadcast, unreadable.

 

The audio flow graph requires a GNU Radio software installation. The FM flow graph requires an SDR dongle to gather a broadcasted signal to feed the GNU Radio FM radio receiver flow graph. The test will be using the audio flow graph since no additional hardware is required.

 

image

cstanton  has agreed to use his Pi4(2G) to run the test. Before starting the exercise, I will ask Christopher to review review the procedures and provide feedback. I'm keeping the the verbiage terse, assuming a higher level of understanding. If more details are required or feel something is more appropriate or missing please let me know.

 

A zip file of two flow graphs is attached. The file with basic is minimal as it gets. The second file provides a test module. I experienced a problem with both.

 

 

Test Procedure:

Fresh install of Raspbian Buster Full, current release.

Apply O/S updates/upgrades & Install GNU Radio

 

///CODE START///

sudo apt-get update -y;sudo apt-get upgrade -y

sudo reboot

sudo apt-get install gnuradio

///CODE END///

 

Take screen shots of htop screen at the following milestones.

1. O/S idle, no application running on the GUI desktop other than what is defaulted.

2. GNU Radio started, no flow graph

3. GNU Radio flow graph loaded.

4. GNU Radio flow graph started.

5. Evaluate audio coming from speaker and advise.

 

Depending on results, i would like to expand the test Ginny pig agreed.

 

Sean

 

Message was edited by: sean conway I have uploaded the two audio flow graphs for GNU Radio. The current version of GNU Radio encourages development in QT widgets verses the WX widgets. Three is discussion in the community support for WX will disappear. The flow graphs provided are QT. Sean

Attachments:
gnuradio.zip
gnuradio_FM.zip
  • Sign in to reply
  • Cancel
Parents
  • cstanton
    cstanton over 6 years ago

    Running Pi 4, 4GB in a cooled case

    - downloaded latest raspbian

    - installed latest updates

    - installed latest firmware

    - installed latest bootloader

    - ran sudo apt-get install rtl-sdr gnuradio gr-osmosdr

     

    image

     

    - opened gnuradio

     

    image

     

    - opened file audio_QTv1.grc

    - clicked to 'generate'

    - clicked to 'run'

    - received error 'xterm executable is missing, you can change this setting in your gnuradio.conf in section [grc] xterm_executable

    fix- https://steemit.com/raspberrypi/@chirimenjako/gnuradio-tips-terminal-error

     

    - Ran again

     

    execute:

    Warning: failed to XInitThreads()

    qt5ct: using qt5ct plugin

     

    (process:2326): Gtk-WARNING **: 21:36:30.684: Locale not supported by C library.

    Using the fallback 'C' locale.

    gr::log :INFO: audio source - Audio sink arch: alsa

    gr::log :ERROR: audio_alsa_sink0 - [default]: set_channels failed: Invalid argument

    Traceback (most recent call last):

      File "/home/pi/gnu/gnur/top_block.py", line 172, in <module>

        main()

      File "/home/pi/gnu/gnur/top_block.py", line 161, in main

        tb.start()

      File "/usr/lib/python2.7/dist-packages/gnuradio/gr/top_block.py", line 109, in start

        top_block_start_unlocked(self._impl, max_noutput_items)

      File "/usr/lib/python2.7/dist-packages/gnuradio/gr/runtime_swig.py", line 5656, in top_block_start_unlocked

        return _runtime_swig.top_block_start_unlocked(r, max_noutput_items)

    RuntimeError: check topology failed on audio_alsa_sink(2) using ninputs=1, noutputs=0

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to cstanton

    G'Day,

    The last line in your error message I have seen on other installs.

    RuntimeError: check topology failed on audio_alsa_sink(2) using ninputs=1, noutputs=0

     

    I haven't narrowed down the problem or a permanent fix. I have seen the error message posted but haven't found any reliable knowledge directing to a solution.

     

    I did stumble across a kludge that got GRC working.

    install gqrx-sdr and/or cubicsdr

     

     

    Take a look at my post above. I have another person who ran into problems.

     

    Can you tell me if you get GRC to run a flow graph. I suspect the audio may suck.

     

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to colporteur

    Another work around is to establish a bluetooth speaker. I just tested this and it eliminates the issue.

     

    A side effect, the audio sounds correctly. I suspect the bad audio was related to what ever audio configuration I had on the Pi. I haven't tested it yet but I am thinking the FM test circuit will work also.

     

    I am not familiar with Pi audio to identify the issue but that is where I think my investigation needs to go.

     

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 6 years ago in reply to colporteur

    Another work around is to establish a bluetooth speaker. I just tested this and it eliminates the issue.

     

    A side effect, the audio sounds correctly. I suspect the bad audio was related to what ever audio configuration I had on the Pi. I haven't tested it yet but I am thinking the FM test circuit will work also.

     

    I am not familiar with Pi audio to identify the issue but that is where I think my investigation needs to go.

     

    Sean