Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiRack and PiFace Digital 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 705 subscribers
  • Views 445 views
  • Users 0 members are here
  • raspberry_pi
Related

PiRack and PiFace Digital 2

nperkins99
nperkins99 over 10 years ago

Hi, I purchased 2 x PiFace Digital 2 and 1 x PiRack thinking that the the PiRack would extend the RPi to allow 2 x Digital 2 's to be connected. I have been trying to find doco on the web to see if the Digital 2 are compatible with the PiRack.

 

The main issue appears to be that the jumpers on the PiRack prevent the Digital2 from being fully connected to the GPIO pins.

 

Can anyone advise if the PiRack is compatible with the Piface Digital 2, or is there a new Rack that is not on Element14.

 

Kind Regards

Nathan

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    The PiRack is meant for the earlier PI's, not the B or PI2, one of the things that also changed was the use of the SPI lines etc. in some situations you can get the PI Rack to work but with board shapes and other factors it is probably not worth it

     

    If it is simply multiple PI Face Digital boards you want and your using a PI 2 then your best bet is the new PI Face Relay and Extra relay board, these have upto 8 relays on one board level and are also aparantly stackable so you would not even need a PI rack

     

    Hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    The PiRack is meant for the earlier PI's, not the B or PI2, one of the things that also changed was the use of the SPI lines etc. in some situations you can get the PI Rack to work but with board shapes and other factors it is probably not worth it

     

    If it is simply multiple PI Face Digital boards you want and your using a PI 2 then your best bet is the new PI Face Relay and Extra relay board, these have upto 8 relays on one board level and are also aparantly stackable so you would not even need a PI rack

     

    Hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • nperkins99
    nperkins99 over 10 years ago in reply to Robert Peter Oakes

    Peter, Thanks for the info, I probably should have researched a bit better.

    Oh well.