Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Lag when using 7" touch screen.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 703 subscribers
  • Views 2972 views
  • Users 0 members are here
  • raspberry_pi
Related

Lag when using 7" touch screen.

fischermachine
fischermachine over 6 years ago

Hi there,

 

I'm experiencing constant lag on loading screens and in all games in a rhythmic pattern in conjunction with the sound. I have multiple Pies and SD card builds that all work perfectly with HDMI tvs and monitors, but all have the same lag issue with this screen. I've updated all core packages from the retropie setup script. Between loading screens I get this error: 1V10 volume control :: init() - failed to find mixer elements.

 

Here is my setup:

 

Retropie on a PI 3 B+

Element 14 Raspberry Pi 7" Touch Screen Display

Northpada 5V 3A power supply

 

Not sure what else to do,
Will

  • Sign in to reply
  • Cancel
Parents
  • fischermachine
    fischermachine over 6 years ago

    On Shabaz's advice I've started looking for audio problems alone that were like mine. Most of the threads/posts seem to be from 2013 or so. Like this one here. https://www.raspberrypi.org/forums/viewtopic.php?t=60353  Unfortunately the solution was to eliminate the component cable and only use HDMI.

     

    This one from 2016 https://raspberrypi.stackexchange.com/questions/3626/how-to-get-better-audio-quality-from-audio-jack-output  has a work around using a USB audio device and some fixes here https://www.raspberrypi.org/forums/viewtopic.php?f=35&t=20445 from 2012.

     

    Seems like this problem was fixed or should have been fixed. Newer posts having to do with audio have a lot of the same fixes , but for different problems. https://github.com/alexa-pi/AlexaPi/wiki/Audio-setup-&-debugging

     

    After reading the negative reviews on Amazon it seems to me this screen should not be sold as an official Raspberry PI - plug and play.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fischermachine
    fischermachine over 6 years ago

    On Shabaz's advice I've started looking for audio problems alone that were like mine. Most of the threads/posts seem to be from 2013 or so. Like this one here. https://www.raspberrypi.org/forums/viewtopic.php?t=60353  Unfortunately the solution was to eliminate the component cable and only use HDMI.

     

    This one from 2016 https://raspberrypi.stackexchange.com/questions/3626/how-to-get-better-audio-quality-from-audio-jack-output  has a work around using a USB audio device and some fixes here https://www.raspberrypi.org/forums/viewtopic.php?f=35&t=20445 from 2012.

     

    Seems like this problem was fixed or should have been fixed. Newer posts having to do with audio have a lot of the same fixes , but for different problems. https://github.com/alexa-pi/AlexaPi/wiki/Audio-setup-&-debugging

     

    After reading the negative reviews on Amazon it seems to me this screen should not be sold as an official Raspberry PI - plug and play.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 6 years ago in reply to fischermachine

    Hi Will,

     

    From the symptoms you described, it still seems like a RetroPie script or Raspbian image or sound driver issue.

    I don't think it is anything to do with the display. The symptom likely has a different root cause basically, and the result is lag from the application itself (some of this is speculation - but it's a reasonable guess). You can test by trying to run an application that has no sound capability. If it runs with no lag (well, no lag compared to HDMI) then that's a strong indicator. Have you run such tests?

     

    The display is a mature product (been available for several years) and is intended for kids to use to learn programming with the Pi.

    Once you go beyond that and start loading up games emulators with sound capability, although it can work, I'm not overly surprised if it needs troubleshooting since whoever last updated the scripts or the drivers may not have tested that combination (display plus particular retropie script you're using).

     

    As well as the test mentioned above, have you tried to disable audio capability in Retropie, as a temporary test to see if it resolves the lag from the application?