Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum RPi 3 B+ with Sense Hat getting "Error: cannot open framebuffer device." from snake.c example
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 703 subscribers
  • Views 5733 views
  • Users 0 members are here
  • sense hat
  • frame_buffer
  • raspberry_pi_3b+
Related

RPi 3 B+ with Sense Hat getting "Error: cannot open framebuffer device." from snake.c example

osenjw
osenjw over 6 years ago

I am new to RPi.

 

I placed the sense hat on an RPi 3B+ and get a nice rainbow display on the LED.

 

When I run the snake example, I get the message "Error: cannot open framebuffer device."

 

I run in debug using Code::Blocks, and I see that the code apparently finds the joystick.  So the frame buffer is not the first thing I checked.

 

My RPi is nearly virgin.  I have installed Code::Blocks and the sense hat.  Raspian is up to date.  I enabled VNC, SSN, SPI and I2C.

 

I am working headless via a VNC window in W10.

 

Is there an incompatibility between a RPi 3B+ and the sense hat?  I am seeing that it is compatible with RPi 3B  (no +).

 

If not, would somebody offer a suggestion for getting snake to get past this error?

 

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • mp2100
    mp2100 over 6 years ago

    Can you try to use the Sense Hat with a computer monitor attached to the RPi, that is, don’t run it headless?  I would have thought that VNC would provide a framebuffer, but it’s perhaps it doesn’t.

     

    There should not be any incompatibility with the RPi 3B+ Model, the Sense Hat is only using the 40 pin header, and that did not change between models.  Raspbian is quite stable between versions.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • osenjw
    osenjw over 6 years ago in reply to mp2100

    Thanks for the response.

     

    I have returned to running with a display attached through the HDMI, VNC off, keyboard + mouse attached, reboot and also shutdown + cold start.

     

    No change in behavior.

     

    Running a couple of the other python examples fail in the same manner.  The humidity sensor example fails when instantiating a sense hat, complaining about the frame buffer.

     

    Is there something I need to set in a boot time file?  I would be surprised, because such a requirement is not mentioned in a half dozen threads.

     

    I see nothing in RPi preferences.

     

    Thanks for any time you can think on this.

     

    This is truly a near clean system.  I just reset my SD card and started a clean slate yesterday, before adding the sense hat package.  As I recall the only other package I added was Code::Blocks.  I cannot imagine how a IDE would change the interface to the sense hat.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • osenjw
    osenjw over 6 years ago in reply to mp2100

    Thanks for the response.

     

    I have returned to running with a display attached through the HDMI, VNC off, keyboard + mouse attached, reboot and also shutdown + cold start.

     

    No change in behavior.

     

    Running a couple of the other python examples fail in the same manner.  The humidity sensor example fails when instantiating a sense hat, complaining about the frame buffer.

     

    Is there something I need to set in a boot time file?  I would be surprised, because such a requirement is not mentioned in a half dozen threads.

     

    I see nothing in RPi preferences.

     

    Thanks for any time you can think on this.

     

    This is truly a near clean system.  I just reset my SD card and started a clean slate yesterday, before adding the sense hat package.  As I recall the only other package I added was Code::Blocks.  I cannot imagine how a IDE would change the interface to the sense hat.