Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Helicopter animation using a Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 704 subscribers
  • Views 7195 views
  • Users 0 members are here
  • raspberry_pi
  • pi animation
  • programming in python
Related

Helicopter animation using a Raspberry Pi

colporteur
colporteur over 6 years ago

We are being encouraged by our leaders to practice social distancing and/or isolate ourselves where possible during this COVID19 crisis. To avoid going stir crazy while isolated in my home, I dug up an old project I have mulled over many times.

 

I would like to use a Pi to construct an helicopter animation. The best way to understand the goal of the project is let you take a look at the video. https://www.youtube.com/watch?v=Hl5--7g3jO0&t=112s

 

My first task is to build the light sequence. My light sequence is slightly different because it matches aviation specifications. There will be cabin lighting, landing lighting(front), position lighting (left/right/rear) and strobe lighting (top/bottom). All lights are either on or off with the strobes flashing when on. The lighting is being done with LEDs. Once I master the lights, I will integrate the audio and then tackle motor control. The Pi is responsible for running the whole show. I am looking to use python to accomplish the task. No, I am not interested in doing the project with an Arduino or in another programming language. Pi and python are my toolset. Hopefully I don't discover it is not possible.

 

What I am hoping for is some direction to developing the solution. I have no doubt this is programming 101 for many of you. I have much experience in programming. I have met and worked with people that have the skills to call themselves a programming. I am not a programmer.

 

The series of LED’s repeats the following sequence:

turn LED1 on solid

turn LED2 on flashing

turn LED3 on solid

turn LED4 on solid

turn LED4 off

turn LED3 off

turn LED2 off

turn LED1 off

cycle starts again.

 

My difficultly is creating the flashing LED within the sequence. I can turn all the LED's on and off. I can flash LED2 on its own. When I add flashing to the sequence LED2 flashes once and then the sequence continues with no more flashes. I require LED2 to flash continuous until it is turned off. I’m thinking I need to have a LED flashing routine (? another script) that is called in the parent script and continues to run (flash) until it is called to stop. I want to call it a fire and forget routine but that is my lack of programming terminology understanding.

 

I had this thought, write a code for a python module that flashes an led. Call the module in another python script giving it the pin number. The module should have a start and stop. Well that simple understanding of writing a module exceeds my knowledge. Since I'm not sure if what I am looking for is actually a solution, my research is proving difficult. If a module is what I need and you have a resource to assist in writing it, please let me know.

 

I'm not looking for someone to write the code but rather guide me to developing the code myself. Care to provide some insight into my helicopter animation COVID19 Isolation Project. There is no badge or points awarded, just a brain share. I look forward to your responses.

  • Sign in to reply
  • Cancel
  • dougw
    dougw over 6 years ago

    You could have a loop that runs at the flashing rate.

    Each time through the loop decide which LEDs and functions are active or inactive based on the loop count.

    Generally only the flashing LED will change each time through the loop, but after a certain number of loops each of the other functions will change state.

    The flashing LED may flash between a start count and an end count.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to dougw

    Thanks Doug for the reply.

     

    Help me understand you defintion of a loop? I have code that causes flashing. When I insert that code it runs once because my understanding of python is it is sequential. Step 1, step 2, step 3 and so forth. If step 2 is a loop that runs continious and the code advances to step 3 then a loop is what I think will work.

     

    I thought step2 as a function but that didn't work. I thought step2 as a called module but that didn't work. Now forgive me when I say module. I import another python script. I have been trying to understand class objects hoping that might be the solution.

     

    Can you provide a loop reference? When I research loops, i get the basic if then else return or while true.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago

    Programming folks I have been put onto something called concurrency through threading or multiprocessing. I will continue to read but would appreciate someone pulling me back from the edge if I am heading in the wrong direction.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 6 years ago in reply to colporteur

    Here is a description of loops in Python:

    https://www.learnpython.org/en/Loops

    Assume your whole sequence takes the same time as 100 flashes, you would have a while loop that runs while count < 100

    Inside the loop you can turn the flashing LED on if it is off else turn it off

    If you want to turn cabin lights on at a count of 10 it is just another if statement inside the loop like if count > 10 turn on cabin led

    if statement syntax can be found here:

    ttps://www.tutorialspoint.com/python/python_if_else.htm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to dougw

    OK we are both on the same page when it comes to understanding loops. I wanted to make sure your loop and my loop were the same before proceeding with the discussion.

     

    The turning on and then off of all lights is eight events. Four on and four offs. One of those events is a strobe. When the strobe is on, it is flashing. The whole sequence will occur over a specified time period. The whole eight event sequence is a loop.  That timing of the full loop will need to be refined as I integrate rotor animation and the sound. I'm estimating approx 2 minutes.

     

    If the strobe was at the end of the sequence then I can see a loop working. Turn all three lights on, run the another loop to generate the strobe and then proceed to turn all three lights off. Restart sequence. Since the strobe is in the middle of turning on the lights, it needs to be a fire and forget. My thought is to have a start loop routine, then proceed with the other events and during the off sequence a stop loop routine.

     

    I have been unable to separate the strobe to run independent from the other events. While the strobe loop is running the other two lights remain off. At least the way I have developed the code so far.

     

    while True:

       #helicopter lights on sequence,cab_lit,stb_lit,pos_lit,lnd_lit
       GPIO.setup(cab_lit, GPIO.HIGH)

      time.sleep(3)

      objled_test.start() <--- this piece of the puzzle (strobe) needs to continue to run as the sequence of events continues. The code is an example of a failed attempt.

      GPIO.setup(pos_lit, GPIO.HIGH)

      time.sleep(3)

      GPIO.setup(lnd_lit, GPIO.HIGH)

      time.sleep(3)

       # helicopter lights off sequence,lnd_lit,pos_lit,stb_lit,cab_lit
       GPIO.setup(lnd_lit, GPIO.LOW)

      time.sleep(3)

      GPIO.setup(pos_lit, GPIO.LOW)

      time.sleep(3)

      objled_test.stop()

      GPIO.setup(cab_lit, GPIO.LOW)

      time.sleep(3)

     

    Intergrated into this will be sound and motor control. I broke the animation into three components, light sound and motors. I'm working the light part now and add the others after that is equipped.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 6 years ago in reply to colporteur

    To calculate the number of loops in your while statement:

    Suppose your strobe flashes 2 times per second (when it is flashing). In 2 minutes it would have flashed 240 times.

    If it toggles on or off in each loop you would need 480 loops, with a 0.25 second delay at the end of each loop to make the 480 loops last 2 minutes.

     

    Suppose you want the strobe to be flashing for 10 seconds at the 1 minute mark and off the rest of the time.

    If the loop count is > 240 and < 280 then toggle the strobe LED on or off on each count else turn the strobe LED off

     

    Suppose you want the cabin lights on after 10 seconds and off after 100 seconds.

    If the count is > 40 and < 400 turn the cabin LEDs on else turn them off.

     

    For any of/off event you just choose at which count it needs to happen and use an if statement to make it happen, even the strobe flashing on and off events..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • glennvanderveer
    glennvanderveer over 6 years ago

    What I think you need for flashing led2 is a timer routine.  In theory, when you wanted the LED2 to start flashing, you would clear a counter(if needed), and start the timer.  When the time expires (this could be you flashing rate) the timer routine would toggle the LED2 GPIO pin, reset the counter(if using), and exit.  Then when you wanted to stop the LED2 flashing, you would just have to stop the timer.  No threading or multiprocessing needed...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to glennvanderveer

    Thank for your input.

     

    I have developed a routine that results in a LED2 flash that simulates a strobe. Varying the on and off times gives me the strobe effect I was looking for. When the routine is called, using my programming skills, the strobes either flash but the other LED's don't change or all the LEDs light up and nothing after that.

     

    House  isolation gives me the time to keep programming. Keep the suggestions coming.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • glennvanderveer
    glennvanderveer over 6 years ago in reply to colporteur

    Try looking here for hints on how to use a timer:  https://www.geeksforgeeks.org/timer-objects-python/

     

    Is this what you want to do:

     

    LED1 on

    LED2 start flashing

    LED3 on, LED2 keep flashing

    LED4 on, LED2 keep flashing

    <time passess>LED2 keep flashing

    LED4 off, LED2 keep flashing

    LED3 off, LED2 keep flashing

    LED2 off, LED2 stop flashing

    LED1 off, LED2 still off

    repeat...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to glennvanderveer

    Probably, this is the most elegant and efficient solution. The possible alternative I see is managing interrupts chained so every state set to a different state in the others but this is tricky and not interesting in this case. A real alternative, instead, at least in my opinion, is creating a dictionary in Python collecting every change in a different boolean variable. Then a single function will set/reset the LEDs on/off as well as the motor, sound, and any other part that should be included in the animation. This optimizes the code and makes easier to change the pattern of the animation.

    In the main infinite cycle while true if using a json file with different animation patterns these can be randomly looped to get a more interesting effect.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>