Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum please i need some help, i have a project but not sure how to ,,,
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 706 subscribers
  • Views 2268 views
  • Users 0 members are here
  • raspberry_pi
Related

please i need some help, i have a project but not sure how to ,,,

hannah_girl
hannah_girl over 6 years ago

hi all, my name is Hannah, i have built a car into a mini caravan, the car used to be a 2004 Citroen C5 estate, it has hydro suspension, which is electronic, i have manage to bypass the ecu which controls the hydro pump and fitted a remote switch, which you can raise or lower the car, that side of the project is fully working, but this is where i need some help,

 

the car has a height sensor which sense if the car is too high or too low etc, i wondered if i can use my Raspberry pi B to raise or lower the suspension when the car moves about,

i have tested the sensor which runs of a 5v power supply when the car is lower the output signal is 0.3v, and when its on high its about 4.3v. for normal height its about 2.3v

i am great at wiring, but a tad rusty to when it comes to software and programming, if anyone could point me in the right direction, i would be totally grateful,

if you would like more info on the c5 caravan project, please check out this video on you-tube,  https://youtu.be/crk6tFNhkYQ

thank you for your time, Hannah

  • Sign in to reply
  • Cancel
Parents
  • luislabmo
    luislabmo over 6 years ago

    Hello Hannah,

     

    Any particular reason why you are planning to use a Raspberry Pi?, usually a RPi is overkill for simple tasks and this sounds like one. From the little information we got maybe you can accomplish what you need with a cheap Arduino or even simpler micro-controllers like the ATtinys.

     

    Another important thing to know is what kind of output is needed from the sensor (is it analog or PWM -it sounds analog to me) considering that a RPi doesn't have analog outputs (you will need a DAC) or if the output is PWM, the RPi handles the PWM by software (which may be an issue as software in RPi is asynchronous) as far as I know.

     

    Finally if you will definitely need a RPi for this, a simple Python script will probably be handy for your needs.

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • hannah_girl
    hannah_girl over 6 years ago in reply to luislabmo

    the reason why i was thinking of a Raspberry pi is that i got 2 sitting in my draw doing nothing so didnt know if i could use them in my project,

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 6 years ago in reply to hannah_girl

    Gotcha!.

     

    Like Enrico said, you can use a RPi but you will need something in the middle as the RPi is not capable of analog (you will need to add a DAC or an Arduino that does the analog part for you). When coding in the RPi, the easiest I can think of is with Python which is already installed in Raspbian if you decide to go with this SO.

     

    Luis

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • hannah_girl
    hannah_girl over 6 years ago in reply to luislabmo

    ok that makes sense, so which arduino would you recommend? i just had a look in my draw and i found a 2 relay module which i can use between the rpi and the hydro pump, thank again hunnie ,

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 6 years ago in reply to hannah_girl

    It doesn't matter I guess, any of the basic ones will do what you need. I regularly use the pro-mini because that is the cheapest and the smallest one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to luislabmo

    Between a DAC and an Arduino, I suggest an Arduino, Amazon sells 5 Arduino Nano by 11 Euro. And these are not the cheapest, works fine and a more flexible, as well as better to program and connect to the Pi. I think that as you still have a Pi at home, it is not a bad idea because after setting the essential parts (sensor reading and car control) you have a powerful machine to do many other things. Just one I think now, is logging the number of times the pump is activated to place a max number of hours after starting the part maintenance, up to adding totally different features like mp3 player and more on your car because you have a Raspberry Pi.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to luislabmo

    Between a DAC and an Arduino, I suggest an Arduino, Amazon sells 5 Arduino Nano by 11 Euro. And these are not the cheapest, works fine and a more flexible, as well as better to program and connect to the Pi. I think that as you still have a Pi at home, it is not a bad idea because after setting the essential parts (sensor reading and car control) you have a powerful machine to do many other things. Just one I think now, is logging the number of times the pump is activated to place a max number of hours after starting the part maintenance, up to adding totally different features like mp3 player and more on your car because you have a Raspberry Pi.

     

    Enrico