Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Official RPI 7'' Touch screen power requirements ???
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 701 subscribers
  • Views 28150 views
  • Users 0 members are here
  • raspberry_pi
Related

Official RPI 7'' Touch screen power requirements ???

romeplstilchen
romeplstilchen over 6 years ago

Hello,

 

as soon as I plugged the official 7'' screen on may RPI 4, the firmware logo appeared

 

Raspberry Pi 7” Touchscreen Display

 

the one that says, there is a problem with the power supply

 

anyway in the end, I want to power the screen (and other peripherals)  with an external power supply

 

but I cannot find any power requirement about that very screen

 

thanks for your help

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 6 years ago

    Hi,

     

    The display consumption alone is about 550mA at 5V.

    With my Pi 3B attached to it, I see about 750 mA total power consumption (Pi + display) when the Pi is idling and not attached to anything else, and with a WiFi connection to a network but not transferring anything. You can use online Pi 3B and Pi 4 supply current consumption measurements done by others to extrapolate.

     

    However, to actually start up the Pi 3B with the display, current bursts to beyond 1100mA need to be supported by the power supply for the Pi + display. And once the Pi is running applications then of course the overall current consumption of the Pi and Display can exceed that.

     

    If you're getting a power supply related issue you'll need to use an 'official' Pi power supply, because it outputs slightly higher voltage of 5.1V, not 5.0V, and has heavier gauge wire to reduce the voltage drop at times of high current demand.

     

    If you're running a high load from the Pi's USB connectors or 40-way connector, then you may need to investigate other ways to power the peripherals independently. So, for instance, a USB keyboard or mouse would be fine, but a USB powered spinning drive might not - it's experimental because there is no datasheet specifying the precise limit, it's a low-end consumer product.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • romeplstilchen
    romeplstilchen over 6 years ago in reply to shabaz

    [admin : I always have to reset my pass to be able to login, afterwards my login/pass never works]

     

    I use the official power supply with nothing else connected to the RPI4 but that screen

     

    actually , the first time I saw that firmware warning was right after installing the screen (which is powered from 5V/GND from the GPIO)

     

    thanks for the infos

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • romeplstilchen
    romeplstilchen over 6 years ago in reply to shabaz

    [admin : I always have to reset my pass to be able to login, afterwards my login/pass never works]

     

    I use the official power supply with nothing else connected to the RPI4 but that screen

     

    actually , the first time I saw that firmware warning was right after installing the screen (which is powered from 5V/GND from the GPIO)

     

    thanks for the infos

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 6 years ago in reply to romeplstilchen

    I see; that could be related to the Pi's software image (the alert threshold could have been tweaked in firmware) or could be benign if you're just on the edge due to tolerances. If there's non-critical things stored/running on the Pi then that may be good enough for some scenarios. Otherwise there is a way to power the display from a separate supply although that can be undesirable sometimes. I can't really suggest much more, my Pi 4's are not connected to that display unfortunately.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • romeplstilchen
    romeplstilchen over 6 years ago in reply to shabaz

    yeah I thought it was odd since it is supposed to be the official RPI screen, yet again the RPI4 seems picky on the side of it's power supply :-)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • hugohu
    hugohu over 6 years ago in reply to romeplstilchen

    I use GPIO power with my Pi4 and there's not been a problem. USB isn't good on the other hand.