Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Expanding the Raspberry Pi file system
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 703 subscribers
  • Views 1609 views
  • Users 0 members are here
  • raspberry_pi
  • raspbian
Related

Expanding the Raspberry Pi file system

colporteur
colporteur over 6 years ago

Does anyone have a quick history lesson so that I avoid a full chase the squirrel engagement, on the A1 Expand Filesystem option, under the Advanced Options in the raspi-config tool?

 

I stumbled across a suggestion to expand the file system while researching a project. Instead of fully engaging and chasing this squirrel, I thought someone in the community might just have a quick answer.

 

I recall at one point in Raspbian (RP OS) development the operating system would indicate it was expanding the filesystem and then reboot. I don't recall seeing that message lately. Does the automatic SD card expansion still exist? Does the option described above utilises the full capacity of any SD card installed or are their limits?

 

I confess this is me being lazy but still curious of the answer. Any response off the top of your head?

  • Sign in to reply
  • Cancel
  • gdstew
    gdstew over 6 years ago

    The Raspberry Pi OS (or Raspbian) image file you copy to an SD card is out of nessesity smaller than the capacity of the SD card. That option expands

    the file system to the full size of the SD card. This has been done automatically after the first boot for a few years now so it is usually not needed. It

    should not cause any problems if you use that option after the file system has already been expanded as the program will see that it has nothing to

    do and exit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago

    Is answering your own question talking to yourself?

     

    While waiting for an E14 webinar to start I took a few minutes to resolve my question.

     

    I used two SD cards a 16G and 32G for this test. I formatted them with RP OS 2020-05-27. When installed the full size of the card capacity was available in the file system without having to perform any actions.

     

    I'm not sure what the raspi-config menu option mentioned in my post provides. It appears the O/S uses what ever the card capacity is to set up the file system. I did notice the 32G card on first boot took a little while longer to respond to an ssh connection. I'm going to assume it was working on the file system formatting for a larger SD card.