Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum amateur transiever
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 529 views
  • Users 0 members are here
Related

amateur transiever

e14 Contributor
e14 Contributor over 10 years ago

Can everybody to make amateur raadio transiever on base arduino or rasberry?

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 10 years ago

    There is a lot of projects on the web for a Software Defined Radio (SDR) using a USB receiver with the RPi.

     

    I have not seen any with a transmitter attached, though I suspect a good RF engineer or HAM radio operator could connect the SDR to a transmitter.

     

    Over the years, I have seen a lot of people set up digital over RF for communications with known receivers and transmitters, so it should be easy to do.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to DAB

    Yes there are plenty of examples. We have the RPI been used to create some RF directly (probably quite dirty).

    Driving modules  like the Ciseco or LPRS or merely providing  control to the display and frequency control in transceiver kits.

     

    For SDR many do have RF outputs for example the HackRF or the ubiquitous USRP .

     

    The reason(s) you see so many more receivers than transmitters are probably several fold.

     

    1) you'll need a licence to transmit on most frequencies

    2)you need reason to transmit something ... many receiver projects are curiosities

    3) transmitters tend to require more exacting standards in terms of filtering outputs, matching to antennas etc which tends to up the cost of entry. While a receiver will work with almost any old bit of wire even if the match is poor.

     

    4) powers tend to be limited out of the device to say less than 200odd mw which isn't  great and PAs tend to be best at given bands (back to no(3)) etc

    QRP(low power) would be an interesting experiment with these devices!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Problemchild
    Problemchild over 10 years ago in reply to DAB

    Yes there are plenty of examples. We have the RPI been used to create some RF directly (probably quite dirty).

    Driving modules  like the Ciseco or LPRS or merely providing  control to the display and frequency control in transceiver kits.

     

    For SDR many do have RF outputs for example the HackRF or the ubiquitous USRP .

     

    The reason(s) you see so many more receivers than transmitters are probably several fold.

     

    1) you'll need a licence to transmit on most frequencies

    2)you need reason to transmit something ... many receiver projects are curiosities

    3) transmitters tend to require more exacting standards in terms of filtering outputs, matching to antennas etc which tends to up the cost of entry. While a receiver will work with almost any old bit of wire even if the match is poor.

     

    4) powers tend to be limited out of the device to say less than 200odd mw which isn't  great and PAs tend to be best at given bands (back to no(3)) etc

    QRP(low power) would be an interesting experiment with these devices!