Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi won't boot with noise and PWR lit only
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 708 subscribers
  • Views 7201 views
  • Users 0 members are here
  • problem
  • issue
  • raspberry_pi
  • raspberrypi
  • boot
Related

Pi won't boot with noise and PWR lit only

wcypierre
wcypierre over 10 years ago

Had been running this pi for 24x7 for about a year now and it has been running fine until I realized that it was down just now when I went to do some checking.

Heard some noises too and now I can't seem to get it back up (noise + PWR lit + dim ACT light only).


Model: Raspberry Pi B

OS: Raspbian

Things attached to the pi: LAN cable, SD Card

Video to demonstrate the noise that the pi makes: https://drive.google.com/file/d/0BwiJswXag8O4dkNKbmlmRVBKOW8/view?usp=sharing


Note: I'm using Powerbank to power the pi up just for the sake of taking the video, normally it is attached to a better power supply.


Symptoms:

1. Red PWR light

2. dim ACT light

3. Noise made as per video above


Things that I've tried:

1. Changing the Power Supply(tried from my original source to genuine Pineng Powerbank to Nokia's official charger to Xiaomi's official charger to the charger that was shipped with the pi)

2. SD Card (it was working on the other pi and the other sd card that I've put into from the other pi doesn't work)

3. LAN cable

4. HDMI - No output

5. Composite - No output

6. Heating it up (https://www.youtube.com/watch?v=AwF6v-4NFdg)

7. Holding the sdcard slot to ensure that the issue isn't with the sd card slot

8. R-Pi Troubleshooting - eLinux.org (the "Red power LED is on, green LED does not flash, nothing on display" part)


Things that I know but I couldn't try because of limitations:

1. Serial console


Any other things that I can try of?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    clem57 over 10 years ago

    Rebuild SD card with the latest version OS rom the web.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wcypierre
    wcypierre over 10 years ago in reply to clem57

    I've rebuilded the latest raspbian jessie lite but to no avail.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to wcypierre

    Look at http://www.element14.com/community/thread/48472/l/raspberry-pi-2-appears-dead to check a possible problem.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 10 years ago in reply to wcypierre

    Look at http://www.element14.com/community/thread/48472/l/raspberry-pi-2-appears-dead to check a possible problem.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wcypierre
    wcypierre over 10 years ago in reply to clem57

    I don't have the tools to power up a pi from gpio. I've tried with a few sd cards that are working on my other pis but it just wouldn't work at this pi. I've already most all of the methods here R-Pi Troubleshooting - eLinux.org  except for the polyfuse one. I don't have a multimeter but I do have this https://gd3.alicdn.com/bao/uploaded/i3/TB10XaoKpXXXXb_XXXXXXXXXXXX_!!0-item_pic.jpg_600x600.jpg and this power output is enough (4.8v 1A). Is the sound made when I boot up the pi a concern over here? because I feel like it does but I don't know which component causes it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to wcypierre

    Do you have a soldering Iron and an old but good USB cable, if so

     

    Cut the end of the USB cable that would go into the PI (Not the end that goes into the power supply)

     

    expose the power wires from the cut end of the USB cable

     

    Make sure the power adapter is giving out 5V (USB specifications allow it to go well below 5V, but the PI may not work), you say your PSU is 4.8V, If this is with no load then it will be less than this once connected and I feer too low for reliable operation, you need to have a better power supply that reads 5 or more volts with no load or 5 when connected to the pi

     

    now connect these to the 5V and 0V GPIO pins taking care to connect only the 5V and 0V pins and not short to ither pins

     

    There is nothing on the PI that should be making a noise, if there is a noise from the PI, this would imply that it is heat related and is a component of some sort expanding or contracting or the inductor on the power supply buck reg is acting up so even by supplying 5V via a GPIO pin does not ensure the PI will work as the 3V3 rail could be the issue and that is generated on board.